Infineon partners with Enphase to enhance energy-efficiency and reduce MOSFET-related costs with 600 V CoolMOS™ 8
Infineon partners with Enphase to enhance energy-efficiency and reduce MOSFET-related costs with 600 V CoolMOS™ 8
テクノロジーニュース
Munich, Germany – 17 March 2025 – The 600 V CoolMOS™ 8 high-voltage superjunction (SJ) MOSFET product family from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) has allowed Enphase Energy, a global energy technology company and a leading supplier of microinverter-based solar and battery systems, to simplify its system design and reduce assembly costs. By using the 600 V CoolMOS 8 SJ, Enphase is able to significantly reduce MOSFET resistance (R DS(on)) for its solar inverter systems, leading to lower conduction losses, which improves overall device efficiency and boosts power density. In addition, the company achieved MOSFET related cost savings.
“We are thrilled to partner with Enphase and support their mission to deliver innovative solar energy solutions,” said Richard Kuncic, Senior Vice President and General Manager at Infineon. “Our 600 V CoolMOS 8 SJ MOSFETs are designed to provide superior efficiency, reliability, and cost savings, which aligns perfectly with Enphase’s and Infineon’s commitment to advancing the performance and affordability of renewable energy technologies, further driving decarbonization.”
“Collaborating with Infineon has allowed us to leverage their CoolMOS 8 SJ MOSFET technology to enhance the performance and cost-effectiveness of our microinverter systems,” said Aaron Gordon, Senior Vice President and General Manager of the Systems Business Unit at Enphase Energy. “This partnership underscores our dedication to innovation and excellence in the solar energy industry, and we are excited about the significant improvements in power density and cost savings that we are now able to offer our customers.”
Infineon's latest CoolMOS 8 MOFETs at 600 V are leading the way in high-voltage superjunction MOSFET technology worldwide, setting the standard for both technology and price performance on a global scale. The technology increases overall system performance and further reinforces decarbonization in applications such as chargers and adapters, solar and energy storage systems, EV charging, and uninterruptible power supplies (UPS).
The CoolMOS 8 SJ MOSFETs have an 18 percent lower gate charge than the CFD7 and 33 percent lower than the P7 series. A reduced gate charge allows for less electric charge to be applied to the gate of a MOSFET to switch it from the off state (non-conducting) to the on state (conducting), enabling a more energy-efficient system performance. Additionally, the CoolMOS 8 SJ MOSFETs have the quickest turn-off time in the market and their thermal performance has been improved by 14 to 42 percent compared to the previous generation. The 600 V CoolMOS 8 SJ technology is equipped with an integrated fast body diode and is available in SMD-QDPAK, TOLL, and Thin-TOLL 8x8 packages, making it suitable for a wide range of consumer and industrial applications.
Availability
Samples for the portfolio extension of 600 V CoolMOS 8 SJ MOSFETs and 650 V CoolMOS 8 SJ MOSFETs are available from early April on. More information is available at www.infineon.com/coolmos8.
Learn more about the benefits of Infineon’s 600 V CoolMOS 8 SJ MOSFETs in the whitepaper here: “Infineon’s CoolMOS 8 proves that high-voltage silicon-based technologies still play a prominent role in power electronics”
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
600 V CoolMOS 8
600 V CoolMOS™ 8 by Infineon enhances energy-efficiency and reduce MOSFET-related costs
JPEG
2126x1152 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFPSS202503-081