TRUSTECH 2024: Infineon showcases solutions that shape the future of payment and identity applications
TRUSTECH 2024: Infineon showcases solutions that shape the future of payment and identity applications
テクノロジーニュース
Munich, Germany – 29 November 2024 – At TRUSTECH, the trade show for innovative payment and identification solutions, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) will present innovative payment and ID solutions that support an environmentally friendly, secured, and convenient lifestyle. At booth G 035 in Pavilion 5.2, visitors can enter Infineon's futuristic green park, a city center hub that demonstrates how the company is enabling the future of payment and identity. The products, demonstrations, and design tools presented at the trade show include environmentally friendly payment cards made from sustainable materials, biometric payment cards with flexible enrollment options, and various eID cards and passports with ultra-thin eDatapages in interactive use cases. The following solutions will be showcased:
- SECORA™ Pay Green for up to 100 percent less plastic waste: SECORA Pay Green is the pioneer of a new generation of payment card technologies. The solution sets new standards in recyclability and combines Infineon's new environmentally friendly Coil-on-Module (eCoM) package, which contains the security controller and all software components, with an integrated contactless antenna to simplify the recycling of dual-interface payment cards. At the end of the card's service life, the complete eCoM package can be removed from the card and disposed of as electronic waste. The homogeneous card body can then be recycled as plastic, wood or paper, depending on the original material used.
- SECORA Pay Bio for the next level of biometric payment cards: SECORA Pay Bio integrates Infineon's enhanced SLC39B System-on-Chip (SoC) Secure Element and the FPC1323 sensor from Fingerprint Cards AB (Fingerprints™) into the Biometric Coil on Module (BCoM) package, utilizing the benefits of inductive coupling technology. The solution uses the biometric credentials securely stored on the card as a second authentication factor, enabling convenient and secured contactless payment.
- Infineon's eID-OS solution and packaging for ultra-thin eDatapages in passports: The eID-OS native government ID solution is based on the proven TEGRION™ SLC26 security controller. It comes with various applets that support all mainstream government applications such as ePassports, national electronic ID cards, electronic driving licenses and eHealthcare cards. eID-OS is available in the innovative CoM contactless package technology, allowing for ultra-thin electronic datapages in passports. This reduces polycarbonate material consumption and helps minimizing carbon emissions, making it a more environmentally friendly option.
- New SECORA ID solutions and applets to accelerate eID projects: SECORA ID is a ready-to-use Java Card™ solution optimized for electronic ID use cases. It accelerates time-to-market while enabling easy and efficient customization to support local eID and multi-application systems. In combination with a dedicated tool, the SECORA ID platform also offers customers maximum freedom to develop their own customized applets.
- FIDO authentication and security solutions redefine modern user authentication. In today's connected world where security is paramount, Infineon's ID key products offer a range of solutions for securing physical and digital assets. These include USB and USB/NFC token products featuring dual-chip SMD packages with integrated security controllers and USB and NFC interfaces certified to Common Criteria EAL 6+ level.
Meet the Infineon experts
At the Innovation Stage at TRUSTECH, visitors will have the opportunity to discuss the following topics with Infineon experts:
- “Next-level controller architectures for the security challenges of tomorrow”, on 3 December 2024 at 3:30 pm presented by Robert Bach, Director Product Marketing for Government ID.
- “Convenient, innovative and trusted biometric solutions: Make easy and scalable biometric payment front-of-wallet” on 4 December at 4:30 pm presented by Fang Lu-Ruhbach, Product Marketing for SECORA Pay Bio.
- “Innovation for more sustainable payment cards: Up to 100% reduction in plastic waste and shrink of carbon footprint with SECORA Pay Green” on 5 December 2024 at 12:30 pm presented by Ester Jimenez, Product Marketing for payment and transport applications.
Infineon at TRUSTECH 2024
Visit Infineon at this year’s TRUSTECH from 3 to 5 December at Paris Expo Porte de Versailles, booth G035 in Pavilion 5.2. This year, the Infineon booth will present a futuristic green park – a city center hub showcasing innovative payment and identity solutions and technologies, all of which can be implemented today. Visitors can dive into the future of payment and identity, where nature and digital technologies interconnect for green, secured, and convenient lifestyles. More information is available at www.infineon.com/trustech.
About Infineon
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Further information is available at www.infineon.com
This press release is available online at www.infineon.com/press
Press Photos
Secora Payment and ID Solutions
Infineon’s innovative payment and ID solutions support an environmentally friendly, secured, and convenient lifestyle.
JPEG
2126x1256 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFCSS202411-031