Infineon at CES 2023: Enabling a sustainable future with smart home, electromobility and IoT security solutions
Infineon at CES 2023: Enabling a sustainable future with smart home, electromobility and IoT security solutions
テクノロジーニュース
Munich, Germany and Las Vegas, Nevada – 20 December, 2022 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced that it will highlight the company’s contributions to mitigate climate change and enable digital transformation at CES 2023. Located at the Venetian Titian Ballrooms 2204 & 2205 and LVCC West Hall booth #3829, Infineon will present IoT security solutions, smart sensors and dependable semiconductor solutions that help shape a sustainable future. With semiconductors at the heart of the transformation to a net zero economy, the company will display a number of demonstrations that outline its drive towards decarbonization and digitalization including:
Innovative, intelligent and IoT security solutions for a sustainable future
Located at the Venetian Titian Ballrooms, Infineon will showcase a variety of security solution ranging from state-of-the-art hardware security controllers with software, to Matter-enabled product solutions. Demonstrations include Infineon’s CIRRENT™ Cloud ID with OPTIGA™ Trust M Express for easy device provisioning and cloud onboarding. The Cloud Connectivity Manager is a service that enables managing a secured device identity between the silicon and cloud layers. Other show highlights comprise Wi-Fi 6 LE audio demonstrations, along with a variety of Matter-enabled devices including battery-powered applications and a Wi-Fi smart lock, and many more.
As a leader in IoT systems and power electronics, Infineon will showcase value-added solutions to today’s green and digital transformation challenges. For example, Infineon is working with the non-profit organization Rainforest Connection (RFCx) to use Infineon’s semiconductor solutions to help monitor and protect vulnerable rainforest ecosystems. The technology enables RFCx and its partners to detect wildfires in real-time, along with other potential threats to wildlife. Along with this demonstration, Infineon will also showcase a variety of environmental, power, smart home and building applications. Demonstrations include Infineon’s smart alarm system (SAS) and XENSIV™ connected sensor kit (CSK) which were both selected as CES 2023 Innovation Award Honorees.
Driving decarbonization and digitalization through dependable electronics
At the LVCC West Hall booth #3829, Infineon will showcase a wide range of automotive solutions in an open car frame. Highlights include Assisted Driving Assistance (ADAS), lighting systems, wireless battery management, and over-the-air security firmware updates, along with a variety of touch solutions throughout the vehicle. Infineon will also highlight its in-cabin monitoring systems solution using a 60 GHz radar sensor and the HybridPACK™ Drive – the company’s market-leading power module. Infineon’s EXCELON™ F-RAM used in automotive was also recently selected as a CES 2023 Innovation Award Honoree.
Additionally, Infineon will showcase the luxury Lucid Air Model EV with over a 400 mile range. The company will also demonstrate the REEcorner™ technology as part of a modular platform design for next-generation vehicles.
Don’t miss the panel titled “The Era of Sustainable Consumer Electronics” on Saturday, January 7, 10:00 – 10:40 a.m. at the LVCC West, Level 2, W219. Moderated by Co-Founder of Penney Consulting & Elemental Content John Penney, the panel will include Infineon’s President of Americas Bob LeFort, along with executives from Qualcomm, 3M and LG Electronics.
Infineon at CES 2023
The Consumer Electronics Show (CES) 2023 will be held from 5 to 8 January 2023 in Las Vegas, Nevada. See how Infineon drives decarbonization and digitalization together with its partners and customers at the Venetian Titian Ballrooms 2204 & 2205 located at The Venetian Hotel, Level 2, and at the Las Vegas Convention Center, West Hall (Booth 3829).
More information is available here. Editors interested in an interview with an executive, can contact their respective regional Media Relations manager. Industry analysts interested in a briefing, can email: MarketResearch.Relations@infineon.com.
Press Photos
CES 2023 Visual
At CES 2023, Infineon will present IoT security solutions, smart sensors and dependable semiconductor solutions that help shape a sustainable future. With semiconductors at the heart of the transformation to a net zero economy, the company will display a number of demonstrations that outline its drive towards decarbonization and digitalization.
JPEG
2126x1196 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFXX202212-042