Background for document preview
Background for thumbnail

AN226036 - SMC_ZPD implementation in TRAVEO T2G family

This application note describes how to implement SMC along with ZPD using the TRAVEO T2G family CYT4D series MCU device. A stepping motor is typically used to operate the needle of an automotive meter. The SMC is implemented by using the counter and PWM functions of the TCPWM block in the TRAVEO T2G MCU. ZPD is a function to recognize the stop position in SMC. ZPD is implemented by using the pulse detection function of the ADC block in the TRAVEO T2G MCU.

• 297.84 KB
• 2023/11/29