AN091611: Radome design guide for XENSIV™ BGT60LTR11AIP 60 GHz radar sensor
This application note provides a guideline on how to design radomes for the Infineon’s XENSIV™ 60 GHz radar BGT60LTR11AIP. General recommendation on the selection of the radome material as well as the proper values for the radome thickness and radome distance are given. Additionally, the effect of deviations from the recommended values are presented to emphasize the importance of a diligent radome design.
ご登録がお済みでない方は、 こちらから登録してください。