AIROC™ CYW559xx Connected MCU: Configuring dual-network stack in hosted mode
This application note provides step-by-step instructions to configure the AIROC CYW559xx Connected MCU in (SDIO) Network Co-Processor (NCP) mode interfaced with the CYW9RPIWIFIBT-EVK Wi-Fi & Bluetooth® Evaluation Kit with Raspberry Pi CM4 module as the host, loading the Linux driver(infhosted), establishing a Wi Fi connection between a station (STA) and an access point (AP).
ご登録がお済みでない方は、 こちらから登録してください。