AN229058 - Secure Firmware Over-The-Air _FOTA_ Update in Traveo II _Japanese
AN229058 explains the different steps involved in developing a secure and reliable firmware over-the-air (FOTA) update in TRAVEO T2G MCU. Note that this document does not explain the setting up of a wireless interface to perform an update over the air, rather explains how a logical flash bank in the TRAVEO T2G MCU can be updated with the new image and how reliably (using TRAVEO T2G MCU s Secure Boot mechanisms) the boot code can jump to the new image if successfully authenticated.
ご登録がお済みでない方は、 こちらから登録してください。