Infineon presents innovative microcontroller solutions supporting high-quality designs at embedded world 2025
Infineon presents innovative microcontroller solutions supporting high-quality designs at embedded world 2025
マーケットニュース
Munich, Germany – 27 February 2025 – Devices and systems – from automotive and industrial to consumer electronics – rely on powerful, efficient, and secured microcontrollers for reliable operation. At embedded world 2025 in Nuremberg, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) will showcase how its innovative semiconductor solutions meet these needs and drive further advancements. The company will present high-quality microcontrollers featuring the latest technologies, enhanced security, and high precision – delivering excellent performance with low-power consumption. True to the motto “Driving decarbonization and digitalization. Together.” the Infineon booth in Hall 4A (booth #138) will present highlights from the consumer and IoT, automotive, and industrial sectors that contribute to a more sustainable future. In addition, customers can register for Infineon's digital platform – the perfect place to dive deeper into the various technologies presented at embedded world during and after the event.
Infineon’s highlight topics at embedded world 2025
- Leading microcontrollers: The world of connected devices demands the highest reliability, precise calculations, robust security, energy efficiency, and user-friendly building blocks for high-quality designs.
At embedded world, Infineon will showcase its extensive MCU portfolio, featuring innovative solutions that drive progress. These include:
- PSOC™ microcontroller families
- TriCore™-based AURIX™ family
- AIROC™ Wi-Fi-connected MCUs
- MOTIX™ MCUs
- Paving the way for RISC-V in automotive: Committed to establishing RISC-V as the open standard for automotive applications, Infineon is collaborating with key ecosystem partners to accelerate the adoption and maturity of RISC-V-based solutions.
- CRA-ready IoT solutions: Security is a prerequisite for connected devices and can be accomplished through either a secured MCU or a discrete security element. Mandatory regulations like the EU Cyber Resilience Act (CRA) or global initiatives like Matter aim to protect consumers and businesses using digital products and software. To meet these requirements, Infineon provides a range of high-security, CRA-ready solutions with Edge Protect: PSOC microcontrollers deliver robust security features, while OPTIGA™ discrete security elements integrate seamlessly with each PSOC.
- System Solutions: To help developers fully leverage MCUs, Infineon offers a comprehensive range of software solutions tailored to various industries. DEEPCRAFT™ Studio, Infineon's edge AI development platform, and the DEEPCRAFT Ready Models, deliver an easy-to-use, end-to-end machine learning development experience – from data input to model deployment. ModusToolbox™, a suite of development tools, libraries, and embedded runtime resources, provides a flexible and powerful development experience.
- Enabling AI: AI is transforming our world, and to unlock its full potential, companies need a partner offering a diverse portfolio of AI hardware and software solutions – from Automotive AI and AIoT to Industrial AI. Infineon provides specialized microcontrollers and highly precise sensors that enable intelligent and adaptive edge AI systems. Infineon’s high-performance, energy-efficient power supply solutions sustainably support the growing demands of AI applications.
Infineon at embedded world
Embedded world will take place in Nuremberg, Germany from 11 to 13 March, 2025. Infineon will present its products and solutions for decarbonization and digitalization in hall 4A, booth #138 and virtually. For press inquiries please contact media.relations@infineon.com. Industry analysts interested in a briefing can email MarketResearch.Relations@infineon.com. Information about the embedded world show highlights is available at www.infineon.com/embedded-world.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Embedded World 2025
Driving decarbonization and digitalization. Together. At embedded world 2025 in Nuremberg, Infineon Technologies AG will showcase high-quality microcontrollers featuring the latest technologies, enhanced security, and high precision – delivering excellent performance with low-power consumption.
JPEG
2126x1196 px
Information Number : INFCSS202502-068