Universal Serial Bus (USB) Type-C
The future-proof connector for power and data transfer
USB (Universal Serial Bus) was introduced in 1996 as plug-and-play standardized interface to unify data and power connectivity across electronic devices. It replaced the fragmented world of serial, parallel, PS/2, and other proprietary ports - eliminating manual configuration, simplifying peripheral setup, and overcoming the slow, inconsistent performance of earlier interfaces.
Early generations relied on larger, one‑directional connectors such as USB Type‑A and Type‑B, which often required different cables for data transfer and charging. As devices grew smaller and demanded higher power and faster data rates, the industry moved through mini‑USB and micro‑USB formats – both designed to reduce size but still limited by orientation issues and lower performance.
Growing pressure from global markets for a universal, waste‑reducing connector finally accelerated the shift toward a single, all‑in‑one solution: USB type-C – a fully reversible, compact interface design to support high-speed data (up to 40-80 Gbps), multi-protocol transmission, and advanced power delivery up to 240 W.
Since its launch, USB evolved from a simple plug-and-play interface for keyboard and mouse connectivity to becoming essential across countless applications and industries, so much so that it is one of the only words we understand regardless of the languages we speak.
Why USB Type-C became the universal connector of choice?
Scalable by design, future-proof for tomorrow
Up to 240 W and smart power negotiation
Up to 80 Gbps for video, storage and docking
Traditional power adapters relied on a wide range of incompatible connectors, fixed voltages, and limited current capabilities, making them impossible to share across devices and contributing heavily to cable clutter and e‑waste. USB‑C, by contrast, is a truly universal connector: a compact, fully reversible interface capable of negotiating voltage and current levels up to 240 W (48 V, 5 A) under USB Power Delivery, able to support high‑speed data rates up to 80 Gbps through USB4.
For consumers, USB‑C means one charger and one cable can power and transfer data across nearly all modern electronics, eliminating the need to accumulate and replace dozens of device‑specific adapters. This reduces both cost and electronic waste, an issue amplified by earlier transitions from Mini‑USB to Micro‑USB.
While USB-C is widely recognized for simplifying charging, its equally important role is enabling a unified and scalable data connectivity platform across modern electronic systems. One of USB-C’s biggest strengths is that it supports the entire spectrum of USB performance—from USB 2.0 at 480 Mbps to USB 3.2 and USB4 operating at tens of gigabits per second.
Due to its simple implementation, lower system cost & power consumption, and broad ecosystem compatibility, USB 2.0 continues to remain highly relevant in applications such as keyboards, audio accessories, industrial devices, microcontroller-based systems, biometric equipment, printers, and service/debug interfaces.
At the same time, through USB 3.x and USB4 technologies, USB-C also scales seamlessly into high-bandwidth applications including external SSDs, AI edge systems, docking stations, industrial cameras, and multi-display computing.
USB‑C has become essential in modern electronics because it solves the biggest limitations of previous connector standards while enabling new levels of performance, universality, and sustainability.
But USB‑C’s importance today extends far beyond technical advantages. Around the world, regulators are increasingly mandating universal charging standards to reduce electronic waste, with the European Union leading the way through its landmark Common Charger Directive. This legislation requires USB‑C as the mandatory charging port for ten categories of portable consumer electronics starting on December 2024, with the scope expanding to eleven categories when laptops are added from 28 April 2026
As more regions adopt similar sustainability‑driven policies, USB‑C is no longer just a convenience feature—it is becoming a compliance requirement and a cornerstone of environmentally responsible product design.
For manufacturers, embracing USB‑C delivers benefits that go far beyond simply meeting new regulations. Standardizing on a single, universal connector reduces production costs by eliminating the need to design, source, and ship multiple proprietary chargers and cables. It also simplifies global logistics—especially as free‑in‑box chargers disappear—while allowing companies to reuse the same power and interface solutions across entire product families. This consolidation streamlines product portfolios, reduces component variation, and supports the industry‑wide shift toward circular, waste‑reducing electronics. Most importantly, USB‑C frees R&D teams from managing legacy connector fragmentation, enabling them to focus on the features and innovations that truly differentiate their products, accelerate development cycles, and shorten time to market.
Said so, embracing USB‑C for manufacturers means future‑proof performance, regulatory compliance, and meaningful environmental impact all at once.
USB‑C has become essential across a rapidly widening range of applications and industries. While it is already the default connector for consumer electronics, its simplicity, high power capability, and universal form factor are now driving adoption in higher‑power segments such as power tools, light electric vehicles (e-kickscooters, e-bikes), and portable home appliances (e.g. cordless vacuum cleaners), where a single robust connector can streamline charging and reduce accessory complexity. The shift of smartphones and tablets to USB‑C has also accelerated the transition in automotive interiors, where in‑cabin chargers increasingly rely on USB‑C Power Delivery controllers to support fast and reliable charging for multiple passenger devices.
Beyond power, USB‑C has also established itself as a versatile data interface across industrial environments. It is widely used in machine vision, data acquisition, test and measurement, medical devices, and robotics, leveraging USB 2.0 and USB 3.2 for reliable connectivity in fields ranging from factory automation to life sciences, retail systems, and security and surveillance. As newer USB data rates such as 10 Gbps and 20 Gbps become mainstream, USB‑C continues to unlock advanced, bandwidth‑intensive applications and bring digitalization into an even broader set of industries.
Infineon’s USB portfolio
USB-IF certified solutions for seamless plug-and-play interoperability
Over five billion units shipped worldwide
Wide documental support, software suites, code examples and peer2peer support via the developer community.
Infineon has been the absolute leader in the USB space, with over one billion units shipped and continuous innovation in emerging USB technologies. In October 2014 the first USB PD controller was introduced to the market, and ever since it kept innovating in power and data transfer.
Today the portfolio covers power adapters, cable, automotive, computer and consumer electronics applications with market-proven, USB-IF certified, highly integrated solutions.
USB selection guide
Get instant access to our USB selection guide, featuring a comprehensive overview of Infineon's USB power and data solutions for consumer, industrial, and automotive applications. Explore the key product categories, including USB-C Power Delivery (PD) controllers, USB 3.2 peripheral controllers, USB 2.0 peripheral controllers, and USB hubs.
- EZ-PD™ family of USB-C Power Delivery controllers for more robust end-to-end PD and charging, including AEC-Q100 certified versions for automotive-grade performance
- EZ-PD™ portfolio of charger adapter power solutions with scalable PD controller architecture to support multi-port market needs
- EZ-USB™ portfolio of programmable USB 2.0 peripheral controllers, including configurable and fixed-function bridging interfaces (UART, I2C, and SPI)
- EZ-USB™ portfolio of 3.2 peripheral controllers for USB 1.1 to USB 20 Gbps
- EZ-USB™ hub controllers support USB 2.0, USB 5 Gbps, and 10 Gbps for advanced USB PD and battery charging capabilities.
- USB-C adoption solutions: plug-and-play EZ-PD™ Barrel connector replacement, or USB-C high voltage MCUs for additional customization and programmability