Aerospace Defense Memory
-
On this page
About
Infineon works with leading ecosystem and chipset vendors worldwide that are comprised of a network of highly qualified and experienced companies such as AMD Xilinx, Microchip and Alpha Data. Our partners are dedicated to designing and delivering exceptional products and solutions for the Space sector. Many also design and produce reference designs which gives you access to turnkey system solutions that give you a head start in your development.
At Infineon, our global ecosystems are the core of our partner program, comprised of highly qualified and experienced companies that are dedicated to designing and delivering exception products and solutions for the Space sector.
Most system designers choose a chipset before selecting a memory device. If this is the case, locate your vendor of choice in the table of chipset pairing charts. Determine which interface or memory type you need, and open the appropriate spreadsheet. In the spreadsheet, locate your specific chipset and select from the list of qualified memories. If you are in an exploratory phase of your design, chipset pairing charts are also a great way of finding the best Infineon solution(s) for your potential chipset choice, and for fine-tuning the selection of memory interface, voltage, density, etc.
Do you have a question about pairing Infineon memory with a particular chipset, whether or not referenced on our site? Do you have a more generic question about Infineon memory support with a given chipset partner? Are you a chipset partner and want to work with us? Please get in touch!
Supported Space FPGA’s
- Xilinx V5SiRF
- Xilinx Kintex KU060
- MicroChip RTG4
- MicroChip PolarFire
- AMD Versal
- Alpha Data Versal
DevKit Mezzanine Cards
CYDK-QDRII-NODT - Memories - On request
QDR-II+ Synchronous SRAM mezzanine card for testing the highest performing memory for space applications This devkit board has been developed to work with the Infineon Rad Hard 72 & 144-Mbit QDR®-II+ Synchronous SRAMs. The board is developed and tested to work with FPGA carrier cards through the FMC-HPC connector.
CYDK-QDRII-LA - Memories - On request
QDR-II+ Synchronous SRAM Logic Analyzer mezzanine card for connecting a logic analyzer to debug the Rad Hard QDR®-II+ Synchronous SRAM interface to the CYDK-QDRII-NODT. This logic analyzer card has been developed to work with the Infineon CYDK-QDRII-NODT mezzanine card to provide a path to debug the interface between the FPGA and Rad Hard QDR®-II+ Synchronous SRAM. The board is developed and tested to work with FPGA carrier cards through the FMC-HPC connector.
CYDK-NOR - Memories - On request
NOR Flash Boot Configuration mezzanine card for NOR Flash used as FPGA configuration memory. This devkit board has been developed to work with the Infineon Radiation Tolerant 256Mb and 512 Mb NOR Flash memory devices. The board is developed and tested to work with Xilinx FPGA carrier cards through the FMC-HPC connector.
IFXDK-RHNOR - Memories - On request
NOR Flash mezzanine cards have been developed to work with the Alpha Data development kits that support the AMD-Xilinx space grade FPGAs. We offer 2 mezzanine card options for the CYRS17B512 and CYRS17B01G families, one for the 68-pin CQFP package and one for the 100- pin CQFP package. The card has been tested to work with the Xilinx FPGA carrier cards through the FMC-HP connector.
Alpha Data’s boot configuration card is a plug in RH NOR Flash memory module for the ADM-VA601 and ADM-VB630. This card is fitted with Infineon’s 1 Gbit Rad Hard NOR Flash.
Please contact our IR HiRel Representative Office
Supported DevKits:
Xilinx FPGA Boot Configuration Support
The QSPI and Dual QSPI NOR Flash memory devices can be programmed either through the FPGA or directly with an external SPI programmer. Details can be found in the Application Note below:
Infineon works with leading ecosystem and chipset vendors worldwide that are comprised of a network of highly qualified and experienced companies such as AMD Xilinx, Microchip and Alpha Data. Our partners are dedicated to designing and delivering exceptional products and solutions for the Space sector. Many also design and produce reference designs which gives you access to turnkey system solutions that give you a head start in your development.
At Infineon, our global ecosystems are the core of our partner program, comprised of highly qualified and experienced companies that are dedicated to designing and delivering exception products and solutions for the Space sector.
Most system designers choose a chipset before selecting a memory device. If this is the case, locate your vendor of choice in the table of chipset pairing charts. Determine which interface or memory type you need, and open the appropriate spreadsheet. In the spreadsheet, locate your specific chipset and select from the list of qualified memories. If you are in an exploratory phase of your design, chipset pairing charts are also a great way of finding the best Infineon solution(s) for your potential chipset choice, and for fine-tuning the selection of memory interface, voltage, density, etc.
Do you have a question about pairing Infineon memory with a particular chipset, whether or not referenced on our site? Do you have a more generic question about Infineon memory support with a given chipset partner? Are you a chipset partner and want to work with us? Please get in touch!
Supported Space FPGA’s
- Xilinx V5SiRF
- Xilinx Kintex KU060
- MicroChip RTG4
- MicroChip PolarFire
- AMD Versal
- Alpha Data Versal
DevKit Mezzanine Cards
CYDK-QDRII-NODT - Memories - On request
QDR-II+ Synchronous SRAM mezzanine card for testing the highest performing memory for space applications This devkit board has been developed to work with the Infineon Rad Hard 72 & 144-Mbit QDR®-II+ Synchronous SRAMs. The board is developed and tested to work with FPGA carrier cards through the FMC-HPC connector.
CYDK-QDRII-LA - Memories - On request
QDR-II+ Synchronous SRAM Logic Analyzer mezzanine card for connecting a logic analyzer to debug the Rad Hard QDR®-II+ Synchronous SRAM interface to the CYDK-QDRII-NODT. This logic analyzer card has been developed to work with the Infineon CYDK-QDRII-NODT mezzanine card to provide a path to debug the interface between the FPGA and Rad Hard QDR®-II+ Synchronous SRAM. The board is developed and tested to work with FPGA carrier cards through the FMC-HPC connector.
CYDK-NOR - Memories - On request
NOR Flash Boot Configuration mezzanine card for NOR Flash used as FPGA configuration memory. This devkit board has been developed to work with the Infineon Radiation Tolerant 256Mb and 512 Mb NOR Flash memory devices. The board is developed and tested to work with Xilinx FPGA carrier cards through the FMC-HPC connector.
IFXDK-RHNOR - Memories - On request
NOR Flash mezzanine cards have been developed to work with the Alpha Data development kits that support the AMD-Xilinx space grade FPGAs. We offer 2 mezzanine card options for the CYRS17B512 and CYRS17B01G families, one for the 68-pin CQFP package and one for the 100- pin CQFP package. The card has been tested to work with the Xilinx FPGA carrier cards through the FMC-HP connector.
Alpha Data’s boot configuration card is a plug in RH NOR Flash memory module for the ADM-VA601 and ADM-VB630. This card is fitted with Infineon’s 1 Gbit Rad Hard NOR Flash.
Please contact our IR HiRel Representative Office
Supported DevKits:
Xilinx FPGA Boot Configuration Support
The QSPI and Dual QSPI NOR Flash memory devices can be programmed either through the FPGA or directly with an external SPI programmer. Details can be found in the Application Note below: