Oct 21, 2026
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
Oct 21, 2026
FMx Softune IDE
SOFTUNE: Streamlining Program Development with Effortless Integration and Efficiency
-
On this page
Browse by category
RealOS™ Real-Time Operating System
Experience Real-Time Efficiency: RealOS™ Now Available for FR 60 Microcontroller-Series on Infineon's Softune IDE!
Softune IDE Language tools
SOFTUNE C/C++ Compilers (V3 & V6) - Unleashing Advanced ANSI-Compliant Code Optimization for Embedded Systems
Softune Workbench
SOFTUNE Workbench: Microcontroller Programming Support
Tool Lineup for F2MC-16 Family SOFTUNE V3
SOFTUNE Professional Pack for FR Family and F2MC-16/F2MC-8FX Families.
Tool Lineup for F2MC-8FX Family SOFTUNE V3
SOFTUNE Professional Pack for seamless Windows 7, 8, and 10 support across F2MC-8FX Families.
Tool Lineup for FR Family SOFTUNE V6
SOFTUNE Professional Pack for seamless Windows 7, 8, and 10.
Virtual Starter Kit
The Virtual Starter Kit offers a simulation environment for FM microcontrollers, aiding software development without an evaluation board
Windows 10 operation of released SOFTUNE product
Infineon's SOFTUNE IDE: Windows 10 Compatible for Microcontroller Development
Windows 7 operation of released SOFTUNE product
Seamless Microcontroller Development with SOFTUNE IDE
Windows 8 operation of released SOFTUNE product
Infineon SOFTUNE IDE: Windows 8 & 10 for Microcontroller Dev
About
SOFTUNE is an integrated development environment that was designed to respond to the various demands of program developers and pursues ease of use.
Program development requires repeated editing, make/build, and debugging operations.
SOFTUNE is designed to perform such repetitive processes smoothly and efficiently.
- WORKBENCH
Unification of manager section and debugger section
Errors that are found can be fixed on the spot, and the result can be debugged immediately. Three types of debugger functions are supported that need to be used at various different stages of the development cycle.
- Simulator
- Emulator
- Monitor debugger
- Language tools
- C/C++ compiler
When a source file represented in C or C++ language is described, the C/C++ compiler generates an assembler source file which is expressed in assembly language.
- Assembler
This Assembler assembles the source programs described with an assembly language.
- Linkage kit
The linkage kit consists of a linker that is used to connect object modules, a librarian that is used to control object modules and a converter that converts to object type in order to write information on a ROM.
Please contact Local sales or raise a technical support case to receive the download link for SOFTUNE IDE
- F2MC is a trademark of Infineon Technologies AG.
- REALOS and SOFTUNE are trademarks of Infineon Technologies AG.
- TRON is an abbreviation for "The Real-time Operating system Nucleus".
- µITRON is an abbreviation for "Micro Industrial TRON".
- Microsoft, Windows and Windows Media are either registered trademarks of Microsoft Corporation in the United States and/or other countries.
- The company names and brand names herein are the trademarks or registered trademarks of their respective owners.
SOFTUNE is an integrated development environment that was designed to respond to the various demands of program developers and pursues ease of use.
Program development requires repeated editing, make/build, and debugging operations.
SOFTUNE is designed to perform such repetitive processes smoothly and efficiently.
- WORKBENCH
Unification of manager section and debugger section
Errors that are found can be fixed on the spot, and the result can be debugged immediately. Three types of debugger functions are supported that need to be used at various different stages of the development cycle.
- Simulator
- Emulator
- Monitor debugger
- Language tools
- C/C++ compiler
When a source file represented in C or C++ language is described, the C/C++ compiler generates an assembler source file which is expressed in assembly language.
- Assembler
This Assembler assembles the source programs described with an assembly language.
- Linkage kit
The linkage kit consists of a linker that is used to connect object modules, a librarian that is used to control object modules and a converter that converts to object type in order to write information on a ROM.
Please contact Local sales or raise a technical support case to receive the download link for SOFTUNE IDE
- F2MC is a trademark of Infineon Technologies AG.
- REALOS and SOFTUNE are trademarks of Infineon Technologies AG.
- TRON is an abbreviation for "The Real-time Operating system Nucleus".
- µITRON is an abbreviation for "Micro Industrial TRON".
- Microsoft, Windows and Windows Media are either registered trademarks of Microsoft Corporation in the United States and/or other countries.
- The company names and brand names herein are the trademarks or registered trademarks of their respective owners.