For more secure AI and ML models: Infineon’s OPTIGA™ Trust M backs Thistle Technologies’ Secure Edge AI solution

Technology news

Sep 22, 2025

Munich, Germany, and Amsterdam, The Netherlands – 22 September 2025 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) provides its OPTIGA™ Trust M security solution to Thistle Technologies for its new cryptographic protection for on-device AI models to its security software platform for embedded computing products based on the Linux® operating system (OS) or on a microcontroller. The new capabilities in the Thistle Security Platform for Devices, along with Infineon OPTIGA Trust M security solution as tamper-resistant hardware-based root-of-trust, protect the valuable intellectual property (IP) in the AI models deployed in edge AI applications, and in the training data sets on which they are based. 

The Thistle Security Platform for Devices that includes the Infineon OPTIGA Trust M security solution, provides ready-made, cloud-managed security components which integrate seamlessly into Linux OS-based devices and microcontrollers. Instead of building and maintaining a one-off cybersecurity stack, OEMs can deploy a proven, continuously updated foundation in hours, and scale it across large, heterogeneous fleets of devices. The Security Platform enables both secured boot and over-the-air (OTA) updating, and is compatible with a broad range of microprocessors, systems-on-chip (SoCs) and microcontrollers. Infineon OPTIGA Trust M security controller enables secured key provisioning, tamper-resistant key storage, and efficient cryptographic operations for encryption and decryption, taking care that only trusted, authenticated, and verified AI models are deployed in edge AI applications.

Thistle has extended its solution to include built-in protection for on-device AI models and data, using cryptographic keys stored in Infineon's tamper-resistant security controllers, OPTIGA Trust M. The three key features of the new Thistle Secure Edge AI solution are:

  • Hardware-backed model encryption – AI model encryption key is secured by OPTIGA Trust M security solution. Each device has a unique AES 256-bit key securely stored in OPTIGA Trust M, which is used to secure the AI Model encryption key. This means that the AES key is used for encryption and decryption inside the OPTIGA Trust M only. Even if a device is lost, decommissioned, or disassembled, the manufacturer’s IP embedded in the model is still efficiently protected. At launch, this feature is enabled on the Infineon OPTIGA Trust M security solution.
  • Secured model provenance – in OTA updates, the Thistle platform enables cryptographically signed, tamper-evident delivery of AI models and firmware directly from the training platform to the device, taking care that every installed instance of a model can be traced and verified.
  • Signed data and data lineage - device-generated or collected data can be signed on-device and tagged with provenance metadata. This means that downstream systems which might use the data to train or refine AI models can check the provenance of the data, and of the version of the model that the device was running when it generated the data. 

Animesh Ranjan, Head of Partnerships & Ecosystem at Infineon says: “At Infineon, we are pleased to expand our collaboration with Thistle Technologies to deliver stronger protection for AI models running at the edge. By combining the OPTIGA Trust M security solution with the Thistle Security Platform, we enable device makers to safeguard their AI with hardware-anchored security that is both practical and scalable.”

Window Snyder, Chief Executive Officer of Thistle Technologies, says: “It is always our goal to make robust security capabilities accessible for device makers. With Infineon’s OPTIGA Trust M and the Thistle Security Platform, manufacturers can protect AI models and data with proven cryptography and deploy at scale quickly. Together we give customers a straightforward way to ship devices that can securely verify, encrypt, and update AI models."

The new Secure Edge AI solution, part of the Thistle Security Platform for Devices backed by Infineon OPTIGA Trust M as hardware-based root-of-trust, is available now. 

More information about Infineon OPTIGA Trust M can be found at https://www.infineon.com/OPTIGA-TRUST-M. Embedded device developers who want a demonstration of the Secure Edge AI Solution can contact Thistle Technologies. 

Visitors to The Things Conference and exhibition (Amsterdam, The Netherlands, 23-24 September 2025) can see a demonstration of these new capabilities at the Thistle Technologies booth B6. 

About Thistle Technologies

Thistle Technologies supplies a set of security tools and services for embedded devices that allows teams to address major areas of security risk immediately. Embedded and IoT devices rarely have the security mitigations that are present in general-purpose operating systems. The modern Thistle Technologies security platform for devices meets the need for comprehensive security protection in an easy-to-use format compatible with the microprocessor and microcontroller platforms in widespread use in embedded devices

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Follow us: Facebook - LinkedIn

Press Photos

Infineon Thistle Secure Edge AI

Infineon Thistle Secure Edge AI

Infineon’s OPTIGA™ Trust M backs Thistle Technologies’ Secure Edge AI solution

JPEG

2000x1125 px

Download
Logo Thistle Technologies

Logo Thistle Technologies

Infineon’s OPTIGA™ Trust M backs Thistle Technologies’ Secure Edge AI solution

JPEG

1400x590 px

Download

Information Number : INFCSS202509-147

avatar

Ulrike Mittereder

Spokesperson Edge Systems Division (ES)

+49 89 234 43951

Send email