Infineon achieves ISO/SAE 21434 certification for SLI37 automotive security controllers
Infineon achieves ISO/SAE 21434 certification for SLI37 automotive security controllers
Technology news
Munich, Germany – 30 January 2024 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is the first company in the industry to receive the ISO/SAE 21434 cybersecurity certification for its SLI37 automotive security controller family. This enables a high level of security with ISO/SAE-compliant products and will facilitate customer integration into automotive applications such as secured devices for V2X (Vehicle-to-everything) communication. It follows the certification of Infineon’s cybersecurity management system, which was announced in November 2022.
“At Infineon, we are constantly improving our security offering,” said Sebastien Colle, Vice President 'Security' at Infineon. “We enable our customers to easily demonstrate their compliance with ISO/SAE 21434. I am particularly proud that the Common Criteria certification has been used as a bridge to demonstrate compliance with ISO/SAE 21434. This is a testament to the power of Common Criteria as a generic tool that can serve application verticals. With the combination of ISO/SAE 21434 and CC EAL6+ (high) certificates, Infineon’s SLI37 controllers provide the best benchmark for security verification in the automotive world today.”
The hardware-based security features of ISO/SAE 21434 certified devices can provide a reliable foundation for a multi-layered security architecture, enabling a root-of-trust. This plays an important role in the automotive industry, where system security is mandatory for vehicle safety. Therefore, Infineon’s SLI37 automotive cybersecurity solutions provide a secured foundation for automotive applications to comply with the ISO/SAE 21434 standard.
As part of the certification process, a security evaluation was conducted by TÜV-IT GmbH, an accredited and independent security evaluator, which concluded that the products have demonstrated resistance to attackers with high attack potential. This also includes protection against physical attacks such as fault and spike attacks, as well as power and side channel analysis.
Availability
Infineon's SLI37 automotive security controller can be ordered. More information is available at www.infineon.com/automotive-security-controllers.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
SLI37 VQFN-32-13
Infineon’s SLI37 automotive security controllers are now ISO/SAE 21434 certified.
JPEG
2126x1453 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFCSS202401-053