- Consumer Wearables
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
- Domestic robots
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
- AMD CPU voltage regulator Ics
- Ampere CPU voltage regulator Ics
- Intel CPU voltage regulator Ics
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
Sep 29, 2026
Business & Financial Press
Sep 23, 2026
Business & Financial Press
Sep 16, 2026
Business & Financial Press
Sep 09, 2026
- Company
- Our stories
- Events
- Press
- Investor
- Careers
- Quality
- Latest news
Business & Financial Press
Sep 29, 2026
Business & Financial Press
Sep 23, 2026
Business & Financial Press
Sep 16, 2026
Business & Financial Press
Sep 09, 2026
EconoDUAL™ 3 modules with TRENCHSTOP™ 1700 V IGBT7 enable highest power densities
EconoDUAL™ 3 modules with TRENCHSTOP™ 1700 V IGBT7 enable highest power densities
Technology news
Munich, Germany – 6 May, 2022 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today launched the new TRENCHSTOP™ 1700 V IGBT7 chip in the standard industrial package EconoDUAL™ 3. With this new chip technology, the EconoDUAL 3 provides a leading current of 900 A and 750 A, and enables an improved power range for inverters. The modules target a wide range of applications including wind, drive and static VAR generators (SVG).
Compared to modules with the previous IGBT4 chipset, the FF900R17ME7_B11 with the TRENCHSTOP IGBT7 chip enables up to 40 percent higher inverter output current in the same package size. The new 1700 V IGBT7 modules also feature significantly lower static and dynamic losses while addressing applications with prevailing static losses in diode chips. In addition, the new chip technology offers enhanced du/dt controllability and improved diode softness. Induced by cosmic rays, the FIT rate has also been significantly improved – an important parameter when working with high DC link voltage. Furthermore, the new power modules feature a maximum overload junction temperature of 175°C.
In addition to the best-in-class 1700 V EconoDUAL 3 with 900 A, a 750 A module with a larger diode has also been introduced to further increase the flexibility of the new portfolio. Overall, the new EconoDUAL 3 1700 V modules with the TRENCHSTOP IGBT 7 chip can increase the power density of the inverter and achieve a new level of performance in a wide range of applications.
Availability
The FF900R17ME7_B11, FF750R17ME7D_B11 and FF225R17ME7_B11 can be ordered now. The roll-out of the portfolio, specifically the current classes from 300 A to 750 A, will follow at the end of 2022. More information is available at www.infineon.com/econodual3.
During PCIM 2022, a paper presentation will be held on 10 th of May (2.00 PM CEST, conference area, room München 2) by Aleksei Gurvich, Senior Manager of Product Definition & Application Engineering, about the new 900 A and 750 A 1700 V EconoDUAL 3 Modules with TRENCHSTOP IGBT7.
Infineon at PCIM 2022
At PCIM 2022, Infineon will be presenting innovative product-to-system solutions for applications that are set to power the world and shape the future. Company representatives are also holding several presentations at the PCIM Conference and Industry & E-Mobility Forum with live and on-demand video presentations, followed by discussions with the speakers. “Experience the difference in power” at Infineon’s booth #412 in hall 7 (10-12 May 2022, Nuremberg/Germany).
More information about Infineon’s contribution to energy efficiency: www.infineon.com/green-energy
Press Photos
EconoDUAL™ 3 with TRENCHSTOP™ 1700 V IGBT7
With the new TRENCHSTOP™ 1700 V IGBT7 chip technology, Infineon’s EconoDUAL™ 3 provides a leading current of 900 A and 750 A, and enables an improved power range for inverters. The modules also feature significantly lower static and dynamic losses while addressing applications with prevailing static losses in diode chips. In addition, the new chip technology offers enhanced du/dt controllability and improved diode softness. Induced by cosmic rays, the FIT rate has also been significantly improved – an important parameter when working with high DC link voltage.
JPEG
2126x1555 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFIPC202205-077