Every new generation of AI processors demands dramatically more current — and delivering it reliably is becoming one of the hardest problems in the data center.

This page explains the "last inch" of power delivery: the final conversion stage that feeds that current from the board directly to the GPU or accelerator core, and why it's pushing power per GPU server past 100 kW in the process.

The numbers tell the story on their own. A traditional server processor drew under 200 A of thermal design current; as AI-optimized chips emerged, that core-rail current doubled to around 400 A, then doubled again to roughly 800 A within a few years — and today's leading AI accelerators push well past 1,000 A each, with 2,000 A-class designs already on the horizon, several times what a single CPU in a general-purpose server would ever draw.

At the same time, vendors have integrated the coprocessor and memory — using high-bandwidth memory as GPU memory instead of separate modules — directly onto the core silicon, concentrating all that current, and the heat it generates, into a smaller area than ever before.

Modern GPUs and dedicated AI processors like Tensor Processing Units (TPUs) increasingly combine two or more dies into a single package to pack in more transistors than any one manufacturing node allows — the same parallel-core architecture that makes them the compute engine of choice for deep learning algorithms and other demanding HPC workloads.

But the industry-standard OAM (OCP Accelerator Module) form factor was sized for chips far smaller than today's accelerators, which can now approach the module's own footprint — leaving little board area for the power components that have to feed it. That's the core of the "last inch" challenge: delivering thousands of amperes the final, short distance from board to processor, in a space that keeps shrinking.

For how this processor-level challenge connects to rack- and facility-level power architecture, see AI and hyperscale growth: how they are reshaping data center power architecture.

Data center operators want to pack more and more GPUs into the same rack space — the data center power density problem in its most concentrated form: inside a single GPU server, each GPU needs its own high-current power delivery, multiplying both compute density and current density within the same shrinking footprint.

Power used to enter the processor from just one side of the board, with the other three reserved for signal and memory. Past roughly 200 A, single-sided entry became impractical due to resistive losses — pushing the industry first to double-sided, then multi-sided, power entry, sourcing current from as many edges of the processor as possible.

That approach has a ceiling: a processor only has four sides, and packing more power phases around that perimeter eventually increases resistance again, as high currents entering from the back have to route around the phases in front of them.

Crowding power delivery into a package already dense with connectors and high-speed signal traces also creates signal-integrity problems, since power planes are electrically noisy neighbors for sensitive data lines. Lateral power delivery runs out of usable space well before it runs out of current demand — which is exactly why high density data centers built around dense GPU clusters are moving to vertical power delivery.

Every stage a current passes through on its way to the processor — bus bars, connectors, power stages, inductors — adds resistive loss, and these power delivery network (PDN) losses don't scale linearly with load; they compound as current climbs into the thousands of amperes. For a 2,000 A processor sourcing all its current laterally from two sides of the package, PDN losses can reach around 180 W — over 10% of the processor's total power loss. Sourcing that same current vertically from underneath instead cuts PDN losses by roughly 70%, to about 50 W, or just over 3% of total losses.

At the scale of a large GPU data center — often 100,000 processors or more — saving just over 100 W per processor adds up to megawatts saved across the facility, and millions of dollars over its lifetime. PDN losses ultimately show up as heat on an already thermally constrained rack, on top of the heat the processor itself generates — so reducing them isn't just an efficiency exercise, it directly affects total cost of ownership.

Trend toward vertical power delivery — compares lateral vs. vertical power delivery paths from a 48 V bus down to the GPU/ASIC.

This is precisely why the industry is moving toward vertical, backside-mounted power modules: shortening the current path and integrating chip sets and inductors more tightly reduces both resistive losses and the physical space the PDN needs, directly cutting the heat waste that scales with load.

See Infineon's vertical power module portfolio, designed specifically to cut PDN losses at high-current GPU rails

Power can reach the processor three ways: lateral (discrete power stages beside the processor, on the same plane), vertical (through the motherboard to backside-mounted modules), or hybrid (a mix of both, often as a transitional step).

All three have to coexist with PCIe and other high-speed interconnects on the same board, since GPU servers need both power and data to reach the processor without interfering with each other.

As GPU acceleration becomes central to high performance computing — spanning AI training, scientific computing, and other performance-hungry workloads once handled by racks of general-purpose CPUs — the board-level power architecture has to keep pace with compute density rather than lag behind it.

The same trend is playing out one level up too: as rack power climbs, facilities are shifting from traditional 48 V architectures to HVDC distribution.

This shift has direct implications for facility-level efficiency and grid demand — see Data center energy consumption: scale, trends, and efficiency pressures.

At 2,000 A and beyond, vertical power delivery isn't just the better option — it's becoming the only practical one.

Feeding power through the motherboard to backside-mounted modules positioned directly under the processor shortens the current path by roughly 30 times compared to routing it laterally across the package, while freeing up the board space AI accelerators need for compute.

That's why vertical power delivery is increasingly the default architecture for next-generation AI processors, not one option among several — a response to physics, not a design preference.

As racks pool ever more GPU resources into a single cluster, an architecture ideal for AI accelerators has to deliver both raw GPU performance and stable power to increasingly powerful GPUs at the same time.

Voltage Regulator Modules (VRMs) step power down from an intermediate bus — typically 12 V — to the sub-1 V level the processor core actually needs, and they have to do it at extremely high currents with fast transient response.

Discrete solutions, built from separate power stages and inductors, were the traditional approach, but at today's current levels they struggle with both space and losses.

Integrating the inductor, capacitors, and power stages of a multiphase design onto a single substrate — a power module — can shrink a voltage regulator's footprint by around 40% compared to an equivalent discrete solution, while also improving signal integrity: the module isolates the switch node from the motherboard, keeping switching noise away from sensitive high-speed signals nearby.

This roadmap toward higher-density, better-integrated VRM modules is a key enabler for keeping pace with rising per-processor current requirements without redesigning the motherboard from scratch each generation.

Explore Infineon's VRM and power module portfolio and DC-DC converter solutions for high-current AI voltage regulation

Vertical power modules come in a few main mounting configurations:

  • Laterally mounted modules sit beside the processor on the same plane — the traditional approach, simpler to implement but limited by available board area.
  • Vertically mounted modules are placed on the backside of the motherboard, delivering power straight through to the processor and freeing up front-side space for compute and interconnect.
  • Substrate-integrated modules go a step further, embedding the power conversion components directly into the package substrate for the shortest possible current path and the highest power density.

Each step in this progression trades some manufacturing complexity for a shorter, lower-loss path from the bus to the core — which is exactly what's needed as per-processor current keeps climbing toward and beyond the 2,000 A range.

As AI processors continue to demand higher current in ever-smaller footprints, the evolution from lateral to vertical and substrate-integrated power delivery is expected to become the defining direction for next-generation accelerator design.

See Infineon's AI accelerator card solutions, covering the full range of module types from laterally mounted to substrate-integrated →

Recommended documents

What is a GPU?

A GPU (Graphics Processing Unit) is a processor originally designed for rendering graphics, built around thousands of small cores that use parallel processing to perform many calculations at once.

That same architecture makes GPUs extremely well suited to the matrix and vector math behind AI model training and inference — and clustering multiple GPUs into a single GPU server is what turns that raw compute capability into the primary compute engine in modern AI data centers.

PDN (Power Delivery Network) losses are the energy lost as heat while current travels from the board-level power bus to the processor core, through bus bars, connectors, power stages, and inductors. These losses grow disproportionately as current increases, which is why they become a major concern at the multi-thousand-ampere current levels modern AI processors require.

"Last-inch power delivery" refers to the final, short stage of the power conversion chain — getting power the last physical distance from the board or package directly to the processor die. It's considered one of the hardest engineering challenges in AI hardware because it has to deliver extremely high current with very tight tolerances, in an extremely small space, right next to the hottest and most sensitive part of the system.

Lateral power delivery places power components beside the processor on the same plane; vertical power delivery routes power through the motherboard to modules mounted on the processor's backside, directly beneath it. Vertical power delivery is increasingly seen as the better approach for high-current AI processors, since it shortens the current path and frees up board space that lateral designs can no longer spare — though lateral and hybrid approaches still have a role at lower current levels.

A VRM (Voltage Regulator Module) is a component that steps down power from an intermediate bus voltage — typically 12 V — to the much lower voltage (often under 1 V) that a processor core actually needs, while supplying very high current with fast response to sudden load changes. Modules integrate the inductor, capacitors, and power stage into a single package, offering better space efficiency and signal integrity than older discrete designs built from separate components.

Current requirements have grown rapidly: traditional server processors drew under 200 A, while today's leading AI accelerators are pushing past 1,000 A each, with 2,000 A-class designs already emerging. This trajectory is the single biggest reason the industry is moving away from lateral power delivery and discrete components toward vertical, integrated power modules.