- Smart TV
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
Nov 17, 2026
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
Nov 17, 2026
Business & Financial Press
Nov 11, 2026
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
Data center power architecture is being rebuilt from the ground up. As AI workloads and hyperscale build-out drive rack power from kilowatts toward megawatts, the 48 V, single-phase infrastructure that powered the last two decades of data centers is running out of road — forcing a shift toward high-voltage DC and disaggregated rack designs inside every AI data center.
This page explains how that architectural shift is unfolding, from the processor core to the facility, and what it means for anyone designing, building, or operating a data center for AI workloads today.
Training large AI models means clustering as many as 100,000 processors into what effectively behaves as a single virtual machine. Every Graphics Processing Unit (GPU) or dedicated AI processor — such as a Tensor Processing Unit (TPU) — has to be kept synchronized with every other GPU in the cluster, exchanging data at extremely high speed over dense copper interconnects within the rack, a network performance requirement non-AI workloads never had to meet.
Traditional, non-AI compute workloads simply don't demand this kind of tightly coupled, always-on parallel operation, and the underlying hardware has to keep pace accordingly.
This kind of clustering is what turns a facility into a true GPU data center, purpose-built to run these tightly coupled workloads — a defining trait of modern AI data centers.
The processors themselves are also built differently. To pack more transistors onto a single die, AI processors increasingly combine two or more silicon dies into one package, pushing chip sizes — and their appetite for current — far beyond what conventional CPUs require. The result is a workload profile that is not just "more compute," but a fundamentally different electrical load: higher currents, sharper transient steps, and far less tolerance for voltage droop.
More compute, more transistors, more current — the chain from AI workload to power infrastructure is direct. As AI processors grow larger and their supply voltage keeps dropping toward roughly 0.4 V, the current needed to deliver the same power rises sharply. Industry projections point to individual processors in AI data centers drawing up to 10,000 amperes within this decade — a tenfold increase over today's requirements, building on accelerators that are already pushing past 2,000 A.
That current has to be delivered from a 12 V (or similar) intermediate bus all the way to the processor core, and every step in that path — from the motherboard to the voltage regulator to the die itself — has to be re-engineered to carry it efficiently.
This is why compute demand doesn't just mean "bigger power supplies" somewhere in the building; it directly drives AI data center power consumption at every level, cascading all the way down to how power physically reaches the silicon.
As individual processor current continues to increase, the cumulative effect across dozens of AI accelerators packed into a single rack fundamentally changes rack-level power requirements — turning a processor-level trend into a facility-level one.
The shift has happened at every level of the data center simultaneously. At the rack level, power has moved from roughly 100 kW to more than 1 MW as operators pack up to 72 AI server blades into a single rack.
At the facility level, newly built AI data centers already draw several hundred megawatts, and dedicated "AI factories" are now being planned or announced at gigawatt — and even multi-gigawatt — scale by major tech companies operating hyperscale infrastructure. This growing AI data center energy consumption is why utilities and regulators are paying closer attention to where new sites are built.
This growth shows no sign of leveling off. As long as AI model sizes and training clusters keep expanding, power demand at the processor, rack, and facility level is expected to keep climbing well beyond current levels, making power infrastructure — not just compute silicon — one of the defining bottlenecks of AI scaling.
This rapid increase makes efficiency and power density central design challenges throughout the entire power chain, from the processor core to the facility's incoming grid connection.
For a closer look at what this growth means for global electricity demand, grid strain, and efficiency targets, see Data center energy consumption: scale, trends, and efficiency pressures.
At the rack level, the classic layout of IT trays is giving way to disaggregated blade-server racks, where power supplies, battery back-up, and capacitor buffering are moved into adjacent side-cars so the main rack can focus purely on compute and interconnect.
Power delivery within these racks is also shifting from single-phase to three-phase supplies as rack power climbs toward and beyond 1 MW in modern AI data centers.
Disaggregated IT rack — illustrates the shift from a classic IT tray rack to a disaggregated blade-server rack with a dedicated power side-car (PSU/BBU/PCS), scaling from <160 kW to 600 kW+ per rack.
Higher rack power makes conventional low-voltage distribution increasingly impractical, because current rises proportionally with power at a fixed voltage — at megawatt-plus rack levels, staying on a low-voltage bus would mean bus bars carrying thousands of amperes.
At the facility level, the well-established 48 V bus architecture is being replaced by high-voltage DC — typically 800 V or ±400 V — once racks cross into the 200–250 kW range, since the alternative would mean impractically high currents in the bus bars.
Looking further out, the industry is moving toward central power generation and distribution as high-voltage DC microgrids, cutting out redundant conversion steps and creating a scalable architecture for the gigawatt-scale data centers of the future.
This shift is prompting data center operators to move away from retrofitting legacy architectures, and toward power solutions purpose-built for AI from the ground up.
AI data center today → immediate power increase → future-proof DC microgrid" — three-step visual of the architectural shift from single-phase AC power shelves to HVDC-to-rack to a DC microgrid with solid-state transformer.
Explore Infineon's data center power distribution solutions for the transition from 48 V to 800 V / ±400 V HVDC architectures
Once racks approach and exceed a megawatt, physical space becomes just as limiting a factor as electrical capacity. Every part of the power conversion chain — from the incoming AC feed down to the sub-1 V rail at the processor core — has to fit into a shrinking footprint while carrying dramatically more current.
That's why power density (how much power a converter can handle per unit of volume or board area) has become as important a design metric as raw efficiency, especially as facilities evolve into high-performance computing environments built specifically for AI.
Efficiency itself is no longer just a cost consideration; at gigawatt-scale power draw, even fractional efficiency losses translate into enormous amounts of wasted energy and heat that has to be removed through cooling.
Higher efficiency and higher power density go hand in hand: they reduce operating expenditure, ease thermal design, and free up rack space for more compute — all while keeping the escalating power demand of AI within reach of what utility grids and facilities can realistically deliver.
In practice, power delivery has become inseparable from overall data center performance: a facility that can't feed its racks enough clean, stable power can't run at its intended compute capacity, no matter how capable the processors inside it are.
These pressures are most extreme right at the processor: see GPU servers and AI compute: the last-inch power delivery challenge for how power density and efficiency play out at the core.
The architectural shift already underway — HVDC, disaggregated racks, DC microgrids — is only part of the answer.
As hyperscalers race to keep pace with AI ambitions and roll out ever more capable AI tools, the energy supply feeding that infrastructure has to adapt just as fast: facility-level Battery Energy Storage Systems (BESS) help buffer the highly variable load patterns created by large GPU clusters during training, smoothing demand on the grid.
And because AI is becoming one of the fastest-growing drivers of global electricity demand, data centers are also under pressure to source that growing energy budget sustainably — integrating renewables, power purchase agreements, and in some cases nuclear power, rather than relying solely on fossil fuels.
Explore Infineon's solid-state transformer and solid-state circuit breaker portfolio, key building blocks for DC microgrid architectures
DC microgrid as the central infrastructure of a GW-scale data center (source: Infineon whitepaper "The Future of Powering AI," Figure 17, p. 19) — shows how a DC microgrid fed from the MV AC grid, coupled to renewables, batteries (BESS) and IT racks, reduces conversion losses across the whole facility.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
What is hyperscale and what are hyperscalers?
Hyperscale refers to computing infrastructure built to scale rapidly and massively — typically tens or hundreds of thousands of servers across a network of data centers.
Hyperscalers are the companies that operate this infrastructure at that scale, primarily the large cloud and technology providers running AI training and inference workloads, cloud services, and global online platforms, whether within a single artificial intelligence data center or across a global network of them.
What is rack power density and why does it matter?
Rack power density is the amount of power (and corresponding heat) concentrated within a single server rack, typically measured in kilowatts per rack. It matters because higher density means more compute in the same physical footprint — but it also means more current has to be delivered, and more heat has to be removed, within that same limited space.
As AI racks move from around 100 kW to more than 1 MW, power density becomes one of the central constraints on data center design.
What is driving the rapid increase in data center power demand?
The main driver is AI compute itself: training and running large AI models requires clustering tens of thousands of power-hungry processors, each drawing significantly more current than a conventional server chip. This is compounded by the broader trend of hyperscale build-out, as cloud providers and AI companies construct ever-larger, purpose-built "AI factories" to keep up with demand for AI services.
Are current power infrastructures sufficient for AI-driven data centers?
Largely, no — not without significant redesign. Established infrastructure built around 48 V bus architectures and single-phase power distribution was designed for a previous generation of compute density. AI-driven power demand is pushing racks and facilities well beyond what these architectures can efficiently support, which is why the industry is transitioning toward high-voltage DC distribution, three-phase power supplies, and eventually DC microgrids.
What role do semiconductors play in improving power efficiency and density?
Largely, no — not without significant redesign. Established infrastructure built around 48 V bus architectures and single-phase power distribution was designed for a previous generation of compute density. AI-driven power demand is pushing racks and facilities well beyond what these architectures can efficiently support, which is why the industry is transitioning toward high-voltage DC distribution, three-phase power supplies, and eventually DC microgrids.