- Smart TV
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
Nov 17, 2026
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
Nov 17, 2026
Business & Financial Press
Nov 11, 2026
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
Data center electricity consumption is exploding — and AI is the single biggest reason why. This page covers the scale of that growth, from small local facilities to gigawatt-scale AI factories, the drivers behind it, and the regulatory and market pressure it's putting on operators to improve efficiency.
Data centers currently account for roughly 2% of global electricity consumption — a figure expected to rise to around 7% by 2030 as artificial intelligence (AI) adoption accelerates.
Much of that growth traces directly back to the chips themselves: every 1 million next-generation GPUs deployed today draws around 0.7 GW, comparable to the output of two mid-size coal-fired power plants, and as equipment power draw across servers keeps climbing, industry-wide GPU shipment volumes are rising fast enough that cumulative demand could soon require the equivalent of more than a dozen additional power plants just to keep up.
It's a clear sign of just how much electricity this sector already consumes to meet growing service demand for AI-powered applications.
A key metric here is Power Usage Effectiveness (PUE) — the ratio of total facility power to the power actually delivered to IT equipment, including servers, storage, and networking equipment. As AI drives up both the density and the intensity of compute, keeping PUE low becomes harder and more important at the same time, since every fraction of overhead multiplies quickly at gigawatt scale. The average data center today still operates well above the theoretical ideal of a PUE of 1.0, leaving significant room for improvement as data center energy needs continue to climb.
As electricity demand grows at this pace, the challenge extends well beyond individual facilities, adding to total electricity demand and increasingly affecting the regional power grid as a whole.
For why individual GPUs are such a big part of this equation, see GPU servers and AI compute: the last-inch power delivery challenge.
In regions where many data centers are geographically clustered, energy supply is already under strain. Research from organizations like the Electric Power Research Institute is helping quantify just how fast annual electricity demand from this sector is rising: projections suggest AI data centers could consume up to 16% of total electricity consumption in the U.S. by 2030, and in Ireland — already one of the most data-center-dense countries in the world — that share could reach as high as 32% within the next year or two. This concentration has started to trigger regulatory responses, including rules in some regions that limit further data center expansion until grid capacity catches up.
For operators — especially those running hyperscale data centers — this means that where a new AI data center can be built — and how fast it can grow — is no longer just a question of land and connectivity, but increasingly one of local grid headroom and regulatory approval.
This is one of the forces pushing operators toward the architectural changes covered in AI and hyperscale growth: how they are reshaping data center power architecture.
According to the International Energy Agency, AI is one of the three biggest drivers of global electricity demand growth over the next decade — alongside rising air-conditioning use from warmer climates and the electrification of transportation. Together, these forces are expected to push electricity demand growth roughly six times higher than it would otherwise be.
At that scale, efficiency stops being a nice-to-have and becomes a hard constraint. In a typical data center today, around 17% of energy is lost as power delivery network losses across the various conversion steps between the grid and the processor — but state-of-the-art power semiconductor technology can roughly halve that figure to about 9%, lifting overall power flow efficiency from around 83% to as high as 91%.
At gigawatt scale, that difference isn't marginal: it translates into major reductions in wasted energy, heat, cooling demand, and ultimately CO₂ emissions.
Improving efficiency at this scale ultimately comes down to the technologies used throughout the power conversion chain — which is where semiconductors enter the picture.
DC microgrid as the central infrastructure of a GW-scale data center (source: Infineon whitepaper "The Future of Powering AI," Figure 17, p. 19) — shows how a DC microgrid fed from the MV AC grid, coupled to renewables, batteries (BESS) and IT racks, reduces conversion losses across the whole facility.
Much of the efficiency gain in modern data centers comes down to power semiconductor technology.
Wide-bandgap devices — such as silicon carbide (SiC) and gallium nitride (GaN) — switch faster and lose less energy as heat than traditional silicon at the same voltage and current levels, across every stage of the power chain from the grid down to the processor.
Solid-State Transformers (SSTs) are one example of this shift: instead of a traditional, bulky medium-voltage transformer, an SST built from power semiconductors can take power directly from a 10–35 kV AC grid and convert it into regulated high-voltage DC, while being smaller, lighter, and installable closer to the racks it serves — reducing transmission losses along the way. Solid-state circuit breakers, built on similar technology, add fast, reliable protection to these DC architectures.
Explore Infineon's solid-state transformer and solid-state circuit breaker solutions for high-voltage DC data center architectures
Individual technologies like wide-bandgap semiconductors or solid-state transformers only deliver their full benefit when they're combined into a coherent system-level strategy. In practice, that strategy rests on a few consistent levers:
- Optimized power architectures — rethinking the entire energy flow from grid to core rather than optimizing individual components in isolation, so gains at one conversion stage aren't offset by losses at another.
- Advanced packaging techniques — approaches like chip embedding and integrated magnetics that shrink the physical space power components need, improving both thermal performance and efficiency around the semiconductors themselves.
- Smart control and monitoring — intelligent systems that dynamically match power delivery to actual workload demand, directly improving Power Usage Effectiveness (PUE) rather than over-provisioning for worst-case load.
Beyond individual components, some of the biggest gains come from rethinking the overall power distribution architecture. Moving from AC to high-voltage DC distribution removes redundant AC-DC and DC-AC conversion steps throughout the facility, letting racks do simple DC-to-DC conversion only. A DC microgrid architecture takes this further by:
- providing a single, flexible connection point for whatever energy sources a facility adds over time, without a dedicated conversion stage for each one
- scaling IT rack power to meet next-generation GPU demand without being constrained by physical space
- delivering end-to-end efficiency that minimizes both energy delivery waste and the cooling effort needed to remove that waste
- reducing the overall CO₂ footprint of the facility
Facility-level Battery Energy Storage Systems (BESS) add another lever: they buffer the highly variable, bursty load patterns created by large GPU clusters during training, keeping the load the facility presents to the utility grid closer to constant.
Explore Infineon's battery energy storage, photovoltaic, and wind power solutions that support renewable integration at data center scale
Even the most efficient power architecture cannot eliminate the need for enormous amounts of electricity — it can only reduce how much is wasted along the way. That makes the source of that electricity increasingly important for meeting data center energy needs sustainably.
There is no AI without power — and increasingly, that power needs to come from clean energy sources. On a global scale, close to half of data center energy is already attributed to renewables, but as AI drives demand sharply higher, simply maintaining that share won't be enough.
Looking ahead, operators of hyperscale data centers are expected to keep investing in both on-site renewable generation and long-term power purchase agreements (PPAs), with solar, wind, and fuel cells leading the way this decade — a single 1 GW data center, for example, could require a solar farm of roughly 8 km² to supply it.
Nuclear power, including small modular reactors, is also being developed as a steady, carbon-free complement to renewables, though renewables are expected to scale faster in the near term. Non-renewable sources like natural gas will likely continue to play a bridging role, but the clear direction of travel is toward decarbonizing the energy that powers AI.
Explore Infineon's battery energy storage, photovoltaic, and wind power solutions that support renewable integration at data center scale
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Are countries and institutions, e.g. the EU, doing anything to prevent AI data centers from draining the grid?
Yes — several countries and regions have started implementing measures to manage the impact of data centers on local grids, ranging from stricter connection requirements to caps on new data center capacity in areas where total data center electricity use is already straining the grid.
The EU and national governments are also pushing energy efficiency reporting and sustainability requirements as part of broader climate policy, though specific rules vary significantly by country and region.
What is Power Usage Effectiveness (PUE)?
PUE is the ratio of total facility power to the power delivered to IT equipment — the closer to 1.0, the less overhead. Typical data centers today run in the 1.5–2.0 range; best-in-class hyperscale facilities can get closer to 1.1–1.2, though AI's higher cooling and power-density demands make hitting those numbers harder than ever.
How can data centers become more sustainable?
Sustainability comes from a combination of measures: improving power conversion efficiency to reduce waste at every stage, adopting more efficient architectures like high-voltage DC distribution, drawing on renewable energy sources (see below), and using intelligent monitoring to match power delivery to actual demand rather than over-provisioning for worst-case scenarios.
What are renewable energy sources, and how can data centers leverage them?
Renewable energy sources — primarily solar, wind, and in some cases geothermal or fuel cells — generate electricity without depleting finite resources or directly emitting CO₂. Data centers can leverage them either through on-site generation (such as an adjacent solar farm) or through long-term power purchase agreements (PPAs) that secure renewable capacity from the grid, often paired with battery storage to smooth out the variability of renewable generation.
How do battery energy storage systems (BESS) support data center operations?
BESS installations buffer the highly variable, bursty power demand created by large GPU clusters during training, absorbing sudden spikes and smoothing the load the facility presents to the utility grid. They can also provide backup power during outages and help data centers make better use of intermittent renewable generation by storing excess energy for later use.
What are the main challenges in scaling data center power infrastructure for AI?
The core challenges are physical space, current-carrying capacity, and heat: as rack and facility power climb toward gigawatt scale, conventional low-voltage AC infrastructure becomes impractical, requiring a shift to high-voltage DC distribution and eventually DC microgrids. On top of the infrastructure itself, operators also have to secure enough clean, reliable electricity supply and navigate increasingly strict regional regulations on data center growth.