- Smart TV
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
Nov 17, 2026
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
Nov 17, 2026
Business & Financial Press
Nov 11, 2026
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
What Is the Microcontroller Used in Arduino Uno?
The short answer, the chip's limits, and how to choose a modern 32-bit MCU — with Infineon PSOC™ and XMC™ examples.
So, what is the microcontroller used in Arduino Uno? The classic Arduino Uno (Rev3) uses the ATmega328P — an 8-bit AVR microcontroller from Microchip (formerly Atmel), clocked at 16 MHz. The newer Arduino Uno R4 (2023) instead uses a 32-bit Renesas RA4M1 (Arm® Cortex®-M4) at 48 MHz. So which microcontroller is used in Arduino Uno depends on the version: 8-bit on the R3, 32-bit on the R4.
That answer is the starting point, not the destination. If you are choosing a microcontroller for your own project today, the more useful question is how to pick the right one. Infineon's 32-bit Arm® Cortex®-M portfolio spans PSOC™ 4, PSOC™ 6, PSOC™ Control C3, PSOC™ Edge and XMC™ — from low-cost mixed-signal parts to multi-core devices with on-chip AI acceleration. XMC™ and PSOC™ 6 are supported in the Arduino IDE, and evaluation kits across the families offer Arduino-shield-compatible headers, so you can move up from 8-bit without abandoning familiar hardware. The rest of this guide covers the ATmega328P's limits, the criteria that drive an MCU choice, and concrete 32-bit options.
The Arduino Uno's microcontroller is an 8-bit AVR. The classic Uno (Rev3) is built around the ATmega328P: an 8-bit AVR RISC core at 16 MHz with 32 KB of flash, 2 KB of SRAM and 1 KB of EEPROM, plus 23 GPIO, a 6-channel 10-bit ADC and UART/SPI/I²C. It has no floating-point unit and no on-chip USB or wireless — the Uno R3 uses a separate ATmega16U2 for USB-to-serial.
For simple sensing, control and learning projects, the ATmega328P is more than enough and its huge community is a real advantage. The limits show up when a project needs more memory (large buffers, displays, audio), faster math (DSP or floating point), native USB, built-in wireless, or on-device AI. That is where a 32-bit Arm® Cortex®-M microcontroller earns its place — and where the rest of this guide helps you choose one. (The 2023 Uno R4 makes the same jump, moving to a 32-bit Renesas RA4M1.)
If you are picking a microcontroller for a new project, six criteria drive the decision. Use them to decide whether an 8-bit part is enough or a 32-bit Arm® Cortex®-M is the better fit.
List what the project must do: GPIO/analog count, whether it needs wireless (Wi-Fi/Bluetooth® LE), USB or CAN, whether it runs on a battery, and whether any of it involves on-device AI. Note a rough performance and memory need — blinking LEDs vs. running a sensor-fusion loop or a neural network. This list drives every choice below.
In today's market the cost of a 32-bit MCU is typically the same as — and sometimes lower than — legacy 8-bit parts, while offering more memory, faster math and more connectivity. Pick the core class to match the job: Cortex®-M0 (e.g. PSOC™ 4 at 48 MHz, or XMC1100 at 32 MHz) for low-cost I/O and mixed-signal; Cortex®-M4 with FPU (e.g. XMC4000, up to 144 MHz) for DSP and math; dual-core Cortex®-M4/M0+ (PSOC™ 6, up to 150 MHz) to run an application core alongside a low-power core; Cortex®-M33 with FPU (e.g. PSOC™ Control C3M5, up to 180 MHz) for advanced motor control and power conversion; or multi-core Cortex®-M33/M55/U55 (PSOC™ Edge, up to 400 MHz) for next-generation edge AI applications.
Map your Step-1 list onto silicon. Need Bluetooth® LE? PSOC™ 63 integrates it. Need Wi-Fi and Bluetooth®? Choose a PSOC™ 6 Wi-Fi/BT kit. Driving a motor or a power stage? PSOC™ Control C3 adds high-resolution PWM and a CORDIC accelerator. Running a vision or audio model on-device? PSOC™ Edge integrates neural-network acceleration. Battery-powered? Prioritize active current (as low as 22 µA/MHz on PSOC™ 6's Cortex®-M4 core) and sleep modes. Want plug-and-play sensors? Infineon's Shield2Go boards and the My IoT adapter (which handles 3.3 V↔5 V level shifting) let you stack sensors onto an XMC™ maker board or an Arduino Uno.
Reduce to two or three candidate families, compare them in the table below, then validate on an evaluation kit — for example the XMC1100 Boot Kit, a PSOC™ 4 or PSOC™ 6 Pioneer Kit, or the PSOC™ Control C3M5 Evaluation Kit (KIT_PSC3M5_EVK) — before committing. Prototyping on the real board surfaces toolchain, pin-mapping and power realities a datasheet will not.
Arduino Uno is a how-many-bit microcontroller?
The Arduino Uno is an 8-bit microcontroller board. The classic Uno (Rev3) uses the ATmega328P, an 8-bit AVR from Microchip (formerly Atmel) at 16 MHz with 32 KB of flash and 2 KB of SRAM. The newer Uno R4 (2023) is different — it uses a 32-bit Renesas RA4M1 (Arm® Cortex®-M4) at 48 MHz. So the answer depends on the board: 8-bit for the R3, 32-bit for the R4. If you are choosing a board today and expect larger, faster or connected projects, a 32-bit Arm® Cortex®-M part such as Infineon's PSOC™ 4, PSOC™ 6 or XMC™ gives more headroom than the original 8-bit design.
What is an Arduino microcontroller?
An Arduino microcontroller is the single chip on an Arduino board that runs your program — reading inputs, running logic and driving outputs. On the classic Arduino Uno that chip is the 8-bit ATmega328P; other Arduino boards use different microcontrollers (the Uno R4 uses a 32-bit Renesas RA4M1). “Arduino” itself is the open-source hardware and software ecosystem, not a chip maker, so an “Arduino microcontroller” means whichever MCU a given Arduino-compatible board is built around. Many third-party boards, including Infineon's XMC™ maker kits, are programmed from the same Arduino IDE while using their own microcontrollers.
Which Infineon microcontroller should I choose instead of an Arduino Uno?
It depends on what the project needs. For low-cost mixed-signal and capacitive-touch designs, PSOC™ 4 (Arm® Cortex®-M0/M0+ at 48 MHz) or XMC1000 is the closest step up from an 8-bit Uno. For battery-powered or connected projects, PSOC™ 6 pairs a 150 MHz Cortex®-M4 with a 100 MHz Cortex®-M0+ and integrates hardware security. For motor control and power conversion, PSOC™ Control C3 runs a Cortex®-M33 at up to 180 MHz with high-resolution PWM. For on-device machine learning, PSOC™ Edge combines a 400 MHz Cortex®-M55 with neural-network acceleration. Start from your performance, memory and connectivity requirements rather than the part number.
Is a 32-bit Cortex®-M microcontroller fast enough for real-time control in a prototype?
Yes. A 32-bit Arm® Cortex®-M microcontroller comfortably handles real-time control loops that an 8-bit board struggles with. Infineon XMC4000 devices run a Cortex®-M4 with FPU and DSP instructions at up to 144 MHz, and PSOC™ Control C3 targets real-time control specifically, running a Cortex®-M33 at up to 180 MHz with high-resolution PWM and a CORDIC accelerator for control-loop math. Real-world latency depends on your interrupt design, clock configuration and peripheral use, not just clock speed — but for maker and prototyping control tasks such as motors, sensors and closed-loop demos, these parts have ample headroom.
Do I need any certification to use a 32-bit MCU in a prototype?
No. Building and testing a prototype needs no certification — you can develop freely on an evaluation kit. Certification only becomes relevant if you turn the prototype into a product sold in a regulated market, where the finished device (not the MCU alone) may need EMC, radio (e.g. RED, FCC) and safety approvals. For connected designs, choosing an MCU with hardware security helps later: PSOC™ 6 integrates a hardware root-of-trust, secure boot and crypto acceleration, and PSOC™ Control C3 is PSA Certified™ Level 2. During prototyping itself, focus on function; plan certification when you scope productization.
Do 32-bit Infineon boards use 3.3 V or 5 V logic, and does that affect my shields?
Most Infineon 32-bit boards use 3.3 V logic, so 5 V-only Arduino shields are not guaranteed to work directly — the single most common hardware-design mistake when moving from an Arduino Uno. Infineon's Shield2Go sensor boards are designed for this ecosystem, and the My IoT adapter provides 3.3 V↔5 V level shifting so Shield2Go boards can be used with a 5 V Arduino Uno. When reusing an existing shield, always check its logic-level and power requirements against the board's datasheet before connecting — mismatched levels can damage parts.
For common project scenarios, here is a direct 32-bit starting recommendation. These are worked starting points — confirm against your Step-1 requirements.
1. Assuming 5 V shields just work. Most Infineon 32-bit boards run 3.3 V logic. Connecting a 5 V-only shield directly can misbehave or damage parts — use the My IoT adapter for 3.3 V↔5 V level shifting, or check the shield's spec first.
2. Assuming Arduino form factor means Arduino IDE support. Arduino-shield-compatible headers describe the board's physical footprint. Programming support is separate: XMC™ has an Arduino IDE board package, while other families are developed in ModusToolbox™. Check both before you plan a build.
3. Over-speccing the MCU. Picking a 400 MHz PSOC™ Edge for a job a PSOC™ 4 or an 8-bit Uno could do wastes cost and power. Size to the Step-1 requirements, not the datasheet maximum.
4. Under-speccing for AI or control workloads. The opposite error is just as common. Neural-network inference and high-frequency power control need dedicated hardware — an NPU on PSOC™ Edge, high-resolution PWM on PSOC™ Control — not just a faster general-purpose core.
5. Forgetting to add the board package. XMC™ parts are not preinstalled in the Arduino IDE — add the ‘XMC™’ package via Boards Manager first, or the board will not appear.
6. Ignoring power modes on battery builds. A 32-bit MCU only delivers long battery life if you use its sleep/low-power modes and dynamic frequency scaling — design them in from the start.
● ModusToolbox™ software — Infineon's cross-platform tools, drivers, middleware and RTOS support; the common professional path across PSOC™ and XMC™.
● Arduino IDE + XMC™-for-Arduino core — add the ‘XMC™’ package via Boards Manager to program XMC™ boards; PSOC™ 6 is also Arduino-supported.
● MicroPython — supported on parts of the Infineon-for-Makers board range for fast scripting.
● Shield2Go / Kit2Go + My IoT adapter — plug-and-play XENSIV™ sensor and security boards for rapid prototyping.
● Evaluation kits — PSOC™ 4 Pioneer Kit • PSOC™ 6 Pioneer Kit • KIT_PSC3M5_EVK • KIT_XMC11_BOOT_001
● Infineon for Makers landing — Infineon for Makers
Training and walkthrough content here.
→ PSOC™ 4 Microcontroller: Arm® Cortex®-M0/M0+ (low-cost mixed-signal and CAPSENSE™ designs)
→ PSOC™ 6 Arm® Cortex®-M4/M0+ (dual-core, low-power, connected prototypes)
→ PSOC™ Control C3 Arm® Cortex®-M33 (motor control and digital power conversion)
→ PSOC™ Edge Arm® Cortex® M55/M33 (on-device AI, vision, audio and advanced HMI)
→ XMC™ MCUs (Cortex®-M0 / Cortex®-M4 maker and control designs)
Ask the Infineon microcontroller community: Infineon Developer Community