Infineon enhances Electreon's electric road charging with high-power silicon carbide technology

Business & Financial Press

Dec 04, 2025
  • Electric road system charges buses and trucks as they drive along streets and highways
  • Customized silicon carbide modules by Infineon maximize power density, enabling electric vehicles to operate 24 hours a day with smaller batteries
  • Wireless in-road charging solution is a key innovation for reducing carbon emissions in transportation

 
Munich, Germany – 4 December 2025 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) will supply customized silicon carbide (SiC) power modules to Electreon (TASE: ELWS), a leading provider of wireless charging solutions for electric vehicles (EVs), for its dynamic in-road charging technology. This wireless electric road system (wERS) lets EVs charge wirelessly using inductive charging. Copper coils embedded beneath the road surface transfer power to buses, trucks and other EVs as they travel. The system connects to the power grid, activating vehicles when they're above the coils. Infineon's customized SiC modules are at the heart of the application and efficiently convert the energy that comes from the power grid for seamless wireless battery charging. Electreon's system leverages these modules to maximize performance, reliability and energy efficiency. This technology is especially beneficial on highways, toll roads and in other high-traffic areas like ports and critical mobility hubs such as airports.
 
The system's power transfer is boosted to an average of 200 kW, with peaks exceeding 300 kW, using EasyPACK™ 3B CoolSiC™ 2000 V modules from Infineon that were specifically developed to meet Electreon's requirements. This performance was confirmed in a milestone achieved recently on France's A10 highway, the world's first highway to wirelessly charge heavy and medium-duty trucks, buses, vans and passenger cars in motion. Continuous on-route charging keeps the battery topped up, allowing vehicles to travel farther and use much smaller battery packs. This cuts upfront vehicle costs and reduces vehicle weight, freeing up more capacity for cargo. Electreon has already incorporated Infineon's customized EasyPACK 3B CoolSiC 2000 V modules in test tracks in the U.S., Germany, France, Norway, Portugal, Sweden, Italy, Israel and Japan. There are current plans to integrate the technology into upcoming longer-distance projects. 
 
"Electreon's wireless charging system is a real game changer on the road to reducing carbon emissions in transportation," said Dominik Bilo, Executive Vice President and Chief Sales Officer Industrial & Infrastructure at Infineon Technologies. "We're proud to contribute to this groundbreaking innovation with our customized SiC power modules, which efficiently convert electrical energy to charge vehicles on the go, tailored to meet Electreon's specific needs. The solution fits perfectly with our goal to contribute to a climate-neutral future, further driving decarbonization and digitalization."
 
"Wireless EV charging is already happening today, and Electreon is at the forefront of this transformation. We're using Infineon's advanced silicon carbide technology to make in-road charging even more powerful and efficient, allowing electric buses and trucks to operate continuously without relying on traditional charging stations. This breakthrough reduces operational costs, lowers emissions and expedites EV adoption on a global scale. The world is embracing wireless charging, and we are proud to lead the way," said Electreon CEO Oren Ezer. 
 
SiC-based semiconductors have revolutionized high-power applications like EV charging by switching electricity at higher frequencies with lower energy loss, enabling more compact designs. These semiconductors also demonstrate high reliability and robustness in extreme conditions and dissipate heat more effectively than silicon does. 
 
About Electreon


Electreon is a global pioneer in wireless charging solutions for electric vehicles. Its groundbreaking technology transforms roads into wireless charging platforms, enabling vehicles to charge both while parked and on the move. The company's modular charging infrastructure is compatible with all types of electric vehicles, providing a universal charging solution. This technology offers a smart solution for electrifying transport fleets, saving energy and operational costs, reducing the need for large batteries, and providing a sustainable charging solution. Since going public in 2018, Electreon has built a global network of over 100 partners, including major automakers such as TOYOTA, DENSO, Ford, IVECO, and Kenworth, as well as infrastructure, engineering, energy and logistics companies like UPS. In 2025, the company received the ISO/SAE 21434 standard for cybersecurity in vehicles.

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Press Photos

Electreon's wireless charging system leverages Infineon’s SiC modules to maximize performance, reliability and energy efficiency.

JPEG

2126x1196 px

Download

Information Number : infgip202512-033

avatar

Veronika Seifried

Spokesperson Power Systems Division (PS)

+49 89 234 61662

Send email