- Complete system solutions for smart TVs
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
- FPGAs in datacenter applications
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
- Complete system solutions for smart TVs
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
Nov 04, 2026
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
Nov 04, 2026
Like Magic: AWL-Electricity and Infineon enable true long-range wireless power across industries
Apr 08, 2026
Forget precise alignment and short cables. Our associated partner, AWL-Electricity, leverages Infineon’s CoolGaN™ solutions to deliver wireless power & charging that works through objects (incl. metal), over distances, and even while moving.
For years, "wireless charging" has often meant placing a device on a very specific spot on a charging pad. While convenient, it hasn't truly severed the cord. Today, AWL-Electricity (AWL-E) is changing that definition. By combining their proprietary IP on system designs with Infineon’s power portfolio, they have developed a next-generation wireless power solution that overcomes past limitations and sets a new benchmark in functionality and significantly extends use cases across applications.
Achieving wireless power transfer with 92% DC-to-DC efficiency and 50% misalignment tolerance in optimal environments requires exceptional switching performance. AWL-E maintains reliable power delivery even in harsh environments by building its platform on a robust Infineon backbone.
The system integrates CoolGaN™ High Voltage switches (IGOT65R035D2, IGLT65R035D2, IGOT65R055D2) to handle the rapid switching frequencies needed for long-distance transmission. These are paired with OptiMOS™ 5 silicon MOSFETs (BSC07N10NS5ATMA1) to manage the buck-boost conversion, creating a highly efficient power stage that generates minimal heat—allowing the hardware to be embedded safely inside walls, furniture, or sealed industrial robots.
Francis Beauchamp-Verdon, Co-founder, VP and Business Development Director at AWL-E, comments:
“Infineon uniquely brings you into their family with a recognition that a strong ecosystem ultimately solves today's power needs. Infineon's GaN transistors, eval boards, and partner opportunities have boosted acceptance of our GaN-based MHz power coupling systems.”
Together, the companies have developed a versatile platform that adapts to diverse industry needs.
(Some products are not for sales in China)
With near-zero intrinsic heat generation, high misalignment tolerance and the unique ability to transmit through metal, AWL-E’s technology unlocks new possibilities for the Industrial, Automotive and Consumer Electronics markets, particularly in sealed enclosures that competing WPT solutions cannot reach.
- High-Power System (∼1.2kW): Delivers focused, 1:1 (one transmitter for one receiver) or 1:2 power transfer.
- Long-Range System (1:N): Creates a wireless "power bubble" that powers multiple receivers simultaneously from a single transmitter over long distances (up to ∼1.5m or more in optimal environments).
High-Power System
Long-Range System
Industrial: Powering the Smart Factory
In environments where downtime and cable maintenance are costly, AWL-E’s technology powers the factories of the future:
- Dynamic Fleets (AGVs & AMRs): High-Power allows charging while in motion, eliminating docking downtime and maximizing operational ROI.
- Humanoids: Utilizing Wireless Power Transmission to achieve 360° movement without wire wear-and-tear.
- IoT Sensors: Long-Range transmission eliminates cables and batteries, fully sealing critical sensors against harsh environments, ensuring uninterrupted data collection.
Mobility: Unrestricted Systems
AWL-E’s technology eliminates complex wiring harnesses to power the future of mobility:
- Autonomous Recharging (Drones & LEVs): High-Power pads automate charging for UAVs and light electric vehicles, removing the need for manual intervention.
- Self-Driving Sensors: Long-Range 1:N transmission can simultaneously power multiple sensors where wires cannot reach, completely eliminating complex cabling and the need for battery replacements.
Consumer Electronics: True Spatial Freedom
For the smart home, AWL-E replaces cable clutter and battery anxiety with an invisible power infrastructure:
- Total Integration (Laptops & Peripherals): High-Power transmitters embedded into wood, stone or polymers deliver a "drop and forget" experience, seamlessly charging devices without fragile ports or altering furniture design.
- Batteryless Smart Homes (Cellphones, IoT & Wearables): Long-Range 1:N transmission simultaneously powers up to 20 devices within a 1.5-meter radius, eliminating battery anxiety and significantly reducing e-waste.
This partnership and the resulting solutions represent a fundamental shift in how we interact with power. By decoupling energy from the physical plug, AWL-E and Infineon are doing more than just eliminating wires—they are proving that wireless can be as attractive as wired. With up to 92% efficiency and 50% misalignment tolerance, the technology minimizes energy waste even when devices aren't perfectly aligned. Together, they enable a new level of autonomy: whether it is an AGV that never stops to move and recharge on-the-go or a smart home that powers all devices invisibly, this technology ensures that the energy we need is always there—seamless, sustainable, and completely untethered.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
AWL-Electricity is a design house and system integrator that has developed a next-generation wireless power solution, overcoming the limitations of traditional induction. They offer adaptations for automotive, industrial, and consumer electronics use cases.