Infineon and Flex launch Zone Controller Development Kit for software-defined vehicles at CES 2026
Infineon and Flex launch Zone Controller Development Kit for software-defined vehicles at CES 2026
Technology news
Munich, Germany – 02 January 2026 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and Flex take the next step in their collaboration to accelerate the development of software-defined vehicles (SDVs). At CES 2026, they will launch a Zone Controller Development Kit—a modular design for Zone Control Units (ZCU) engineered to fast track the development of SDV-ready E/E architectures. The new development kit follows a scalable approach and is based on reusable assets, combining approximately 30 unique building blocks. This allows developers to configure different ZCU implementations flexibly in short development cycles and offers a clear path from concept to series implementation.
In next-generation E/E architectures, ZCUs connect and power a large number of diverse peripherals. Not all of those peripherals remain consistent across vehicle platforms and models, leading to different ZCU requirements. Current ZCUs, however, are often not optimized for the specific use case or vehicle platform in which they are used.
With the development kit’s building block concept, developers can right size their designs for many individual implementations while preserving feature headroom for future models. This reduces the bill of materials and shortens development cycles. The design platform allows OEMs to realize well over 50 power distribution, 40 connectivity, and 10 load control channels for rapid evaluation and early application development. A dual MCU plug-on module is available for high end ZCU implementations where high I/O density and computational power are paramount. This flexibility enables customers to start with the superset, then optimize to either two cost effective MCUs or a single MCU based on feature and budget requirements. This approach aligns with the platform’s guiding principle: start with the superset, then reduce components to optimize for cost without compromising quality or program velocity.
Infineon and Flex’s Zone Controller Development Kit enable all essential zone control functions, including I2t (ampere-squared seconds), overcurrent protection, overvoltage protection, capacitive load switching, reverse polarity protection, secure data routing with hardware accelerators, A/B swap for over-the-air software updates, and cybersecurity. The pre-validated hardware combines best in class automotive semiconductor components from Infineon, including AURIX™ microcontrollers, OPTIREG™ power supply, PROFET™ and SPOC™ smart power switches, MOTIX™ motor control solutions and other products with Flex’s design, integration, and industrialization expertise. The software stack includes contributions by Vector to leverage widely adopted tooling and know how in embedded software, testing and integration.
Availability
Pre orders for the Zone Controller Development Kit are open now. For more information, please visit https://www.infineon.com/evaluation-board/FlexZoneXTM or contact your local Infineon sales representatives. Shipments are foreseen to begin in the end of CY Q1 2026. More information is available in the Infineon Meeting Room LVCC West W307 at CES 2026.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Infineon and Flex launch Zone Control Reference Kit to fast-track the development of SDV-ready E/E architectures
PNG
2126x1196 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : infatv202601-038