A MOSFET (Metal Oxide Semiconductor Field Effect Transistor) is a semiconductor device that is typically used as a voltage-controlled switch.
It comprises three terminals: the gate, the drain, and the source. The main purpose of the MOSFET is to efficiently deliver power to a load.
What is a MOSFET explanation with a Gate, Drain and Source
A MOSFET is a voltage controlled device composed of a gate, a source and a drain. The gate voltage is typically provided by a microcontroller or a driver IC.
By applying the gate voltage to the gate terminal, the current will start to flow from the source to the drain terminals.
How MOSFETs work schema
To understand the efficiency of the current flow, we can take a look at the RDS(on) rating of the device.
The RDS(on) is the resistance from the source terminal to the drain terminal when the device is on.
This rating is measured in ohms or milliohms.
RDS(on) (resistance) rating of a MOSFET device
There are two different MOSFET modes, the enhancement and the depletion. Both of these modes have two channel types, the N-channel, and the P-channel. The enhancement mode means that the device is always off, and needs a gate voltage to turn on.
On the other hand, the depletion mode means that the device is always on, and needs a gate voltage to turn off. Nowadays, the most commonly used MOSFETs are N-channel enhancement-type devices.
MOSFET operation modes: enhancement and depletion
MOSFETs can also be lateral or vertical when it comes to their structure, which means that the conducting channel of the MOSFET is either lateral or vertical.
In the lateral structure, all three terminals are on top, on the same side of the silicon die.
It is very common for planar-type MOSFETs and it may also still be used nowadays for low-power MOSFETs, such as small signal types.
Lateral MOSFET structure
In vertical-type MOSFETs, the gate and source terminals are usually on top, on the same side of the die, while the drain terminal is on the vertically opposite side, as you can see here.
This type of structure is known as a trench MOSFET, and it is the most used design by MOSFET suppliers today.
For example, CoolMOS™, OptiMOS™, and StrongIRFET™ are all vertical-type trench MOSFETs.
Vertical MOSFET structure
N-type enhancement mode planar MOSFET
Let‘s use the N-type enhancement mode planar MOSFET to deep dive into the MOSFET structure. The most important element is the metal oxide semiconductor interface because it is responsible for its operation. Here, you can see the detailed structure of an N-type enhancement mode planar MOSFET.
The basis of the MOSFET construction is a silicon material that is lightly doped with Boron atoms to make it slightly P-type in concentration. This is called the p-substrate. To build the source and the drain regions, high-energy and high-concentration implants of N-type atoms are used.
The gate oxide, which is built with thin oxide, is on the silicon region between the source and the drain, partially overlapping these regions. When the gate voltage is applied, the negative atoms are attracted under the gate and the N-channel is formed. At this moment, the current will begin to flow.
Please note that other manufacturing steps may vary depending on the MOSFET type. Nevertheless, these are the basic operational building blocks of a MOSFET.
MOSFETs operate in three different modes: Depletion, Accumulation and Inversion.
These modes refer to the status of the MOSFET channel and are described below:
Depletion mode
The depletion mode refers to the MOSFET in the off state. That is when the voltage of the gate is lower than the gate threshold voltage.
The gate threshold voltage is the minimum voltage required to form the channel between the drain and the source terminals.
So, when the gate voltage is lower than the gate threshold voltage, a depletion is formed between the drain and the source and the MOSFET is in the off state. This way, no current will flow.
N-channel MOSFET depletion mode
Accumulation mode
The accumulation mode happens when the gate voltage increases above zero but is still lower than the threshold voltage. This occurs at the beginning of the channel formation due to the positive gate voltage.
Note that there may be a very small sub-threshold or leakage current occurring in the channel! Here, an inversion layer begins to form, where the polarity of the P-substrate under the gate starts changing.
N-channel MOSFET accumulation mode
Inversion mode
The inversion mode has two types of operation:
› Triode or linear mode
› Saturation mode
Let’s start by focusing on the first one. In this operation mode, the current increases in a linear way with the applied drain voltage.
In this case, the gate voltage is higher than the gate threshold voltage. The inversion layer increases and the N-channel is formed between the drain and the source terminals, which means that the current will flow. This current is proportional to the gate and drain voltage, which is higher than zero.
On the other hand, the saturation mode occurs when the current through the device starts to level off or flatten.
This happens because the current cannot increase in a linear way for a long period of time with the applied drain voltage.
When the drain voltage reaches a value equal to the difference between the gate voltage and the threshold voltage, the conducting channel becomes “pinched off”, and the current will remain constant.
This “pinch off” occurs due to the reverse biasing effect on the drain terminal caused by the increase in the drain voltage.
N-channel MOSFET Triode/linear mode
On the right are typical datasheet curves related to the linear and saturation modes, where we can see the relationship between voltage and the output current.
Example of MOSFET current-voltage curves
By analyzing this graph, we can see the relation between the drain-source current and the drain-source voltage, applied for different values of the gate to source voltage.
Here, the dotted line indicates the edge of the saturation boundary, until the current increases linearly with the applied drain voltage. When this limit is exceeded, the drain current remains more or less constant with the increasing drain voltage.
Relation between the drain-source current and the drain-source voltage of MOSFETs
By analyzing this graph, we can see the relation between the drain-source current and the drain-source voltage, applied for different values of the gate to source voltage.
Here, the dotted line indicates the edge of the saturation boundary, until the current increases linearly with the applied drain voltage. When this limit is exceeded, the drain current remains more or less constant with the increasing drain voltage.
Additionally, this graph shows the relation between the drain current and the applied gate voltage for a fixed value of the drain voltage.
As you can see, the current quickly increases once the gate voltage is higher than the threshold voltage.
Please note that there is some amount of current flow before the threshold voltage is reached. This is called subthreshold current or leakage current.
Relation between the drain-source current and the drain-source voltage of MOSFETs
Share in WeChat
Scan the QR code with your WeChat App to share this page.
What is a MOSFET?
A metal–oxide–semiconductor field effect transistor (MOSFET) is a voltage-controlled semiconductor device used for switching and amplification.
It has three main terminals — gate, drain, and source (plus an internal body diode) — and is controlled by the electric field from the gate rather than by a control current.
Is a MOSFET basically a switch?
In most power and digital designs, yes — a MOSFET is used as an electronic switch. A gate voltage above the threshold turns it fully ON (a low-resistance path), and below the threshold it is OFF (an open circuit).
It can also act as an analog amplifier in its linear region, but switching is by far its most common role — see how does a MOSFET work as a switch for using a MOSFET as a switch in real circuits.
Does a MOSFET control current or voltage?
A MOSFET is voltage-controlled. The voltage between gate and source (VGS) sets how much current flows from drain to source, while the gate itself draws virtually no current. This is the key difference from a current-controlled BJT.
Why does a MOSFET gate draw no current?
The gate is separated from the channel by a silicon dioxide insulating layer, so no DC current can pass through it.
How does a MOSFET turn on and off?
A MOSFET turns on when the gate-to-source voltage rises above the gate threshold voltage (VGS(th)), which forms a conducting channel between drain and source. It turns off when VGS falls back below that threshold and the channel disappears.
For an enhancement-mode MOSFET, a positive gate voltage switches an N-channel device on; a depletion-mode device works the other way around.
Is a MOSFET just a transistor?
A MOSFET is one specific kind of transistor — a metal-oxide-semiconductor field effect transistor. It belongs to the field effect transistor (FET) family and behaves differently from bipolar transistors (BJTs): it is controlled by an electric field at an insulated gate rather than by a base current.
For the general principle behind all transistors, see how does a transistor work.
What are the critical parameters of a MOSFET?
The parameters that govern conduction and switching behavior are:
- RDS(on): influences conduction losses and thermal rise
- Gate charge (Qg): determines the drive energy needed per switching cycle
- Safe operating area (SOA): defines the permitted combinations of voltage, current, and time during transients
- Body diode: affects reverse-current behavior and synchronous-rectifier design
How to read the parameters on a datasheet?
Datasheet parameters guide MOSFET selection:
- VDS defines the maximum voltage capability, with margin for transients
- ID reflects continuous current under specific thermal conditions
- RDS(on) determines conduction loss
- Gate charge (Qg) and capacitances influence switching losses and gate-driver sizing
Designers must also review SOA curves, thermal resistance, package ratings, and diode characteristics.
For how to read and apply breakdown-voltage specs in detail, see MOSFET voltage ratings - how to read and apply breakdown voltage specs.
How do I find the right MOSFET for my application?
MOSFET selection depends on application requirements, operating voltage, control strategy, and desired switching performance. A few rules of thumb:
- Motor control: prioritise low RDS(on) for conduction losses, sufficient VDS margin for inductive spikes, and a manageable Qg for efficient switching at the motor's PWM frequency.
- Switching power supplies: focus on adequate VDS breakdown voltage, minimal RDS(on) for efficiency, and low Qg and reverse-recovery charge (Qrr) for reduced switching losses.
Should I use an N-channel or a P-channel MOSFET?
The choice comes down to where the switch sits and how it is driven:
- N-channel MOSFETs use electrons (higher mobility, lower RDS(on)) and, with the source tied to ground, are ideal for low-side switching. They dominate high-efficiency designs such as synchronous rectifiers and DC-DC converters.
- P-channel MOSFETs use holes (higher RDS(on) for the same die area) but simplify high-side switching, where the source is referenced to the positive supply.
How do I drive the MOSFET?
A MOSFET is driven entirely by the gate-to-source voltage (VGS): no steady current flows into the gate, but the gate capacitance must be charged and discharged every cycle — which is what gate charge (Qg) quantifies.
An enhancement-mode device stays OFF until VGS exceeds VGS(th), so a gate-driver IC or a resistive pull-down is used to keep the OFF state defined. How the gate is driven then depends on high-side vs. low-side placement — see Driving high-side and low-side MOSFETs above.
Which MOSFET is most commonly used?
Enhancement-mode N-channel MOSFETs are the most common, thanks to their low conduction losses, simple drive requirements, and wide availability.
What does "normally-on" mean?
"Normally-on" refers to depletion-mode MOSFETs, which conduct current at zero gate voltage and require an external gate bias to turn them off.
What is the difference between a power MOSFET and a small-signal MOSFET?
A power MOSFET uses a vertical structure to handle high current and high voltage, with low RDS(on) and fast switching for power conversion. A small-signal MOSFET uses a lateral structure and is optimised for low-power, low-current analog or logic-level tasks.
How is a MOSFET used in CMOS circuits?
CMOS (complementary metal-oxide-semiconductor) circuits pair an N-channel MOSFET (NMOS) with a P-channel MOSFET so that one is always off, drawing almost no static power. That efficiency is why CMOS logic is the basis of nearly all modern digital integrated circuits — processors, memory, and logic chips.
Unlike bipolar junction transistors (BJTs), these MOSFETs need almost no drive current, which keeps CMOS circuits cool and dense and lets them work across both digital and analog circuits.