Infineon expands its OptiMOS™ 7 automotive MOSFETs offering with the ultra-low on-resistance TOLL package

Technology news

Oct 27, 2026

Munich, Germany – 27 October 2026 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) has introduced new OptiMOS™ 7 automotive MOSFETs that take the established TOLL package to a new performance level. By combining OptiMOS 7 semiconductor technology with a clip-based interconnection concept, Infineon has achieved ultra-low on-resistance in the proven 10 × 12 mm² TOLL footprint. This enables automotive customers to meet increasing power density and efficiency requirements in 12 V and 48 V systems without changing to larger package architectures or redesigning their board layouts. With best-in-class on-resistance performance, the new devices reduce power losses and enable higher-performing automotive power systems.

As vehicles become increasingly electrified, the demand for more efficient, compact, and high-performance power systems continues to grow. Automotive engineers face a design challenge: power and efficiency requirements are increasing, but moving to larger packages adds cost, board space, and design complexity. The new OptiMOS 7 TOLL devices address this challenge by delivering substantially lower conduction losses within the same form factor, combining leading electrical performance with design continuity.

The new 40 V, 80 V, and 100 V MOSFETs achieve RDS(on) values of 0.24 mΩ, 0.57 mΩ and 0.88 mΩ respectively, representing significant improvements of 65 percent, 48 percent and 37 percent compared with the referenced previous-generation OptiMOS TOLL products respectively. The combination of OptiMOS 7 technology and clip-based interconnection also improves capacitance and gate-charge characteristics, reducing switching losses in addition to conduction losses. A significantly tighter gate-threshold-voltage range supports more balanced current sharing when devices are connected in parallel, lowering the risk of damage to an individual MOSFET. 

This performance advance enables customers to implement high-current automotive power stages with reduced losses in the same package they already use. Depending on their system priorities, customers can leverage the ultra-low RDS(on) to achieve higher efficiency, reduced heat generation, greater current capability, or fewer parallel MOSFETs, providing strategic design flexibility without requiring changes to their existing ecosystem.

The new devices target high-power 12 V and 48 V applications including EPS, battery-disconnect switches, motor drives, and HV-LV DC-DC converters, where conduction losses directly impact system efficiency and thermal management. By enabling higher usable power within this established architecture, the OptiMOS 7 devices help automotive designers optimize their power distribution and conversion systems for next-generation electric and electrified vehicles.

Availability
Products are available. Further information is available at www.infineon.com/automotive-toll. 

Infineon at electronica 2026 
At this year’s electronica in Munich, Germany, Infineon showcases semiconductor innovations and system solutions for the AI era. As intelligence moves beyond the cloud and into machines, vehicles, industrial systems and everyday devices, technology from Infineon helps machines sense, process, connect and act in a safe, secure and energy-efficient way. At electronica 2026, Infineon will show technologies for Physical AI in robotics, for intelligent edge devices, software-defined electric vehicles, and future power supply from renewable power generation to AI data centers. Infineon will present innovative and energy-efficient solutions for an increasingly intelligent and connected world from November 10 to 13 in Hall C3, Booth 502. More information is available at www.infineon.com/electronica. 

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

 

Follow us: Facebook - LinkedIn

Press Photos

The new Infineon OptiMOS™ 7 automotive MOSFETs take the established TOLL package to a new performance level. With best-in-class on-resistance performance, the new devices reduce power losses and enable higher-performing automotive power systems.

JPEG

2126x1152 px

Download

Information Number : inftn202610-020

avatar

Oliver Scharfenberg

Spokesperson Automotive Division (ATV)

+49 89 234 38063

Send email