Nov 09, 2026
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
Nov 09, 2026
Business & Financial Press
Nov 04, 2026
Business & Financial Press
Nov 02, 2026
Business & Financial Press
Oct 27, 2026
Infineon Advances USB 20Gbps Ecosystem with PCIe Reference Design for 5-Meter Cabling and 36W Power Delivery
Infineon Advances USB 20Gbps Ecosystem with PCIe Reference Design for 5-Meter Cabling and 36W Power Delivery
Technology news
Munich, Germany – 30 September 2026 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY), a global leader in USB semiconductor solutions, today announced a new PCI Express® Gen4 x4 add-on card reference design that addresses key barriers to USB 20Gbps (USB 3.2 Gen 2×2) adoption. Debuting at VISION Stuttgart 2026, the industry-first standalone reference design integrates ASMedia’s ASM4242 USB4® host controller with Infineon’s EZ-PD™ CCG7 USB Power Delivery (PD) controller to support robust, high-performance connectivity for machine vision systems.
A primary focus of this release is Infineon’s continued effort to expand and mature the USB 20Gbps ecosystem. While the standard offers double the bandwidth of previous generations, widespread industrial adoption has been limited by signal integrity challenges over longer distances and complex power requirements. This new reference design directly addresses these hurdles by enabling reliable data transmission over 5-meter passive USB cables, which is important for industrial environments where cameras are often mounted far from the host PC. By demonstrating USB 20Gbps operation over passive cabling at this length, Infineon helps reduce an integration challenge for system designers.
The reference design features two USB-C® ports, each supporting USB 20Gbps data transfer and USB Power Delivery up to 36W (supporting 5V/3A and 12V/3A profiles). This combination allows for the deployment of AI-based camera systems without the need for separate power supplies, simplifying cabling and improving reliability in factory and lab settings. Targeting machine vision manufacturers, industrial PC suppliers, and system integrators, this solution provides a ready-to-use platform that accelerates time-to-market for next-generation imaging applications.
“Infineon is committed to driving the USB 20Gbps ecosystem forward by solving the real-world challenges that have slowed its adoption in industrial markets,” said Ganesh Subramaniam, Senior Vice President of Wired Connectivity Solutions at Infineon. “One of the key hurdles for machine vision applications has been maintaining signal integrity over long passive cables while delivering sufficient power to advanced sensors. This PCIe Gen4 x4 reference design demonstrates that USB 20Gbps is not just a high-speed data standard, but a practical, robust solution for industrial connectivity. By supporting 5-meter passive cabling and 36W of power per port, we are empowering camera OEMs and system integrators to deploy AI-driven vision systems with confidence, knowing that the underlying connectivity infrastructure is reliable and easy to implement.”
Availability
Learn more about Infineon’s EZ-USB™ FX20 USB 20Gbps peripheral controller here.
For more information on machine vision, please visit our application page.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Industry-First USB 20Gbps Reference Design for Machine Vision adoption integrates ASMedia’s ASM4242 USB4® host controller with Infineon’s EZ-PD™ CCG7 USB Power Delivery
JPEG
2126x1417 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : inftn202609-148
Ulrike Mittereder
Spokesperson Consumer, Compute and Communication, CSS Division
+49 89 234 43951