Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
Business & Financial Press
Nov 04, 2026
Business & Financial Press
Nov 02, 2026
- Company
- Our stories
- Events
- Press
- Investor
- Careers
- Quality
- Latest news
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
Business & Financial Press
Nov 04, 2026
Business & Financial Press
Nov 02, 2026
Infineon’s EZ-USB™ FX20 controller and EverProX 10-meter Active Optical Cable enable 20 Gbps connectivity for USB3 Vision cameras
Infineon’s EZ-USB™ FX20 controller and EverProX 10-meter Active Optical Cable enable 20 Gbps connectivity for USB3 Vision cameras
Technology news
Munich, Germany – 30 September 2026 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and EverProX (SZSE: 300548) are collaborating to introduce a 10-meter-long USB 3.2 Gen 2x2 Active Optical Cable (AOC) for next-generation USB3 Vision cameras, supporting data transfer rates of up to 20 Gbps. The solution combines Infineon’s EZ-USB™ FX20 peripheral controller technology with EverProX’s active optical technology. The AOC uses optical fiber for high-speed data transmission, addressing the signal loss and range limitations of conventional passive copper cables. At the same time, integrated copper conductors supply power through the cable, allowing a connected camera to receive both high-speed data and operating power via a single cable. This simplifies camera installation and reduces cable complexity in industrial systems, supporting applications such as high-speed defect inspection, 3D imaging, medical imaging, precision measurement, robotics, and AI-based visual analytics.
“The collaboration with EverProX underlines Infineon’s commitment to building a strong partner ecosystem and driving digitalization through innovations in connectivity,” says Ganesh Subramaniam, Senior Vice President of Wired Connectivity Solutions at Infineon. “By combining our expertise in USB peripheral controller solutions with EverProX’s advanced active optical cable technology, we are enabling a new generation of machine vision systems that require significantly higher bandwidth, longer transmission distances, and more flexibility in camera placement.”
“As machine vision cameras move toward higher resolutions, faster frame rates, and more sophisticated real-time image analysis, a high-bandwidth connection is becoming increasingly important,” says Tom Tang, President and CEO at EverProX. “By delivering USB 3.2 Gen 2x2 performance over a distance of 10 meters while simultaneously powering the camera, our Active Optical Cable provides a flexible and scalable connectivity solution for industrial machine vision applications.”
The EZ-USB FX20 peripheral controller enables USB 3.2 Gen 2x2 connectivity for machine vision cameras with data rates of up to 20 Gbps. Its high-bandwidth LVDS and LVCMOS interfaces support high-speed data transfer between image-processing devices and the USB interface, while integrated USB Type-C orientation detection and correction, high-capacity data buffering, and firmware support for USB3 Vision applications facilitate camera system development. Combined with the EverProX 10-meter AOC, the FX20 enables high-speed data transmission over distances beyond the practical range of conventional passive copper USB cables. The optical data path provides high signal integrity across the entire cable length and offers immunity to electromagnetic interference, making the solution suitable for electrically noisy industrial environments.
The 10-meter cable length gives developers greater flexibility when positioning cameras in factories, on production lines, in laboratories, and in robotic work cells, while host computers and image-processing equipment can remain in protected or centralized locations. Carrying both power and data through the AOC further simplifies deployment and helps reduce the number of cables, power adapters, and installation points required for each camera. The combination of high bandwidth, low latency, and long-distance data transmission supports higher camera resolutions and frame rates, reduced image compression, richer pixel formats, and faster delivery of image data to Edge AI processors and host computers.
Availability
Further information on Infineon’s EZ-USB FX20 USB 20 Gbps peripheral controller is available here, and more information on Infineon’s machine vision solutions is available at Infineon Machine Vision.
Further information on EverProX USB Active Optical Cable solutions is available at EverProX USB 3.2 Gen 2x2 AOC.
About EverProX
EverProX is a provider of advanced high-speed connectivity solutions specializing in Active Optical Cables for industrial, imaging, consumer, and enterprise applications. Its broad portfolio of USB, HDMI, and DisplayPort AOCs combines high-speed optical data transmission with application-specific cable lengths, connector configurations, mechanical features, and integrated power delivery. EverProX solutions enable longer reach, reliable signal integrity, flexible installation, and simplified system connectivity for next-generation machine vision cameras and other high-bandwidth devices.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Infineon EZ-USB™ FX20 peripheral controller enables USB 3.2 Gen 2x2 connectivity for machine vision cameras with data rates of up to 20 Gbps.
JPEG
2126x1263 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : inftn202609-147
Ulrike Mittereder
Spokesperson Consumer, Compute and Communication, CSS Division
+49 89 234 43951