SECORA™ ID V2 platform enables industry’s first FIDO Level 3+ certified secured authentication solutions
SECORA™ ID V2 platform enables industry’s first FIDO Level 3+ certified secured authentication solutions
Technology news
Munich, Germany – 1 December 2025 – As cyberattacks exploiting security vulnerabilities rise across industries, secured authentication is becoming critical for safeguarding digital identities. Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) reinforces its position as a leader in advanced security solutions with the world’s first FIDO CTAP2.1 Authenticator Level 3+ certificates on the SECORA™ ID V2 platform. The Infineon FIDO applet is part of Infineon’s applet collection and runs on the SECORA ID V2 platform, the same base as Eviden’s recently Level 3+ certified cryptovision ePasslet Suite. Both solutions provide robust protection against physical and software-based attacks, safeguarding private keys with strong security measures. Designed for high-security environments like government, finance, critical infrastructure, healthcare, and aerospace they offer future-ready protocol compliance and enhanced manageability.
Level 3+ is the highest level of security defined for FIDO Authenticator Certification, protecting against advanced software and hardware attacks, including invasive, side-channel and fault injection attacks. This certification level requires chip-level protection, making private key extraction or physical tampering extremely difficult. Customers benefit from reduced risk, compliance with stringent standards, and future-proof authentication. Level 3+ certified devices offer strong resistance to tampering, side-channel attacks, and phishing, allowing to keep private keys secured even if endpoints are compromised.
“This milestone reinforces Infineon’s leadership in advanced security solutions. Our customers can offer the strongest FIDO authentication available today, setting a new standard for secured authentication, access, and transactions,” says Maurizio Skerlj, Senior Vice President and Product Line Manager for Authentication and Identity Solutions at Infineon. “The fact that all first-to-market Level 3+ certified products are built on our SECORA ID V2 platform is a strong confirmation of Infineon’s position as a leader in security and most trusted partner.”
“Now that our Common Criteria EAL 5+ certified cryptovision ePasslet Suite has been extended by the Level 3+ certified FIDO authenticator application, based on SECORA ID V2 platform, our customers gain a first-mover advantage, enabling them to deliver the top security level for convenient authentication.” says Benjamin Drisch, Head of Citizen ID at Eviden.
SECORA ID V2 is built on Infineon's advanced 40 nm SLC38 security controller, offering high performance and robust security. It provides a versatile platform for use-cases such as eID documents, digital signatures, online authentication, and multi-applications, featuring an ARM® SecurCore® SC300 processor and match-on-card capabilities. The product complies with high-security standards like Common Criteria EAL 6+ (high) and is supported by powerful tools for streamlined integration and customization.
Infineon at TRUSTECH 2025
Visit Infineon from 2 to 4 December at Paris Expo Porte de Versailles, booth F025 in Pavilion 5.2, to discover our solutions for authentication and access. Learn more at www.infineon.com/promo/trustech.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Secured authentication for protecting digital identities enabled by the world’s first FIDO CTAP2.1 Authenticator Level 3+ certifications on Infineon’s SECORA™ ID V2 platform
JPEG
2126x1417 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : infcss202512-029
Ulrike Mittereder
Spokesperson Consumer, Compute and Communication, CSS Division
+49 89 234 43951