10 billion chips with Integrity Guard delivered – milestone proves Infineon's leadership in security

Technology news

Jun 11, 2025

Munich, Germany – 11 June 2025 – Security controllers are an essential part of modern digital life. They are embedded into ePassports, ID cards, payment cards, and smartphones, protecting the personal data and digital identities of billions of people worldwide. Since its introduction, well over 10 billion security controllers based on Integrity Guard security architecture by Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) have been delivered – marking a major milestone in the architecture’s global adoption. To withstand increasingly complex threats, these controllers themselves must meet highest security standards. The fundamental principles of the Integrity Guard architectures were introduced over 15 years ago with the first 16-bit security controllers of the SLE78 family and have since formed a central element of Infineon's security controller portfolio. Designed to deliver a high level of protection, it is integrated into various members of Infineon’s controller families and features a dual-CPU design with hardware-based error detection. In response to the growing demands for security and certification, Infineon is now adding a new member to the family: the TEGRION™ SLC27G with security architecture Integrity Guard 32.

“With over 10 billion security controllers with Integrity Guard being shipped, we statistically reached the whole earth population with our security architecture”, says Maurizio Skerlj, Senior Vice President and Product Line Manager for Authentication and Identity Solutions at Infineon Connected Secure Systems. “And the value of robust security controllers is now more evident than ever. We face rapid increases in global cyberattacks, combined with expanding digitalization that opens new avenues for cybercriminals, and tightening regulatory frameworks such as the EU Cyber Resilience Act. All this underscores the urgent need for advanced, secured solutions. This is precisely where our new member of the Integrity Guard 32 family, TEGRION SLC27G, steps in.”

This dual-interface and contactless controller is designed for secured identification, payment, authentication applications well into the future. Based on the powerful 32-bit Arm® v8-M instruction set, which has been further optimized with Infineon's security expertise, combines security, efficiency, performance, and easy implementation. With its excellent Integrity Guard 32 security architecture, it is perfectly equipped for long-term security and the ideal choice for products meeting the requirements of the Cyber Resilience Act (CRA). Integrity Guard 32 features highly efficient error detection and a self-contained, self-checking 32-Bit dual CPU system. With its update capability, it is the answer to future security requirements, accelerates certification processes, and enables a higher level of security without compromising performance or reliability, equally addressing the resistance against the exponentially increasing computing power of quantum computers.

The TEGRION Security Controller SLC27G is currently undergoing certification by the German Federal Office for Information Security (BSI) and is aiming for CC EAL6+ certification. This once again highlights Infineon's ongoing commitment to the global advancement of security.

Availability

The TEGRION SLC27G security controller, with up to 584 KB of non-volatile memory and a clock frequency of 100 MHz, is available as a sample and for large-scale production orders. Further information is available at www.infineon.com/products/security-smart-card-solutions/security-controllers/tegrion-security-controllers.

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Follow us: Facebook - LinkedIn

Press Photos

Integrity Guard

Integrity Guard

More than 10 billion security controllers based on the Infineon Integrity Guard security architecture have been shipped since its introduction

JPEG

2126x1871 px

Download

Information Number : INFCSS202506-115

avatar

Ulrike Mittereder

Spokesperson Edge Systems Division (ES)

+49 89 234 43951

Send email