- Consumer Wearables
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
- Domestic robots
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
- Intel CPU voltage regulator Ics
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
Oct 19, 2026
Business & Financial Press
Oct 15, 2026
Business & Financial Press
Oct 14, 2026
Business & Financial Press
Oct 07, 2026
- Company
- Our stories
- Events
- Press
- Investor
- Careers
- Quality
- Latest news
Business & Financial Press
Oct 19, 2026
Business & Financial Press
Oct 15, 2026
Business & Financial Press
Oct 14, 2026
Business & Financial Press
Oct 07, 2026
Infineon presents new ASIL-D-compliant 3-phase gate driver IC for braking systems and electric power steering in vehicles
Infineon presents new ASIL-D-compliant 3-phase gate driver IC for braking systems and electric power steering in vehicles
Technology news
Munich, Germany – 31 October 2024 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is launching the new MOTIX™ TLE9189 gate driver IC for safety-critical applications for 12 V brushless DC (BLDC) motors. With this new three-phase gate driver IC, Infineon is responding to the growing demand for motor control ICs required for by-wire solutions. The driver IC is qualified according to AEC Q100 Grade 0 and ISO 26262 (ASIL D). This makes the device particularly suitable for brake-by-wire and steer-by-wire systems, where conventional mechanical connections will be eliminated in the future.
“With the TLE9189 we are introducing the 4th generation automotive 3-phase smart gate driver IC to the market. It offers enhanced functionalities and unique features for intelligent motor control supporting the increasing demand of our customers for by-wire-solutions,” said Andreas Doll, Senior Vice President and General Manager Smart Power from Infineon. “The high reliability of the motor control design enabled by our new device is particularly important for safety-critical by-wire solutions.”
The MOTIX TLE9189 gate driver IC will be available in two different packages, the TQFP-48 (9 x 9 mm²) and the VQFN-48 (7 x 7 mm²). This allows customers to select the appropriate package for their application requirements. The device's supply voltage range is from 4.2 V to 36 V and is optimized for 12 V automotive battery systems. It features a conventional motor control concept consisting of PWM input and integrated current sense amplifiers for accurate current sensing. Compared to other devices, the TLE9189 offers very high flexibility and granularity for gate sequencing. In addition, various monitoring and diagnostic functions are integrated for monitoring of the device, the inverter, the microcontroller and the MCU interfaces. The product also features the unique adaptive MOSFET control function, patented by Infineon, which can help improve EMC performance, achieve target switching time and reduce power losses.
Infineon supports its customers during the design-in process with comprehensive support materials. These include a wide range of technical documentation like application notes. Simulation models, configuration tools and a complex device driver are available on request.
Availability
MOTIX TLE9189 gate driver IC in VQFN and TQFP samples are available now. Further information is available at www.infineon.com/bldc-motor-gate-driver-ics. A demo of the new gate driver IC will be showcased at electronica 2024 in Munich from November 12 to 15 (hall C3, booth 502).
Infineon at electronica 2024
At this year's electronica in Munich, Infineon presents innovative solutions that are helping to shape an all-electric society. Visitors can explore sustainable technologies that are transforming the mobility and automotive landscape, enabling sustainable buildings and smarter living, and promoting the growth of artificial intelligence with minimal environmental impact. The company will present intelligent and energy-efficient solutions for tomorrow's connected world from November 12 to 15 in Hall C3, Booth 502 under the motto “Driving Decarbonization and Digitalization. Together.” More information is available at www.infineon.com/electronica.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
The new MOTIX™ TLE9189
The new MOTIX™ TLE9189 gate driver IC is qualified according to AEC Q100 Grade 0 and ISO 26262 (ASIL D). This makes the device particularly suitable for brake-by-wire and steer-by-wire systems.
JPEG
2126x1363 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFATV202410-016