- Smart TV
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
Nov 17, 2026
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
Nov 17, 2026
Business & Financial Press
Nov 11, 2026
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
EU research project “Listen2Future” makes acoustic sensors for healthcare, energy and industry smaller and smarter
EU research project “Listen2Future” makes acoustic sensors for healthcare, energy and industry smaller and smarter
Business & Financial Press
- EU project Listen2Future brought together 27 partners from seven countries to research compact acoustic sensor technologies
- Innovative solutions enable faster diagnoses, better hearing systems and smart monitoring of production and energy infrastructure
- Research strengthens Europe’s sensor technology value chain
Villach, Austria, 17 November 2026 – The European research project “Listen2Future” has been successfully completed after more than three years. Led by Infineon Technologies Austria, 27 partners from seven countries worked on a new generation of compact acoustic sensor and system technologies. Through 14 demonstrators, the consortium demonstrated their functionality for applications in medicine and healthcare, energy and industry.
Acoustic sensors are used in medical ultrasound devices, hearing systems and industrial equipment, for example. They detect audible and inaudible sound waves, making it possible to obtain relevant information about materials, biological samples or the condition of technical equipment. However, some existing systems are still too large, energy-intensive or costly for mobile or continuous use.
This is where Listen2Future came in: The project developed new piezoelectric materials and used them to build innovative acoustic sensors. Combined with advanced electronics, innovative packaging solutions and new AI-based signal processing methods, the sensors were integrated into demonstrators. These show how future acoustic sensor systems can be made more compact, energy-efficient and intelligent.
“Sensor technology is a key enabling technology and an area of European strength. Through this application-oriented research and collaboration with leading partners from science and industry, we are strengthening Europe’s technological expertise in highly relevant fields. What matters is that the results move from the laboratory into practice and deliver real benefits. The project has successfully achieved this, creating impactful innovations for medicine, healthcare, energy and industry. It also helps to further strengthen the market position of European companies,” says Sabine Herlitschka, CEO of Infineon Technologies Austria AG.
Acoustic sensor systems: Small, intelligent, efficient
With 14 demonstrators, Listen2Future shows how intelligent acoustic sensor systems can transform future applications in healthcare, energy and industry. MEMS sensor technology, ultrasound technologies, electronics and AI-based signal processing open up new possibilities for diagnostic procedures, hearing systems, industrial quality control and energy infrastructure monitoring. The research team developed integrated system solutions – from new materials and microelectromechanical (MEMS) devices to electronics and packaging, software and algorithms – that translate acoustic signals into actionable information.
Healthcare: From mobile ultrasound and rapid infection detection to hearing aids
In healthcare, the consortium designed compact ultrasound demonstrators and researched novel sensor technologies for future mobile ultrasound systems. One focus was on miniaturized ultrasound transducers and the associated electronics, signal processing and system integration.
For infection diagnostics, ultrasound demonstrators were further developed to support the rapid, simple and non-invasive detection of serious infections. In one use case for detecting meningitis in newborns, the scan time was reduced from ten to three minutes.
Listen2Future also investigated new compact sensor solutions for future hearing aids and hearing systems. The technologies developed showed promising characteristics, particularly at high sound pressure levels. At the same time, further research is needed in system integration, long-term testing and user trials under realistic application conditions.
Monitoring for power grids and industry
For the energy sector, the project designed an AI-based acoustic sensor system to detect so-called partial discharges. These are small electrical discharges that can indicate early signs of insulation damage. Detecting and locating such partial discharges at an early stage allows maintenance to be planned more precisely and potential outages to be avoided.
Tests carried out during the project successfully demonstrated the potential of acoustic sensor technology for condition monitoring of power lines, substations and transformer stations. The technology can thus contribute to predictive maintenance and the long-term reliability of energy infrastructure.
In industrial quality assurance, Listen2Future also investigated contactless, non-destructive testing of components and materials. Compact piezoelectric micromachined ultrasound transducers were used to detect material changes and small defects. A testing system developed within the project was made 80 percent lighter and 50 percent smaller than the reference solution used for comparison. This opens up additional possibilities for mobile and automated testing methods, for example in industrial manufacturing, energy technology and aviation.
Bringing technologies together at system level
“Listen2Future has demonstrated the potential of integrating new materials, acoustic sensors, advanced electronics, packaging technologies and AI-based signal processing. It was particularly important that we were able to test these technologies using demonstrators under realistic conditions – from medical applications to energy infrastructure. The results provide a strong and validated foundation for further research, development and technology transfer activities in application areas of economic and societal relevance,” says Andreja Rojko, Listen2Future Project Manager at Infineon Technologies Austria.
Results with international visibility
Listen2Future produced 14 demonstrators. The consortium published 77 scientific publications, including 49 open-access publications. The project results were presented at 67 international conferences, workshops and specialist events. In total, the project recorded more than 354 communication and dissemination activities, including scientific publications, conference contributions, podcasts and videos. In addition, all partners developed patents, technology roadmaps and individual exploitation plans.
With a total project budget of around €30 million, Listen2Future brought together companies, research institutes and universities in a research network spanning the entire technology value chain, from materials and sensor development through electronics and packaging to software, algorithms and application-specific system integration.
Project partners
Austria: Infineon Technologies Austria AG (Project Coordinator), Silicon Austria Labs GmbH, GE Healthcare Austria GmbH & Co OG | Belgium: Pulsify Medical BV, IMEC Interuniversitair Micro-Electronica Centrum | Czech Republic: Vysoke Uceni Technicke v Brne, Ustav Teorie Informace a Automatizace av cr VVI, Institut Mikroelektronickych Aplikaci SRO | Germany: Hahn-Schickard-Gesellschaft für angewandte Forschung EV, Codasip GmbH, Infineon Technologies AG, Infineon Technologies Dresden GmbH & CO KG, Inoson GmbH, Path Medical GmbH, Technische Universität Darmstadt, Technische Universität München | Netherlands: Solmates BV, Sonion Nederland BV, Universiteit Twente | Norway: Elliptic Laboratories ASA, Sintef AS, Sonitor Technologies AS | Spain: Agencia Estatal Consejo Superior de Investigaciones Cientificas, Dasel SL, New Born Solutions, SMD Inductor de Analgesia SL, Universidad de Granada
The Listen2Future project received funding under Chips JU grant agreement No. 101096884. Funding was provided by the European Union and the national funding authorities of the participating countries.
Infineon Technologies Austria AG is a subsidiary of Infineon Technologies AG, a global semiconductor leader in power systems and IoT. Semiconductors are essential for mastering the energy-related challenges of our time and helping to shape the digital transformation. Infineon's microelectronics drive decarbonization and digitalization and enable groundbreaking solutions for green and efficient energy, clean and safe mobility as well as a smart and secure IoT.
Infineon Austria pools competencies for research and development, production as well as global business responsibility. The head office is in Villach, with further branches in Graz, Klagenfurt, Linz, Innsbruck and Vienna. With 5,787 employees (including around 2,500 in research and development) from 80 nations, the company generated revenue of EUR 4.7 billion in the 2025 fiscal year (ending 30 September). With research expenditure of 721 million euros, Infineon Austria is the strongest research company in Austria.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : infpr202611-032