In a power converter, the controller and the power stage work in different electrical domains. The controller operates at a few volts and is often connected to user interfaces, communication lines or protective earth. The power switches operate at hundreds or thousands of volts, and their switching node can jump by hundreds of volts within nanoseconds.

Galvanic isolation keeps these domains apart. There is no direct electrical connection between the two sides; only the information needed – such as the gate-drive command – is transferred across an isolation barrier. In an isolated gate driver, the input side is referenced to the controller and the output side to the power switch, and the output side runs from its own isolated supply.

 

Galvanic isolation is used for three main reasons:

  • Protection against electric shock: isolation of hazardous live parts is a requirement of safety standards in many systems.
  • Different reference potentials: the two sides can sit at very different voltages, for example ±2300 V or more across an Infineon coreless-transformer driver.
  • Robustness against fast transients: the barrier, together with high common-mode transient immunity (CMTI), keeps fast voltage changes on the power side from corrupting the control signal.
In one sentence...

Galvanic isolation separates two circuits so that there is no direct conductive path between them, while switching signals or energy still cross the isolation barrier – for example magnetically, through a transformer.

Gate drivers fall into three groups, depending on how the control signal reaches the power switch. Only the first group provides galvanic isolation.

A level-shift driver such as an SOI driver isolates its internal transistors from each other – SOI uses a buried silicon-dioxide layer – but this is not galvanic isolation between the input and output of the driver. Likewise, a truly differential input (TDI) driver tolerates ground shifts (for example ±70 V DC and ±150 V AC for 1EDN-TDI), but its input and output are not galvanically separated.

Decision tree for choosing a gate driver IC: isolation requirement, then number of channels and configuration, then voltage class.

The isolation requirement is the first decision when choosing a gate driver: non-isolated, functional level shift, or galvanic isolation (functional, basic or reinforced).

Insulation standards distinguish several levels of isolation. The level a system needs is set by the applicable system standard and the system’s insulation concept, not by the gate driver alone.

These definitions follow IEC 60664-1, VDE 0884-11 and UL 1577.

Hexagon graphic with galvanic isolation at the centre and the definitions of basic, supplementary, double, functional and reinforced isolation around it, citing IEC 60664-1:2020, VDE 0884-11 and UL 1577.

Galvanic isolation types: functional, basic, supplementary, double and reinforced isolation.

Isolated gate driver datasheets list several voltages. Each describes a different stress, so a single test-voltage figure is not enough to judge whether a driver fits the system.

Certificates apply to specific parts and packages. Always check the certificate and datasheet of the exact part, and remember that creepage on the board also depends on the PCB layout, material group, pollution degree and altitude.

3D illustration of two copper spiral coils on a silicon chip forming an on-chip coreless transformer

On-chip coreless transformer: metal spirals separated by silicon-oxide insulation carry the switching signal across the isolation barrier.

Infineon EiceDRIVER™ isolated gate drivers use coreless transformer (CT) technology. Using semiconductor manufacturing processes, an on-chip transformer made of metal spirals and silicon-oxide insulation is integrated into the driver. It transmits switching information and other signals magnetically between a separate input chip and output chip.

Benefits of the coreless-transformer approach include:

  • Functional, basic and reinforced isolation options, certified to UL 1577 and VDE 0884-11 / IEC 60747-17 in selected parts.
  • Large voltage swings of ±2300 V or more between input and output.
  • Robust signal transfer that is independent of common-mode noise, with CMTI of more than 300 V/ns in selected families.
  • Tight propagation-delay matching that does not vary with ageing, current or temperature.
  • Low power losses.

The output side of an isolated driver needs its own supply referenced to the power switch. Infineon’s EiceDRIVER™ Power 2EP1xxR full-bridge transformer drivers generate this isolated supply with few external components.

Use the system requirements, not the driver, as the starting point:

  • Galvanic isolation is mandatory: because of the safety standard, the working voltage, the grounding scheme or accessible control circuits: use a galvanically isolated (coreless transformer) driver, choose functional, basic or reinforced isolation according to the system insulation concept, and plan the isolated bias supply.
  • No galvanic barrier is needed, but the switch is floating (high-side or half-bridge): a level-shift driver based on SOI or JI technology can drive switches up to 1200 V, usually with a bootstrap supply.
  • The switch is ground-referenced (low-side): a non-isolated driver is sufficient; choose a truly differential input (TDI) driver if the ground potential shifts.

 

Then refine the choice by voltage class, number of channels, drive current, timing, CMTI, UVLO, package and qualification.

Next step

Compare isolated gate drivers by isolation class, package and protection features. Compare gate driver technologies.

Recommended Documents

What is galvanic isolation?

Galvanic isolation separates two circuits so that there is no direct conductive path between them. Signals or energy cross the isolation barrier by other means, for example magnetically through a transformer.

In an isolated system, the input and output sides have no direct electrical connection and can sit at different potentials. In a non-isolated system, they share a common reference. Isolated designs need an isolated supply on the output side; non-isolated designs do not.

Functional isolation is needed only for the equipment to work and does not protect against electric shock. Basic isolation provides basic protection against electric shock. Reinforced isolation provides protection equivalent to double isolation (basic plus supplementary).

No. Level-shift drivers based on SOI or JI technology transfer the signal to a floating high-side channel inside one monolithic chip. There is no galvanic barrier between input and output.

The isolation barrier withstood 5.7 kV rms for one minute in the UL 1577 test. It is a short-duration test value, not a working voltage; repetitive and working-voltage ratings such as VIORM are specified separately under IEC 60747-17 / VDE 0884-11.

VIORM is the maximum repetitive peak isolation voltage defined in IEC 60747-17 / VDE 0884-11 – for example 1767 V for many Infineon reinforced isolated drivers.

When the power switch turns on or off, the potential of the output side jumps relative to the input side. High common-mode transient immunity keeps the driver from misinterpreting these fast transients as switching commands.

In current EiceDRIVER™ names, the letter after “ED” shows the isolation: N = non-isolated, F = functional, B = basic, S or R = reinforced (for example 2EDN, 2EDF, 2EDB, 2EDS, 2EDR). In 1ED3xxx isolated drivers, “MU” marks UL-certified functional isolation and “MC” reinforced isolation certified by UL and VDE.

No component alone makes a system safe. The required isolation class comes from the system standard; the driver’s certificate, the PCB creepage and clearance, the bias supply and the rest of the insulation system must all meet it.