Infineon key visual in RGB

GaN, Decoded: What does “fast switching” really mean?

We’re bringing you the latest from the world of semiconductors – straight to your ears! From quick takes on trending applications to deep dives on product innovations, our experts give you their take on the tech behind the tech.

Podcast

What does “fast switching” really mean when we talk about GaN? In the first episode of GaN Decoded, host Peter Balint sits down with Infineon lead principal engineer Edward Jones to explore the difference between switching frequency and switching speed, and why GaN can deliver benefits ranging from higher power density and efficiency to lower switching losses. From AI data centers and humanoid robots to appliances and bidirectional switches, they examine where GaN’s unique characteristics matter and what engineers need to consider when designing fast-switching systems.

In this episode of the Podcast4Engineers, host Peter Balint speaks with Dr. Edward A. Jones, a Lead Principal Engineer in GaN Application Development at Infineon.

Peter Balint

Host:

Peter Balint has shaped visual and audio narratives at Infineon since 2021. He’s a video producer with 20 years of experience and has produced podcasts for the past 10 years. Over his career, Peter has interviewed speakers from all over Europe, bringing high-quality media production and engaging conversations to the forefront of his work.

Edward Jones

Guest:

Dr. Edward A. Jones is a Lead Principal Engineer in GaN Application Development at Infineon Technologies. He completed his Ph.D. at The University of Tennessee in 2017, and his B.S.E.E. in 2007 at Virginia Tech. Over 3500 papers have cited his peer-reviewed work, which includes 36 IEEE papers, 6 tutorial seminars, 3 patents, and one book.

He has also contributed to several other books, application notes, and keynote talks. His current focus is on developing the next generation of GaN power devices and GaN-optimized power electronics designs.

Guest: What does fast switching really mean? People use this pretty interchangeably to mean high frequency. Like I said, megahertz or 100kHz, but also the time it takes for the transistor to turn on and off. So there we're not talking about kilohertz or megahertz. We're talking about nanoseconds.

 

Host: Hello and welcome to the podcast for engineers. It's the podcast. You just have to listen to if you're interested in what's happening in the semiconductor market. I'm your host, Peter Balint. And today we're kicking off our brand new series called GaN decoded. In our first episode, we're asking a deceptively simple question: what does fast switching really mean? Our guest today is my colleague Edward Jones, who is a lead principal engineer in GaN here at Infineon. Thank you for coming on today.

 

Guest: Yeah, I'm happy to be here. Peter, let's get into it.

 

Host: Okay, so we often hear GaN as being a high frequency switch or being used for fast switching. This is maybe the primary thing we hear when people talk about GaN. What can you say about that? Yeah. It's true. Sometimes it really depends on on how and why you're using the GaN switch.

So let's think of some examples. The hot topic today is AI artificial intelligence. So if you look at an AI data center, one of the the key use cases for GaN there is the intermediate bus converter, what we call the high BC stepping down 800 to 50V and the MV IVC stepping down 50 to 12. In both of those cases.

You're going to use GaN likely in the in the megahertz range 1, 2, 3MHz. And this is something you maybe wouldn't do with another semiconductor technology because the switching losses or the switching transition times take too long and you just can't afford to go to that high frequency. But the reason why you're using GaN there is to go to the high frequency.

And the reason you want the high frequency is space. You know, the space real estate in an AI data center rack is at a premium. You you don't want to spend more space processing the power than you need to, because the point of the the rack is to process your requests online. You know, the the AI, the the intelligence of the artificial intelligence.

But that's not true for all applications. So some other exceptions would be motor drives. So if we look at physical AI, meaning humanoid robots, they're using GaN for, for the inverter, for the motor drive on a, on the, you know, the elbow joint or the wrist joint is also very popular. And there it is also about going into high frequency.

But in this case high frequency is maybe 100kHz at most, not megahertz. So an order of magnitude or more lower, but still higher frequency than what you might use with silicon, for example. And the reason why using the higher frequency there again, space real estate. You know, the elbow joint, right. But there's a counterexample. So think about your refrigerator or your washing machine in the refrigerator there's a compressor that keeps the food cold, and it's somewhere in the back of the refrigerator. You don't care how big that is, right? Then neither does the manufacturer. It's not about size. Their GaN is a very hot topic because, it runs at such a higher efficiency with so much less switching loss that there's less heated dissipate, and then you can get rid of a heat sink, so that getting rid of a heat sink means a big savings in weight and overall system cost.

But the switching frequency there is, let's say 20kHz. With GaN, it would be 20kHz without GaN. So it's not about going to higher frequency. It's just about the switching loss and the switching transition time being shorter. So what about bidirectional switching. I mean we just announced a 900 volt ColGaN BDS.

 

Host: How does that play in with this scene here?

 

Guest: Yeah, that's that's a really interesting use case as well. Because again, the the reason to use cool gain there is not about the switching frequency. There are topologies that are, you know, decades old that need a bidirectional voltage blocking transistor, which, you know, a MOSFET can't do that. It can block voltage in one direction. Conduct currents in both directions.

So it's bidirectional current. But if we wanted to be able to block 900V in either direction, for example in a cyclo converter or a matrix converter, then that's the motivation to use GaN in the first place, is that we can make a bi directional single switch, what we call CooGaN BDS and we can do this up to 900V and replace back to back IGBTs, back to back MOSFETs.

Now, because it's gain, you could go to a higher frequency, but very often people don't when they're doing these single stage topologies, because the benefit of using the bidirectional switch and this cyclo converter or matrix converter topology is that you've already reduced the overall system size and weight so massively by replacing two stages, an AC, DC and a DC DC stage with a single AC to DC stage.

You know the improvement further in size from going to higher frequency. It's not really the point. And then there's also an even more interesting example with the BDS, which is our 40 volt BDS. It's a bit different technology from the 900 volt or 650 volt BDS you were mentioning. So here the 40 volt cooling and BDS is a static switch.

And this its use case is in your cell phone. So to protect the charging port from the battery inside and to protect the battery from the charging port. So if you plug in a bad charger, you don't want the battery to be destroyed. But also if you if there's something wrong inside the phone, you don't want to cause the charger to be destroyed.

And that is a static switch. So I mean, talk about switching frequency. That's right. I mean, that's there's no frequency. It stays on as long as you're charging and then it's off.

 

Host: So as we dig into GaN a little bit, I have to ask, what is it about GaN that can perform these functions, these high switching functions so rapidly as opposed to silicon or silicon carbide?

 

Guest: Yeah. I mean this gets into really the core message of this podcast. What is fast switching really mean? People use this pretty interchangeably to mean high frequency. Like I said, megahertz or 100kHz, but also the time it takes for the transistor to turn on and off. So they're we're not talking about kilohertz or megahertz. We're talking about nanoseconds.

Is it two nanoseconds or is it 200 nanoseconds? Because the time that it takes for a transition transistor to go from on to off or off to on equates to switching losses, or at least it equates to the time where power isn't being transferred in the converter. So if we look at why GaN can go to higher frequency, it's because the losses and the times are shorter.

And that is this other meaning of fast switching. High DVDT high DIDT shorter time in the end. And you again can do this for a lot of reasons. The first and the biggest one I think is because it has no reverse recovery, no Qrr. This in a, in a hard switching topology, a motor drive or a buck or a boost converter is, I would say, the first reason why you end up lowering your frequency, because the Qr losses and the Qr radiated emissions of the ringing really problematic.

So you end up slowing down the switching, taking, you know, 200 nanoseconds instead of two nanoseconds to turn it on and off. And then because of that extra loss, you're going to go to a lower switching frequency for less loss. But the Qr isn't the complete story. There's also much lower Qss much lower Qg and the shape of those capacitance is over voltage is much flat, much more linear.

So you get these nice clean transitions whether you're switching fast or slow.

 

Host: So do you have to do this fast switching with GaN or can you tune this in some way?

 

Guest: Yeah of course. I mean as I mentioned you can switch at any frequency in that definition of fast, but also all these properties that I just mentioned, the low key and the, the lower and the more linear COSS these benefits you even or I would say maybe especially if you want to slow down the slew rate, slow down the DVDT and take a bit longer.

Hopefully you don't need to take 200 nanoseconds to turn on and off. Like I said, you probably need to take maybe 20. But if DVDT or, any kind of EMI considerations leads you to want to slow down and take 20 nanoseconds to turn it off again, GaN do this, I would say more effectively than a vertical MOSFET technology with silicon or silicon carbide, because the capacitance are very flat, because you don't have these variable charges in the minority carriers, the Qrr I mentioned.

So you can slow down to five volts per nanosecond or less with GaN and still get a lot of the same benefits, and still go to, yeah, somewhat of a higher frequency, not as much of a high frequency, you know, not megahertz if you're going to slow down the switching that much, but certainly in the hundreds of kilohertz.

 

Host: So if you're operating in these higher frequencies, what kind of special considerations do you have?

 

Guest: Yeah. So I mean for the higher frequency the main thing is, is magnetics design and your choice of capacitors. But I think it's more interesting to think about what what you have to consider to switch fast in terms of DVDT or, you know, fewer nanoseconds to turn on and off.

Because then you have not just DVDT but also did for DIVD, for DVDT, you need to manage your parasitic capacitance, everywhere in your board. This can lead to a lot of functional issues, breakdown of isolation, and, and just glitches. For did you need to manage your inductance. And in both cases, you largely have to take very good care of your gate driving circuit, the way that the components you use, as well as how you lay them out in your PCB and route them.

But the good news there is we have a lot of material on how to how to handle those challenges.

 

Host: So you mentioned gate driving and parasitic inductance. And these are great points. And I know that a lot of these are built into our GaN optimized ICS in our eice driver family.

 

Guest: Yeah. You know, we're coming out with a lot of great drivers, and have had a few already in the past few years.

But more coming out every, every day seems optimized for driving our, MV GaN, you know, in the 40 to 200V range and also our HV GaN, 650V. 900V. And, you know, these gate drivers don't have to drive GaN. They are also compatible with silicon and silicon carbide most of the time. But they include a lot of features that make sure that you get that GaN performance out of your transistor.

A lot of times when people ask me, can I use this gate driver, that gate driver with GaN, you know, because they've been using it for 20 years. With older technologies and I say you maybe could use it, but you may only get that same performance you've been getting for the past 20 years with that older technology, because those drivers are not meant for a fast switching transistor.

But I think even with the right gate driver. The parasitic inductance is. And the way you place everything can be a real challenge, which is where we have some upcoming webinars and this CoolGaN Tech Pro series that includes a lot of trainings within it. How to tackle these challenges.

 

Host: So let's talk about this idea of integrate GaN so this is an integrated GaN package with a driver and half bridge. How does this play into your frequency or your switching frequency. Calculations.

 

Guest: Yeah. They're not directly related. I think there is a, a conception in the industry that in integrated GaN is for high frequency, higher frequency than you would use regular discrete GaN transistors for or that you need integrated GaN to go to a certain frequency.

There's, there's an element of truth to it, the parasitic inductance that I mentioned in the PCB layout between the different components can be reduced if you put those components together in the same package or in, in the same chip. But if you follow the advice in the webinars that I mentioned and then in our other, you know, application notes and trainings, you can get good enough inductance in any board with discrete GaN and with GaN optimized gate drivers to achieve megahertz, multi megahertz frequencies.

But you might find that you have to make some compromises in that to meet other system considerations. The overall architecture of the board, the way you're cooling it, the capacitors you typically use. So with the integration this takes some of the guesswork out of it. It it reduces those. Inductance is inherently you still have to follow the PCB layout guidelines, because the way you connect the capacitors still matters.

And it can still impact ringing and have EMI issues. But it is a simple truth that the choice of integration is not, stemming from a need to go to higher frequency. There really two different motivations. Okay, so safe to say that there's no connection between GaN integration and switching frequency. Yeah. Like I said, not directly. So indirectly there is you know, I mentioned before at the beginning of the podcast that the main motivation for people going to higher frequency with GaN is to shrink the overall size of their system just to, like I said, to reduce the actuator and the the elbow of the robot or to reduce the the size of the

power conversion in the AI server rack So if you're trying to make something smaller, going into higher frequency helps. It allows you to shrink your magnetics or to shrink the amount of capacitors you use. But there's a number of other parts in that board, whatever that board is, that are going to take up space. Things like the gate driver, of course, could be quite large.

The isolated power supply or bootstrapping circuit, current sensing, temperature sensing protection circuits, short circuit protection alone can be a large functional block of your circuit that takes up a lot of space in your board. This is where integrated GaN can help. So if you're already using higher frequency with GaN to shrink your overall size, the integrated GaN can get you that last mile to the smallest size.

So actually brought a prop here to to show you this is a one kilowatt motor drive for a humanoid robot actuator. So this would supply a motor in a wrist or an elbow or a shoulder of a humanoid robot. And this can run at more than a kilowatt. It's so small for two reasons. One is that it's using integrated GaN, which has features like current sensing, protection, driving, bootstrapping, but also because it's running at a higher frequency, which reduces the amount of capacitors.

You see, it's not so many capacitors on the board at all. And the whole thing is the size of a US quarter or a two Euro coin.

 

Host: Okay. So if you're if you don't have access to the video for this podcast, you should know that this is really small and it is about the size of a coin and maybe even the thickness of a coin. And this could drive a one kilowatt motor.

 

Guest: Yeah, a little bit more. I mean probably it could go up to 1.5kW in a, in a transient case, if you imagine, you know, a humanoid robot lifting something by the shoulder, lifting a weight that's, I don't know, ten kilograms. This thing can, can really, pack some power.

And the power, the size of the power handling components, that's all. GaN this could be discrete components, and it would be the same. But the ability to fit in the driving and the sensing and the protection features, with virtually no increase to the size of the transistors. That is unique to the integrated GaN parts.

 

Host: Well, a big thank you for coming on today and sharing your GaN knowledge with us.

 

Guest: Well, you know, GaN knowledge is GaN power.

 

Host: And for our listeners, thanks for tuning in. Today I would ask you to subscribe to our podcast, if you haven't already, to get the latest episodes, and we'd like to hear from you if you have any ideas about topics for the future. So send your burning questions to podcast@infineon.com

Thank you and see you soon.