- Smart TV
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
Nov 17, 2026
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
Nov 17, 2026
Business & Financial Press
Nov 11, 2026
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
How module materials influence SiC performance and selection
Optimizing SiC module materials for performance and reliability
The right SiC module substrate and materials depend on the key application constraint. Selecting the appropriate materials for a SiC power module is essential for achieving the desired balance of efficiency, reliability, thermal performance, and cost. Several module materials and construction technologies influence thermal, electrical, and mechanical performance.
- Ceramic substrate: Supports the conductor structures, provides electrical insulation, and enables efficient heat transfer away from the semiconductor dies
- Heat-transfer path components: Heat flows through joining layers, copper structures, the module base or exposed substrate, the thermal interface material (TIM), and finally to the heatsink or cold plate
- Die-attach and top-side interconnection technologies: Die-attach and interconnection technologies affect heat flow, reliability, and power-module lifetime
- Package material stack: Temperature gradients and material differences create mechanical stress during load cycles, causing modules with similar semiconductor dies to perform differently under the same mission profile
- Additional package components: Housing materials, bond wires, pins and terminals, and the direct copper bonded (DCB) substrate also contribute to overall module performance and reliability
Material selection affects not only thermal conductivity but also temperature distribution, reliability, and power-cycling performance. The ceramic substrate, joining technologies, and package construction work together to determine how efficiently the heat generated by power losses is removed and how the module withstands thermal stress over time.
For example, using an AlN substrate material can help lower junction temperatures in high-power-density applications, while improved joining technologies can enhance resistance to temperature cycling and extend module lifetime. These material choices influence overall system efficiency, thermal margins, and long-term reliability
Key selection criteria include:
- Thermal performance: Substrate materials such as AlN and Al₂O₃ offer different levels of thermal conductivity. Higher thermal performance supports improved heat dissipation and power density
- Reliability and power cycling capability: Material and interconnection choices influence resistance to thermal cycling, mechanical stress, and long-term operation
- Electrical insulation and voltage requirements: The substrate must provide adequate insulation while supporting the required voltage class and operating conditions
- Package and interconnect technology: Die-attach materials, wire bonds, sintered connections, and advanced interconnects affect thermal behavior, electrical performance, and lifetime
- Mechanical robustness: Material selection should account for vibration, thermal expansion mismatch, and assembly-related stresses
- Cost and system-level value: A higher-performance material may increase module cost but reduce cooling requirements, improve efficiency, and enhance overall system performance
Selecting the right build-up material for a SiC module requires balancing thermal performance, reliability, manufacturability, and cost. The optimal choice depends on the application's power density, operating environment, cooling concept, and lifetime requirements.
Ceramic substrates provide electrical insulation between the semiconductor and the baseplate while transferring heat away from the SiC chips. Two commonly used substrate materials are aluminum oxide (Al₂O₃) and aluminum nitride (AlN). Al₂O₃ is widely used as it offers a good balance of performance and cost, while AlN provides significantly higher thermal conductivity for applications with demanding thermal requirements.
The choice becomes important when substrate heat transfer influences power cycling capability, junction temperature, or long-term reliability.
AlN is most beneficial when ceramic heat transfer limits output power, junction temperature, or reliability of the module, whereas Al₂O₃ may be sufficient when cooling margins are adequate and the main thermal bottleneck lies elsewhere in the system.
The evaluated AlN construction demonstrated improved power-cycling capability compared with the evaluated Al₂O₃ construction in EasyPACK™ CoolSiC™ MOSFET modules. However, substrate selection should not be based on power-cycling performance alone. Thermal requirements, cooling architecture, reliability targets, mechanical considerations, and system cost must also be evaluated when choosing between Al₂O₃ and AlN.
Validate the substrate decision with measured module data.
Module temperature up-and-down swing, known as thermal cycling, creates mechanical stress in joining layers and material interconnections. Higher power density can amplify these effects through larger temperature swings.
To improve cycling lifetime, select materials and package technologies that minimize thermal gradients and mechanical strain at critical interfaces. Evaluate ceramic substrates, joining technologies, and interconnection concepts together, particularly in demanding applications such as solar, energy storage, EV charging, UPS, and drives.
Discover how advanced joining and interconnection technologies help extend power-module lifetime under repetitive thermal cycling conditions.
Module materials and package design influence not only thermal performance but also how the power stage integrates with the PCB and cooling system. Pin construction affects assembly method and current transfer, while the package format affects mounting, available cooling area, and production integration. As a result, thermal performance cannot be separated from mechanical and electrical integration.
The following module families are optimized for different integration priorities:
Package construction can shift the thermal, mechanical, and assembly constraints of the design.
- Repeated temperature swings: These can load the die attach, topside connection, copper layers, and nearby material transitions. Increasing interface resistance can then raise operating temperature and accelerate additional degradation
- Damage to ceramic and bonded layer: The substrate carries electrical, thermal, and mechanical functions simultaneously. Mounting conditions and thermal distributions should therefore be evaluated at module level rather than inferred from a standalone ceramic property
- Poorly controlled thermal interface: These can increase junction temperature even when semiconductor losses have not changed. Designers should check mounting guidance, surface requirements, TIM application, and cooling-system consistency for the selected product
- Start with the application, not from the ceramic. Define voltage, topology, switching conditions, losses, cooling, insulation, environment, and lifetime expectations. Then identify which part of the module or cooling system prevents the design from meeting its target
- Evaluate power modules as complete solutions rather than comparing substrate materials alone. Product-specific thermal data, cycling results, and application guidance provide a better basis for selection than bulk material properties
- Choose AlN when it addresses a proven thermal or lifetime constraint. If the application already has sufficient thermal margin, Al₂O₃ remains a cost-effective and reliable option
Successful SiC module selection requires evaluating thermal performance, reliability requirements, package construction, and cooling architecture together. System-level analysis helps identify whether substrate material, joining technology, TIM, or package design is the primary constraint and ensures the chosen module delivers the required performance and lifetime.
1. Is AlN always better than Al₂O₃ for a SiC module?
No. AlN offers higher thermal conductivity, but the overall benefit depends on the complete thermal path. If other elements such as TIM or the cooling system dominate thermal resistance, the improvement may be limited.
2. How can engineers determine whether ceramic is the thermal bottleneck?
Use thermal modeling or direct measurements to compare junction temperatures before and after changing the substrate. If the temperature change is minimal, another part of the thermal path is likely to limit system performance.
3. Can a better performing TIM remove the need for an AlN substrate?
Not necessarily. A better-controlled interface may reduce case-to-heatsink resistance, while AlN addresses heat transfer through the ceramic construction. Either change may be more valuable depending on the dominant resistance. In demanding designs, both elements may require optimization as one thermal stack.
4. Why does power cycling matter when selecting module materials?
Power cycling repeatedly heats and cools the module, creating thermal and mechanical stress on material interfaces. Materials that reduce temperature gradients can improve reliability and extend module lifetime.
5. How do pins affect SiC module selection?
Pins affect PCB integration, assembly, and electrical connection of the module. Infineon’s Easy B-and C-Series and Econo material identifies PressFIT as an available connection technology, with different package constructions and integration concepts for each family.