- Complete system solutions for smart TVs
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
- FPGAs in datacenter applications
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
- Complete system solutions for smart TVs
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
Nov 17, 2026
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
Nov 17, 2026
Business & Financial Press
Nov 11, 2026
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
A gate driver converts a controller’s logic signal into the gate voltage and current that switch a power transistor on and off. What the driver must deliver depends on the transistor:
- Gate-voltage levels: the on-state and off-state gate voltages, and whether a negative off-state voltage is used.
- Threshold voltage: the lower the threshold, the smaller the margin against unwanted turn-on caused by noise or ground bounce.
- Gate charge and switching speed: how much current the driver must source and sink, and how fast the switch-node voltage changes.
- Short-circuit behaviour: how quickly a fault must be detected and how the switch must be turned off.
- Voltage class and isolation: whether a non-isolated, level-shift or galvanically isolated driver is needed.
Infineon EiceDRIVER™ gate driver ICs are designed to complement Infineon IGBT discretes and modules, silicon MOSFETs (CoolMOS™, OptiMOS™ and StrongIRFET™), CoolSiC™ silicon carbide MOSFETs and CoolGaN™ gallium nitride HEMTs.
In one sentence...
Each power-switch technology needs a gate driver matched to its gate-voltage range, threshold voltage, switching speed and short-circuit behaviour: IGBTs need robust short-circuit protection, SiC MOSFETs need fast, precisely timed drive with high CMTI and accurate DESAT, and GaN HEMTs need tightly controlled gate voltage and immunity to ground bounce.
Threshold values are approximate, typical values for each technology. UVLO examples are from specific Infineon drivers (1ED3010MC12I, 1ED3011MC12I and 1ED3012MC12I for MOSFET, IGBT and SiC). Always use the datasheets of the selected switch and driver.
Silicon MOSFETs cover a wide voltage range. Low-voltage OptiMOS™ and StrongIRFET™ MOSFETs (20 V to 300 V) are used in motor drives, battery-powered tools, light electric vehicles and DC-DC converters; StrongIRFET™ suits low switching frequencies below about 100 kHz and high current, while OptiMOS™ covers a broad frequency range. High-voltage CoolMOS™ superjunction MOSFETs are used in PFC stages, chargers, adapters, lighting, and server and telecom power supplies.
What the gate driver must provide:
- Enough source and sink current to move the gate quickly through the Miller plateau, where most switching loss arises. Low-side drivers such as 2EDN offer 4 A / 5 A per channel, and isolated 1EDi / 2EDi drivers 5 A / 9 A.
- A supply range that suits the gate: logic-level MOSFETs need drivers that operate from low supply voltages – the 2EDL6014AC, for example, works from 4 V to 16 V.
- A UVLO threshold matched to the MOSFET, so that it is never driven with too low a gate voltage. MOSFET versions of Infineon drivers use lower UVLO thresholds than IGBT or SiC versions.
- Short delays and good delay matching at high switching frequency, for example 20 ns propagation delay with 1 ns typical matching in the 2EDL6014AC.
- The right architecture: non-isolated low-side drivers for ground-referenced switches, level-shift half-bridge drivers (for example 650 V SOI drivers) for bridges, and isolated drivers where the converter stage needs galvanic isolation, for example in server power supplies.
IGBTs are used from 600 V to 1700 V in drives, solar inverters, UPS, EV charging and traction inverters. Their gate threshold is around 5 V, and Infineon IGBT families specify a short-circuit withstand time – typically 3 µs to 10 µs for discrete IGBTs. The gate driver therefore focuses on safe gate levels and fast, controlled fault handling:
- UVLO for IGBTs at around 10 V to 12 V, so the IGBT is never operated with insufficient gate voltage.
- Desaturation (DESAT) protection that detects a short circuit within the withstand time. A current source and a comparator monitor the collector-emitter voltage after turn-on; blanking and filter times prevent false trips.
- Controlled fault turn-off: two-level turn-off (TLTO) and soft-off lower the collector-emitter voltage overshoot when a short-circuit current is switched off.
- Short-circuit clamping, which limits the gate voltage that rises through the Miller capacitance during a short circuit.
- Active Miller clamp to prevent parasitic turn-on caused by high dV/dt.
- High output current for large IGBTs and modules: up to ±18 A in isolated drivers reduces the need for an external booster.
Short-circuit sensing with DESAT: the driver monitors the voltage across the switch after turn-on and reports a fault when it desaturates during a short circuit.
For lower-power drives, level-shift drivers such as the 1200 V 6ED2230S12T and 2ED132xS12M (with ±5% accurate overcurrent protection) are an alternative to isolated drivers where galvanic isolation is not required.
Silicon carbide MOSFETs such as CoolSiC™ (650 V, 1200 V and 1700 V) switch much faster than IGBTs and have very low switching losses. CoolSiC™ MOSFETs have a benchmark gate threshold of 4.5 V, a wide gate-source voltage range and fully controllable dV/dt; they can be turned off at 0 V and driven with silicon MOSFET drivers and driving schemes.
To use these advantages safely, Infineon recommends isolated gate drivers with the following features for ultra-fast switching of 650 V to 2000 V SiC MOSFETs:
- Tight propagation-delay matching and precise input filters, so deadtime can be short and timing predictable.
- A wide output-side supply range with negative gate-voltage capability.
- Extended common-mode transient immunity (CMTI) for the very fast switching edges.
- Active Miller clamp against parasitic turn-on.
- Fast and accurate DESAT protection to protect the SiC MOSFET in a short circuit.
Further points:
- UVLO optimised for SiC: higher thresholds than for IGBTs, for example 12.5 V / 13.6 V in the 1ED3012MC12I; the 1ED3145MC12H offers an adjustable UVLO.
- Slew-rate control: the 2L-SRC Compact family switches between two gate resistors to balance dv/dt (EMI) and switching losses.
- Isolated bias supply: the 2EP1xxR transformer drivers support the asymmetric output voltages often used for SiC.
For lower-power designs that do not need galvanic isolation, level-shift drivers such as the 1200 V 2ED132xS12M offer UVLO thresholds for both IGBTs and SiC MOSFETs.
With a single-ground driver (top), power current and gate current share a path; with a split-ground driver (bottom), the gate loop is decoupled from the shunt and stray inductance.
CoolGaN™ enhancement-mode HEMTs have low output charge and gate charge and no reverse-recovery charge. This enables very fast, nearly lossless switching, higher switching frequencies and new topologies such as the CCM totem-pole PFC. At the same time, GaN HEMTs have a low gate threshold of about 2.5 V, which leaves little margin against false turn-on.
What the gate driver must provide:
- Precise, limited gate voltage, for example a 5 V gate clamp, as offered for GaN driving in the 2EDL90xG3 family.
- Immunity to ground bounce: drivers with truly differential inputs (TDI), such as the 1EDN71x6 family, set the output state only from the voltage difference between their two inputs. This prevents false triggering from ground bounce in low-side applications and even allows high-side use, as long as the common-mode voltage stays below 150 V static and 200 V dynamic.
- Separate gate-current and power-current paths in motor drives: motor-drive boards have large ground loops. With a single-ground driver, the voltage drop across the shunt and stray inductance adds directly to the GaN gate-source voltage. Split-ground drivers such as the 2ED21064S06J decouple gate current from power current. Single-ground drivers remain suitable for designs with tight ground loops, such as SMPS or four-layer PCBs.
- Adjustable switching speed without external gate resistors (four driving strengths in the 1EDN71x6), an active Miller clamp and an optional negative charge pump for additional immunity against induced turn-on.
- Galvanic isolation where required: single-channel functional and reinforced isolated drivers are available for CoolGaN™ HEMTs.
Typical application of 1EDN71x6 drivers with truly differential inputs driving the high-side and low-side switches of a half-bridge.
- 1. Take the recommended on-state and off-state gate voltages, threshold, gate charge and short-circuit data from the switch datasheet.
- 2. Choose non-isolated, level-shift or galvanically isolated drive based on the topology and the system’s insulation requirements.
- 3. Choose a driver whose output-side supply range covers the gate voltages, including a negative off-state voltage if used.
- 4. Select a UVLO threshold that matches the switch technology (MOSFET, IGBT or SiC).
- 5. Check source and sink current, propagation delay and delay matching for the switching frequency and deadtime.
- 6. Check CMTI against the fastest switching edge and, for level-shift drivers, the negative VS rating.
- 7. Add the protection the switch needs: DESAT or OCP, soft-off or TLTO, Miller clamp, short-circuit clamping.
- 8. Plan layout and grounding – especially for GaN – and verify with double-pulse and application tests.
Next step
Find a driver for your switch with the Gate Driver Finder
Evaluate isolated drivers with Infineon power switches
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Can I use a MOSFET driver for a SiC MOSFET?
CoolSiC™ MOSFETs can be driven with silicon MOSFET driving schemes and turned off at 0 V. For fast, high-voltage SiC switching, however, drivers with SiC-specific UVLO, negative gate-voltage capability, high CMTI, Miller clamp and fast DESAT protection are recommended. Check both datasheets.
Why do SiC MOSFETs need a higher UVLO than IGBTs?
SiC MOSFETs need a sufficiently high gate voltage to reach their specified on-state performance, so SiC versions of Infineon drivers switch the output off at a higher supply voltage – for example 12.5 V / 13.6 V instead of 11.0 V / 12.0 V for IGBT versions.
Why are GaN HEMTs sensitive to ground bounce?
Their gate threshold is low – about 2.5 V – so a small voltage drop on a shared ground path can turn the device on unintentionally. Truly differential inputs and split-ground drivers address this.
What is DESAT protection for IGBTs?
The driver monitors the collector-emitter voltage after turn-on. If it rises because the IGBT leaves saturation during a short circuit, the driver turns the IGBT off within its short-circuit withstand time, often with soft-off or two-level turn-off.
Do GaN HEMTs always need an isolated driver?
No. Low-side, level-shift and TDI drivers are used for GaN HEMTs; isolated drivers are used when the stage needs galvanic isolation.
What is an active Miller clamp and which switches need it?
It holds the gate low through a low-impedance path while the switch is off, preventing parasitic turn-on caused by high dV/dt. It is especially relevant for fast-switching IGBTs and SiC MOSFETs and is also offered in GaN drivers.