New Infineon EiceDRIVER™ gate drivers for electric vehicle inverters boost power stage utilization at reduced bill of materials
New Infineon EiceDRIVER™ gate drivers for electric vehicle inverters boost power stage utilization at reduced bill of materials
Technology news
Munich, Germany – 3 June 2026 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) has introduced a new family of reinforced isolated gate-driver ICs for battery electric vehicle (BEV) traction inverters, EiceDRIVER™ 1EDI3040AS and 1EDI3041AS. The family supports both IGBTs and silicon carbide (SiC) MOSFETs, enables more usable performance from a given power stage than common solutions on the market, and integrates a comprehensive feature set into a single gate driver IC. This helps OEMs and Tier-1 suppliers to reduce the number of necessary external components and lowers the bill of materials (BOM) for the inverter control electronics.
“Infineon combines traction inverter system know how with a differentiating portfolio spanning OPTIREG™ PMICs, AURIX™ microcontrollers, EiceDRIVER gate drivers, and HybridPACK™ SiC modules at the power stage,” said Andreas Doll, Senior Vice President and General Manager Smart Power at Infineon. “Our deep expertise and extensive product range enable us to integrate key functions directly in the gate driver, allowing customers to achieve higher inverter efficiency and increased performance combined with more compact layouts and shorter design cycles.”
The new EiceDRIVER family features a multi-level slew rate control that enables precise switching during different driving conditions such as acceleration, cruising, and others. This allows to reduce inverter losses by up to 35 percent over drive cycles such as WLTP. Dynamic boost modes minimize dead times, further reducing losses and total harmonic distortion (THD). In addition, the 1EDI3040AS variant integrates a closed-loop flyback controller with 2 percent regulation that allows on-the-fly adjustment of the secondary supply (VCC2). This enables designers to adjust the gate supply for optimized efficiency and performance across operating conditions, lowering the SiC RDS(on) and increasing the peak current capability while reducing the number of external components.
Additional features include DESAT protection with digital filtering for sub-microsecond response times and power device state monitoring. An integrated SPI interface enables configuration and diagnostics, supported by a 6-channel 11-bit ADC. The devices are ISO 26262 ASIL-D-compliant and available in a compact PG-LFDSO-36 package.
To accelerate implementation, Infineon provides a comprehensive suite of design resources including safety documentation, application notes, simulation models, evaluation boards, a configuration tool, supporting software, as well as application examples. As a key component of Infineon's system offering for electric vehicle traction inverters, the new drivers help accelerate efficient, reliable powertrain designs.
Availability
The EiceDRIVER 1EDI304xAS isolated gate driver ICs for electric vehicles are now in production and will be showcased at PCIM as part of the traction inverter booth section. Further information is available at www.infineon.com/eicedriver-xev.
Infineon at PCIM Europe 2026
PCIM Europe will take place in Nuremberg, Germany, from 9 to 11 June 2026. Infineon will present its products and solutions for decarbonization and digitalization in hall 7, booth 470. For press inquiries, please contact media.relations@infineon.com. Industry analysts interested in a briefing can email MarketResearch.Relations@infineon.com. Information about Infineon’s PCIM 2026 show highlights is available at www.infineon.com/pcim.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
The new EiceDRIVER™ family integrates a comprehensive feature set into a single gate driver IC and enables more usable performance from a given power stage than common solutions.
JPEG
2126x2025 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : infatv202606-106