Character LCD with an I2C Interface (I2C LCD)
I2C LCD Component Simplifies 2x16 Character LCD Integration with I2C Interface
-
On this page
About
The I2C LCD component drives an I2C interfaced 2 line by 16 character LCD. The I2C LCD component is a wrapper around an I2C Master component and makes use of an existing I2C Master component. If a project does not already have an I2C Master component, one is required in order to operate. When one of the API functions is called, that function calls one or more of the I2C Master functions in order to communicate with the LCD.
The API enables communication on a 2-wire I2C bus and is compatible with the current character LCD component. A single component has the capability to drive one or more LCDs on the same I2C bus. Moreover, the I2C LCD component can coexist on an existing I2C bus if the PSoC serves as the I2C master, and it offers support for the NXP PCF2119x command format.
The I2C LCD component drives an I2C interfaced 2 line by 16 character LCD. The I2C LCD component is a wrapper around an I2C Master component and makes use of an existing I2C Master component. If a project does not already have an I2C Master component, one is required in order to operate. When one of the API functions is called, that function calls one or more of the I2C Master functions in order to communicate with the LCD.
The API enables communication on a 2-wire I2C bus and is compatible with the current character LCD component. A single component has the capability to drive one or more LCDs on the same I2C bus. Moreover, the I2C LCD component can coexist on an existing I2C bus if the PSoC serves as the I2C master, and it offers support for the NXP PCF2119x command format.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Design resources
Image gallery