Analog Net Constraint (Cy_Net_Constraint)
Analog signal routes with Analog Net Constraint
-
On this page
About
The Analog Net Constraint component allows you to define the route of the analog signal to which it is connected. This is an advanced feature that is not needed for most designs, and should be used with caution.
This function confines analog signal routing to a specific resource and mandates direct connection of all signal terminals to that routing resource.
Routing is strict. All of the devices connected to the net with the resource constraint must have a direct hardware connection to the resource. If the resources do not have a hardware connection to the specified constraint, an error will occur.
The Analog Net Constraint component allows you to define the route of the analog signal to which it is connected. This is an advanced feature that is not needed for most designs, and should be used with caution.
This function confines analog signal routing to a specific resource and mandates direct connection of all signal terminals to that routing resource.
Routing is strict. All of the devices connected to the net with the resource constraint must have a direct hardware connection to the resource. If the resources do not have a hardware connection to the specified constraint, an error will occur.