Infineon advances Powering AI roadmap with cutting-edge Battery Backup Unit (BBU) technology for AI data centers
Infineon advances Powering AI roadmap with cutting-edge Battery Backup Unit (BBU) technology for AI data centers
Business & Financial Press
- Next-generation Battery Backup Units for AI data centers underscore Infineon's commitment to setting new standards in powering AI
- Roadmap includes world's first 12 kW BBU
- Backup units deliver highly efficient, reliable, and scalable power conversion, achieving a power density up to 400 percent higher than industry average
Munich, Germany – 12 March 2025 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) has introduced its roadmap for next-level Battery Backup Unit (BBU) solutions for uninterrupted operations of AI data centers to avoid power outages and the risk of data losses. The comprehensive BBU roadmap includes power solutions from 4 kW up to the world’s first 12 kW battery backup unit. The BBU solutions are designed to deliver highly efficient, reliable, and scalable power conversion in AI server racks, and achieve a power density up to 400 percent higher compared to industry average. BBUs are essential for AI data centers to provide an uninterruptible power supply and furthermore protect sensitive AI hardware from voltage spikes, surges, and other power anomalies by filtering and conditioning the power that is supplied to the data center equipment. Combined with various best-in-class topologies enabling an increased ease-of-use for customers, the BBU solutions are bolstering Infineon’s leading position in the field of powering artificial intelligence.
“Ensuring an uninterrupted power supply to AI systems is critical for maintaining process continuity and seamless operation,” said Adam White, Division President Power & Sensor Systems at Infineon. “Our energy efficient battery backup units are designed to keep AI servers running smoothly with exceptional performance, flexibility, and efficiency catering to the diverse power levels required by AI servers. By mastering all three relevant semiconductor materials silicon (Si), silicon carbide (SiC), and gallium nitride (GaN) we are confident that Infineon semiconductor solutions will set a new standard in powering AI data centers.”
Downtime or system failures in AI data centers can be extraordinarily costly, with 41 percent of firms interviewed in an ITIC survey from 2024 indicating losses from $1 million to over $5 million per hour of downtime. 35 percent of these failures are attributed to issues with power component quality. To address this, Infineon’s Partial Power Converter (PPC), a semiconductor solution that focuses on improving performance and reliability of power supply systems, stands out as a leading technology for battery backup units.
The intermediate solution, represented by the 5.5 kW BBU, features an Infineon proprietary topology that integrates Si and GaN technologies providing ultra-high efficiency and high-power density. The industry-first 12 kW system combines several 4 kW power converter cards utilizing Infineon’s PSOC™ microcontrollers, 40 V and 80 V OptiMOS™ and EiceDRIVER™ Gate Drivers enabling unparalleled performance and flexibility, achieving a power density four times higher than industry average. Higher power levels can be attained by paralleling multiple cards on a motherboard, offering ease of scalability and simplified maintenance. If one card fails, the system continues to operate at a reduced capacity, minimizing downtime and ensuring high reliability. This modular approach allows the system to be tailored to specific power requirements without the need for a full system redesign creating substantial customer benefits in performance and reliability.
To further demonstrate the capabilities of the latest BBU technology, Infineon is developing full system demonstrators for its battery backup solutions. These demonstrators will showcase the advantages of the PPC technology in real-world applications offering a clear path forward for next-generation AI data centers.
Learn more about the Battery Backup Unit technology from Infineon at 2025 APEC (March 16-20). For further information, check out the BBU page.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Battery Backup Units
Infineon’s Battery Backup Units deliver highly efficient, reliable, and scalable power conversion in AI server racks, achieving a power density up to 400 percent higher compared to industry average.
JPEG
1280x720 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFPSS202503-076