A backdrop of natural surroundings features alongside several transmission towers.

We make power infrastructure future-proof

The age of electricity is here – and it demands advanced power infrastructure. As renewable energy scales up, robust power grids are vital to support energy-intensive applications such as AI data centers and modern industries. Infineon semiconductors help meet this need by enabling innovative solutions for optimized power use and grid stability.

Power infrastructure
Powering AI
Article

The future of energy depends on solving a critical equation: meeting the soaring power needs of AI data centers and modern industries while integrating more renewable energy into the grid. Semiconductors provide the intelligence that keeps power infrastructure reliable, efficient, and ready for the challenges ahead. 

When it comes to green energy, nature sets the pace! You flip the switch – the light goes on. Your electric car charges overnight. Data centers run non-stop, powering Artificial Intelligence and processing our data streams. And it takes a stable flow of electricity to keep all this working. The challenge grows more complex as the share of renewable energies in the power network increases: We have to stabilize the electric power grid with reliable semiconductor technology and scale it to meet the growing demands of energy-intensive applications. Infineon semiconductor solutions capture, channel and manage the unpredictable forces of nature – turning them into reliable, on-demand power. 

1,650 GW waiting to connect

In 2024, the International Energy Agency (IEA) tracked 1,650 GW of solar and wind projects in advanced stages - still waiting to be connected to the grid. A huge, missed opportunity for clean, cost-effective energy.

Source: IEA, Building the Future Transmission Grid (2025)

100,000 KM global HVDC lines

Since 2010, the global length of HVDC lines nearly tripled, now exceeding 100,000 km - with major growth in China, Brazil, and Europe. 100,000 km is equivalent to a network that could circle the Earth two and a half times.

Source: IEA, Building the Future Transmission Grid (2025)

Reliable, sustainable electricity is no longer a given. As renewables, electrification and rising energy demand reshape the grid, power infrastructure has to evolve in order to keep electricity flowing securely and efficiently.

Graphic HVDC

Challenge
Renewable energy sources are essential to achieving our climate goals. However, electricity generated by photovoltaics and wind power varies with the weather, the seasons and the time of day. As renewable energy makes up an ever-increasing part of the energy mix, future power grids have to be able to manage these fluctuations seamlessly, ensuring a reliable and resilient supply of electricity whenever and wherever it is needed.

Solution
Battery energy storage systems (BESS) bring stability and reliability. They unlock the full potential of renewables by balancing out fluctuations in the renewable energy mix, aligning supply and demand and preventing power outages. Semiconductor solutions from Infineon play a central role in many aspects of BESS – from power conversion and battery management to temperature control, safety and security. Grid-forming converters in wind turbines act as stabilizers within the energy grid. Grid-forming wind turbines can use power electronics to generate a stable frequency and maintain grid voltage, even when the load in the power grid changes. Infineon is advancing this technology with its highly efficient XHP™ 2 power modules.

Data Center

Challenge
Rising global electricity demand from AI data centers and modern industries requires smarter and more efficient grids. The traditional grid infrastructure – conventional transformers, protection systems and distribution – was not designed for fast-ramping, hyperscale AI demand. This results in bottlenecks in grid connection, power conversion capacity, reliability and fault protection.

Solution
Resolving this bottleneck requires semiconductor-driven innovation. Infineon's advanced power semiconductors enable next-generation solid-state transformers (SST) and solid-state circuit breakers (SSCB), delivering the efficiency, power density and reliability that modern AI data centers and industries need. Solid-state transformers are a key step in modernizing grid connections for AI-scale power demand. SSTs enable higher efficiency, less weight and more compact installations than conventional transformers do. SSTs provide a more flexible bridge between the grid and high-power electronic loads for data centers, battery energy storage, solar farms, EV charging and DC microgrids. Solid-state circuit breakers apply this principle to electrical protection by replacing the electromechanical circuit with semiconductor technology. SSCBs isolate faults within microseconds and without arcing, thereby improving the reliability and fault tolerance of the system in high-power environments.

Bidirectional Energy Flow

Challenge
Low-loss transmission of green electricity is crucial to the energy transition. Electricity is often generated far from where it is consumed, for example at an offshore wind farm. When this green electricity is transmitted over long distances, some of it is lost as heat due to resistance in the wires.

Solution
High-Voltage Direct Current (HVDC) transmits power over hundreds of kilometers with minimal power losses compared to alternating current (AC) systems. Increasing voltage makes it possible to decrease current, which in turn reduces the amount of energy lost as heat. Offshore and onshore converter stations turn AC into DC for the journey via underground, subsea cables or overhead lines and convert DC back to AC at the destination. HVDC offers several advantages such as reduced power loss, improved controllability and grid stabilization. A rough idea of the order of magnitude: More than 16,000 Infineon 6.5 kV IGBT modules can be installed in a single 2 GW HVDC project.

Private Green energy generation

Challenge
The traditional power grid was designed for a one-way flow of electricity—from large, centralized power plants to consumers. Today, millions of distributed assets are now both consuming and generating electricity; they create increasingly complex and bidirectional power flows which the grid has to handle across multiple voltage levels. For example, private green energy generation, like rooftop solar panels, is growing as we work towards energy independence. Surplus energy generated privately is fed back into the distribution grid.

Solution
Semiconductors are the key technology that enables intelligent, flexible and highly efficient management of these complex power flows. They make it possible to convert, control, monitor and protect electricity at every stage of the energy value chain. Intelligent technologies such as 3-phase hybrid solar inverters enable on-site storage capacities for privately generated power, thus contributing to grid stability.

Modern power infrastructure relies on high-performance semiconductors to create smarter, more efficient grids. Compared to conventional transformers and protection devices, high-performance semiconductors deliver higher energy efficiency, better power quality, faster response times, greater reliability and more compact designs. This helps power grids meet the growing demands of energy-intensive applications such as AI data centers.

Infineon solutions for solid-state transformers and solid-state circuit breakers

A solid-state transformer (SST) is an advanced, semiconductor-based power conversion device that replaces conventional copper and iron-based transformers. It delivers higher efficiency, significantly greater power density and improved scalability.

SSTs are up to 30 percent smaller and lighter than conventional transformers. SSTs are a key future technology that connects the public grid to energy-intensive and industrial applications such as AI data centers, while actively controlling voltage, power quality and energy flow.

SSTs enable direct power conversion from the medium-voltage levels supplied by the grid to the low voltages required by applications such as AI data centers, electric vehicle (EV) charging infrastructure, renewable energy systems and industrial microgrids.

A semiconductor circuit breaker (SSCB), or solid-state circuit breaker, protects electrical circuits from excessive current flow such as short circuits and overloads.

Unlike traditional electromechanical breakers that rely on mechanical parts, operating on the millisecond scale, SSCBs use semiconductor components and smart protection algorithms to interrupt current in microseconds—up to 1,000 times faster.

This capability is essential for DC grids and significantly improves protection and system availability in applications such as industrial manufacturing and AI data centers, where even brief delays can cause costly downtime, data loss and hardware damage.

CoolSiC™ MOSFET EasyPACK™ modules with .XT

Gain deeper insights:

CoolSiC™ JFET technology

Gain deeper insights:

The electricity grid of the future will have to do more than just deliver electricity. It will have to predict and compensate for power fluctuations, protect against unexpected overloads and communicate in real time. Hidden in the background, yet essential, semiconductors ensure that energy gets where it is needed. Infineon is driving this development forward with innovative technology at all voltage levels.

Infineon semiconductor solutions infographic showing 6 key applications to enable sustainable energy systems, grid reliability and optimize power infrastructure

Why is power infrastructure becoming such a critical topic now?

Electricity is becoming the foundation of modern life and industry. At the same time, renewable energy sources such as photovoltaic and wind power are becoming a larger part of the electricity mix. Unlike conventional power generation, renewable energy depends on weather conditions, which makes electricity generation more variable and less predictable. Modern power grids will therefore have to be smarter, more flexible, and more resilient in order to balance supply and demand in real time. A resilient grid helps ensure a stable and reliable power supply, even when generation and consumption patterns change rapidly.

What role do semiconductors play in modern power infrastructure with more renewable energy?

Semiconductors are the invisible technology behind the generation, conversion, transmission, distribution and use of electricity. They help control the flow of power, ensuring that energy is delivered efficiently and safely where it is needed. This is especially important given the growing share of renewables: Renewable energy sources such as photovoltaic and wind power deliver green electricity, but their output fluctuates depending on weather and time of day. Semiconductors enable advanced power electronics that help stabilize the power grid by supporting technologies such as battery energy storage systems that balance supply and demand, and grid-forming inverters, which stabilize voltage and frequency throughout the grid.

How do semiconductors improve energy efficiency?

Electrical energy typically undergoes multiple AC/DC and DC/DC conversion stages before reaching the end application. Every conversion stage introduces loss in terms of conduction and switching that impact overall system efficiency. Advanced power semiconductors reduce these losses through lower on-resistance, faster switching characteristics and improved thermal performance. Wide-bandgap technologies such as Silicon Carbide (SiC) and Gallium Nitride (GaN) further increase efficiency by enabling higher switching frequencies and operating temperatures. This not only reduces energy losses but also decreases cooling requirements, lowers system size, and improves overall power density.

What are solid-state transformers and why do they matter?

Solid-state transformers represent a new generation of grid technology that replaces traditional transformer functions with advanced power electronics. They can be smaller, lighter, more efficient and more flexible than conventional transformers. SSTs make power distribution more intelligent and more adaptable, helping prepare grids for future energy demands. SSTs are expected to become key building blocks in future applications including renewable energy integration, fast EV charging hubs, battery energy storage systems, and high-power AI infrastructure.

What are solid-state circuit breakers and how do they improve reliability?

Traditional circuit breakers rely on mechanical components to interrupt fault currents. Solid-state circuit breakers use semiconductor technology to react much faster, isolating faults in microseconds. This rapid response helps protect critical equipment, reduce downtime, and improve overall system resilience. In addition, they enable advanced monitoring, diagnostics and digital control capabilities. These smart protection systems are becoming increasingly important as power networks become more complex.

Which semiconductor technologies are important for future power infrastructures?

Silicon remains the dominant semiconductor technology for many applications, but wide-bandgap materials are increasingly driving next-generation power systems. Silicon Carbide (SiC) offers superior performance in high-voltage and high-power environments by reducing switching loss and enabling operation at higher temperatures. Gallium Nitride (GaN) excels in high-frequency applications requiring maximum power density and efficiency. Together, these technologies enable smaller passive components, simplified thermal management and significantly improved system performance. As power infrastructure continues to evolve, the combination of silicon, SiC and GaN will optimize performance across a wide range of voltage and power classes.

With the industry’s broadest power device portfolio and many years of expertise in all relevant power technologies such as silicon, silicon carbide, and gallium nitride we stand for design flexibility and leading application know-how along the entire power conversion chain.