Device Driver & Libraries
HX3 USB 3.0 Hub Controllers: USB-IF Compliance and Firmware Updates
-
On this page
Browse by category
AIROC™ Wi-Fi & Bluetooth EZ-Serial Module Firmware Platform
Learn all about our AIROC™ solutions
AIROC™ Wi-Fi & Bluetooth Linux and Android Drivers
Proprietary and Open Source Linux Support Models for Enhanced Connectivity
emWin Graphics Library and GUI for PSOC™
emWin is an embedded graphic library and graphical user interface (GUI) framework
Infineon Complex Device Driver for Battery Management Systems
Discover Infineon's Complex Device Drivers for Battery Management Systems
Infineon Complex Device Driver for Battery Management Systems Subfamilies
Memory Solutions Hub
All the necessary building blocks to successfully integrate Infineon memory products
PSOC™ 6 Peripheral Driver Library (PDL) for PSOC™ Creator
The Peripheral Driver Library (PDL) simplifies software development for the PSOC™ 6 MCU architecture.
USB Controllers EZ-USB™ GX3 Software and Drivers
Efficient GX3 Integration: Enhanced Drivers for Various OSs
About
HX3 Rev. *C and *D silicon of USB 3.0 Hub Controllers passes USB-IF compliance (TID#330000060) with internal ROM firmware. Customers can save BOM by eliminating the EEPROM. Customers using Rev. *C Silicon and choosing to boot from an external EEPROM must use the Version B5 or B7 firmware. Customers using Rev. *D Silicon and choosing to boot from an external EEPROM must use the Version B7 firmware.
The method of identification of the HX3 Rev *D Silicon and earlier Silicon is included in the Version B7 - Release Notes.
Version B5 or B7 should not be used with the HX3 Rev *A Silicon. To pass USB-IF certification with Rev *A Silicon, customers are required to use Infineon Version B3 firmware.
All versions of HX3 firmware needs to be downloaded to HX3 using either an I2C EEPROM or an external I2C master. If an external EEPROM is used, Cypress provided Blaster Plus software tool can be used to program the EEPROM. Procedure to download firmware to EEPROM is provided at - Downloading Firmware for HX3 - KBA91657.
HX3 Rev. *C and *D silicon of USB 3.0 Hub Controllers passes USB-IF compliance (TID#330000060) with internal ROM firmware. Customers can save BOM by eliminating the EEPROM. Customers using Rev. *C Silicon and choosing to boot from an external EEPROM must use the Version B5 or B7 firmware. Customers using Rev. *D Silicon and choosing to boot from an external EEPROM must use the Version B7 firmware.
The method of identification of the HX3 Rev *D Silicon and earlier Silicon is included in the Version B7 - Release Notes.
Version B5 or B7 should not be used with the HX3 Rev *A Silicon. To pass USB-IF certification with Rev *A Silicon, customers are required to use Infineon Version B3 firmware.
All versions of HX3 firmware needs to be downloaded to HX3 using either an I2C EEPROM or an external I2C master. If an external EEPROM is used, Cypress provided Blaster Plus software tool can be used to program the EEPROM. Procedure to download firmware to EEPROM is provided at - Downloading Firmware for HX3 - KBA91657.