Analog Multiplexer (AMux)
Enhanced Analog Multiplexing: The AMux Component's Versatile Functionality
-
On this page
About
The analog multiplexer (AMux) component can be used to connect none, one, or more analog signals to a different common analog signal. The ability to connect more than one analog signal at a time provides cross-bar switch support, which is an extension beyond traditional mux functionality.
- Single or differential connections
- Adjustable between 1 and 64 connections for single AMux, 1 and 32 connections for Differential AMux.
- Software controlled
- Connections may be pins or internal sources
- Multiple simultaneous connections
- Bi-directional (passive)
The analog multiplexer (AMux) component can be used to connect none, one, or more analog signals to a different common analog signal. The ability to connect more than one analog signal at a time provides cross-bar switch support, which is an extension beyond traditional mux functionality.
- Single or differential connections
- Adjustable between 1 and 64 connections for single AMux, 1 and 32 connections for Differential AMux.
- Software controlled
- Connections may be pins or internal sources
- Multiple simultaneous connections
- Bi-directional (passive)