Infineon to revolutionize power delivery architecture for future AI server racks with NVIDIA
Infineon to revolutionize power delivery architecture for future AI server racks with NVIDIA
Business & Financial Press
- Infineon collaborates with NVIDIA for industry-first 800 V power delivery architecture for AI data centers
- New high-voltage direct current (HVDC) distribution ensures reliable and even more efficient power delivery for future AI server racks
- Infineon aims to create new power delivery standards for AI data centers
Munich, Germany and Santa Clara, CA – 20 May 2025 Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is revolutionizing the power delivery architecture required for future AI data centers. In collaboration with NVIDIA, Infineon is developing the next generation of power systems based on a new architecture with central power generation of 800 V high-voltage direct current (HVDC). The new system architecture significantly increases energy-efficient power distribution across the data center and allows power conversion directly at the AI chip (Graphic Processing Unit, GPU) within the server board. Infineon’s expertise in power conversion solutions from grid to core based on all relevant semiconductor materials silicon (Si), silicon carbide (SiC) and gallium nitride (GaN) is accelerating the roadmap to a full scale HVDC architecture.
This revolutionary step paves the way for the implementation of advanced power delivery architectures in accelerated computing data centers and will further enhance reliability and efficiency. As AI data centers already are going beyond 100,000 individual GPUs, the need for more efficient power delivery is becoming increasingly important. AI data centers will require power outputs of one megawatt (MW) and more per IT rack before the end of the decade. Therefore, the HVDC architecture coupled with high-density multiphase solutions will set a new standard for the industry, driving the development of high-quality components and power distribution systems.
“Infineon is driving innovation in artificial intelligence,” said Adam White, Division President Power & Sensor Systems at Infineon. “The combination of Infineon's application and system know-how in powering AI from grid to core, combined with NVIDIA’s world-leading expertise in accelerated computing, paves the way for a new standard for power architecture in AI data centers to enable faster, more efficient and scalable AI infrastructure.”
"The new 800V HVDC system architecture delivers high reliability, energy-efficient power distribution across the data center,” said Gabriele Gorla, vice president of system engineering at NVIDIA. “Through this innovative approach, NVIDIA is able to optimize the energy consumption of our advanced AI infrastructure, which supports our commitment to sustainability while also delivering the performance and scalability required for the next generation of AI workloads.”
At present, the power supply in AI data centers is decentralized. This means that the AI chips are supplied with power by a large number of power supply units (PSU). The future system architecture will be centralized, making the best possible use of the constraint space in a server rack. This will increase the importance of leading-edge power semiconductor solutions using fewest power conversion stages and allowing upgrades to even higher distribution voltages.
Infineon is a leader in power semiconductor solutions and systems integration. The company expects the proportion of power semiconductors in a centralized HVDC architecture to be similar or higher than in today's AC distribution architecture. Additionally, to the scaling of the HVDC power architecture, Infineon continues to support state of the art DCDC multiphase solutions and intermediate architectures for hyperscalers and AI data center operators with a broad product portfolio based on all relevant semiconductor materials along the entire power flow.
Learn more about Infineon’s AI power and data center solutions here.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Servers in data center
Infineon to revolutionise power delivery architecture for future AI server racks with NVIDIA
JPEG
4600x2400 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFXX202505-107
Michael Burner
Spokesperson Consumer, Compute and Communication, PSS Division
+49 89 234 39300