Infineon launches industry‑first TLVR quad‑phase module exceeding 2 A/mm² for next‑generation AI compute

Technology news

Mar 26, 2026

Munich, Germany – 26 March 2026 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) unveils a high‑current‑density quad‑phase power module with TLVR (trans‑inductor voltage regulator) inductors to meet the power demand of advanced AI data centers. The TDM24745T is a new OptiMOS™ quad‑phase power module designed to meet the rapidly growing power requirements of next‑generation AI accelerators. Integrating four power stages, a TLVR inductor and decoupling capacitors into a compact 9 x 10 x 5 mm³ package. The module delivers industry‑leading current density exceeding 2 A/mm². This combination enables exceptional transient performance and supports the high‑current core rails required by advanced GPU and AI processors, in lateral as well as vertical power delivery configurations.
 
“As AI workloads scale at unprecedented speed, the need for highly efficient and extremely compact power delivery has never been greater,” said Athar Zaidi, Senior Vice President and General Manager Power ICs and Connectivity, at Infineon. “With the TDM24745T, we are redefining what is possible in high‑current voltage regulation. By combining industry‑leading current density with TLVR technology in an exceptionally small footprint, we enable our customers to unlock more compute performance, reduce energy consumption, and accelerate the deployment of next‑generation AI data centers.”
 
As the power requirements of AI data centers continue to rise, power architectures must become more compact, responsive and efficient. The TDM24745T addresses these challenges by simplifying power architecture design, enabling higher power density to free up PCB space for additional compute resources, and delivering an extremely fast transient response. The TLVR architecture can also reduce the required output capacitance by up to 50 percent, helping system designers achieve more efficient, space‑saving layouts that directly contribute to energy savings and improved TCO across AI server platforms.
 
As the industry’s first TLVR quad‑phase module in this compact form factor, the TDM24745T offers up to 320 A peak current capability, making it especially well-suited for next‑generation AI processors and high‑current multiprocessor platforms. Combined with Infineon’s digital multiphase controllers, the module supports flexible and scalable architectures that accelerate system deployment in fast‑evolving AI environments. Powered by OptiMOS‑6 MOSFET technology, chip‑embedded integration and proprietary magnetics, it delivers improved efficiency and thermal performance even in the densest AI server designs, contributing to the development of more energy efficient AI factories.
 
The TDM24745T power module integrates seamlessly into Infineon’s end‑to‑end AI server power delivery ecosystem, which spans everything from the grid interface to the core processor rails. Leveraging the combined benefits of silicon (Si), silicon carbide (SiC) and gallium nitride (GaN) technologies, Infineon offers a comprehensive and scalable approach to achieving the highest efficiency, robustness and power density for AI‑optimized data center architectures. 
 
Availability
Further information is available at TDM24745T OptiMOS quad-phase power module 
 
Infineon AI Day Taiwan
The Infineon We Power AI Day is an industry event for business and technology leaders in Taiwan. Together with our ecosystem partners and customers, we explore the latest advances in the field of power technologies. The goal is a sustainable AI infrastructure enabled by Infineon’s innovative solutions – from grid to core. The event will take place in Taipei on March 31.

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 57,000 employees worldwide (end of September 2025) and generated revenue of about €14.7 billion in the 2025 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

 

Follow us: Facebook - LinkedIn

Press Photos

As the industry’s first TLVR quad‑phase module in this compact form factor, the Infineon TDM24745T power module offers up to 320 A peak current capability.

JPEG

2126x1196 px

Download

Information Number : infpss202603-076

avatar

Michael Burner

Spokesperson Power Systems Division (PS)

+49 89 234 39300

Send email