Infineon launches new radiation hardened GaN transistors, including one of the first DLA JANS certified GaN device
Infineon launches new radiation hardened GaN transistors, including one of the first DLA JANS certified GaN device
Technology news
Munich, Germany – 29 May 2025 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced the first of a new family of radiation hardened Gallium Nitride (GaN) transistors, fabricated at Infineon’s own foundry, based on its proven CoolGan™ technology. Designed to operate in harsh space environments, the company’s new product is the first in-house manufactured GaN transistor to earn the highest quality certification of reliability assigned by the United States Defense Logistics Agency (DLA) to the Joint Army Navy Space (JANS) Specification MIL-PRF-19500/794.
The new radiation hardened GaN High Electron Mobility Transistor (HEMT) devices are engineered for mission-critical applications required in on-orbit space vehicles, manned space exploration, and deep space probes. Combining the robust performance of GaN HEMTs with Infineon 50+ years of experience in high reliability applications, the new power transistors deliver best-in-class efficiency, thermal management and power density for smaller, lighter, and more reliable space designs. The devices complement Infineon’s proven legacy radiation hardened silicon MOSFET portfolio, providing customers with access to a full catalog of power solutions for space applications.
“The Infineon team continues to push the limits of power design with our new GaN transistor line,” said Chris Opoczynski, Senior Vice President and General Manager HiRel, at Infineon. “This milestone brings the next-generation of high reliability power solutions for mission-critical defense and space applications that utilize the superior material properties of wide bandgap semiconductors to customers serving the growing aerospace market.”
The first three product variations in the new radiation hardened GaN transistor line are 100 V, 52 A devices featuring an industry leading (R DS(on) (drain source on resistance) of 4 mΩ (typical) and total gate charge (Qg) of 8.8 nC (typical). Encased in robust hermetically sealed ceramic surface mount packages, the transistors are Single Event Effect (SEE) hardened up to LET (GaN) = 70 MeV.cm2/mg (Au ion). Two devices, which are not JANS certified, are screened to a Total Ionizing Dose (TID) of 100 krad and 500 krad. The third device, screened to 500 krad TID, is qualified to the rigorous JANS Specification MIL-PRF-19500/794.
Infineon is the first company in the industry to achieve the DLA JANS certification for fully internally manufactured GaN power devices. DLA JANS certification requires rigorous levels of screening and Quality of Service Class Identifiers to ensure the performance, quality, and reliability required for space flight applications - making Infineon a leader in GaN for high reliability applications. Infineon is also running multiple lots prior to full JANS production release to ensure long term manufacturing reliability.
Availability
Engineering samples and evaluation boards are available immediately with the final JANS device being released in the summer of 2025. Additional JANS parts are launching soon, expanding available voltages and currents to enable customers greater flexibility in creating efficient and reliable designs. For more information, visit www.infineon.com/radhardgan
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
HiRel space satellite
The rad hard GaN transistors from Infineon are engineered for mission-critical applications required in on-orbit space vehicles, manned space exploration, and deep space probes.
JPEG
1480x1500 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFPSS202505-111