Infineon PSOC™ Edge E8x microcontrollers are the first devices designed to meet the new PSA Level 4 certification requirements

Technology news

Apr 10, 2024

Munich, Germany– 10 April 2024 – With embedded security considered to be a vital aspect in deployment of Internet of Things (IoT) applications, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced that its new PSOC™ Edge E8x MCU product family has been designed to meet the highest certification level provided by the Platform Security Architecture (PSA) Certified program, a framework for embedded security. The PSA Certified Level 4 device certification is targeted by implementing an on-chip, hardware-isolated enclave that provides secured boot, key storage and crypto operations in all PSOC Edge E8x devices.  

“By aspiring to achieve this robust embedded security certification, IoT designers for edge applications such as wearables and smart home applications can be confident their products can achieve highest levels of security,” said Erik Wood, Senior Director Product Security for IoT, Computer and Wireless business, Infineon Technologies. “Integrating hardware security on the MCU also unlocks new edge computing markets such as printers and payment terminals that previously required discrete security chips. As a security leader, we are committed to enabling designers to reach the highest level of security for all applications.”

PSA Certified is a security framework established by Arm and industry partners in 2019. It provides both design guidelines and independent security evaluations through third-party labs intended to assure that all connected devices are built upon a Root of Trust. PSA Certified certifications achieved by an MCU extend through the value chain, allowing device builders and application providers to reuse that certification as they deploy products in the field. 

“Connected device security is critical to scaling IoT deployments, and something that Arm and its ecosystem is committed to continuing to drive through initiatives like PSA Certified,” said David Maidment, Senior Director, Secure Devices Ecosystem at Arm. “We applaud Infineon’s ongoing commitment to robust device security by striving to achieve PSA Certified Level 4 iSE/SE for its new family of MCUs.”  

About the PSoC Edge Family

Infineon’s new PSOC Edge E81, E83 and E84 microcontrollers are based on the high-performance Arm Cortex®-M55, including Helium™ DSP support paired with Arm Ethos™-U55, and Cortex-M33 paired with Infineon’s ultra-low power NNLite — a proprietary hardware accelerator intended to accelerate neural networks. Optimized for machine-learning applications running on connected systems at the Internet edge, the fully-integrated system-on-chip devices allow designers to bring advanced artificial intelligence functionality to IoT and consumer applications.

As with all Infineon MCUs, the series is supported by Infineon’s ModusToolbox™ software platform, which provides a collection of development tools, libraries, and embedded runtime assets for a flexible and comprehensive development experience. ModusToolbox supports a wide range of use cases including consumer IoT, industrial, smart home, wearables, and many other applications.

Infineon at Embedded World

Embedded World will take place in Nuremberg, Germany, from 9 to 11 April 2024. Infineon will present its products and solutions for decarbonization and digitalization in hall 4A, booth #138 and virtually. Company representatives will also hold several TechTalks as well as presentations at the accompanying Embedded World Conference, followed by discussions with the speakers. If you are interested in interviewing an expert at the show, please email media.relations@infineon.com . Industry analysts interested in a briefing can email MarketResearch.Relations@infineon.com . Information about the Embedded World show highlights is available at www.infineon.com/embedded-world.

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Follow us: X - Facebook - LinkedIn

Press Photos

PSOC™ Edge

PSOC™ Edge

Infineon PSOC™ Edge E8x microcontrollers are the first devices designed to meet the new PSA Level 4 certification requirements

PNG

1547x1249 px

Download

Information Number : INFCSS202404-092

avatar

Veronika Seifried

Spokesperson Power Systems Division (PS)

+49 89 234 61662

Send email