Transparency and object identity: Infineon and DIGISEQ develop secured physical asset verification to provide end-to-end brand protection
Joint press release of DIGISEQ and Infineon Technologies AG
Munich, Germany – 1. February 2021 – In a joint project, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and DIGISEQ, an IoT platform provider with end-to-end service, utilize SECORA™ Blockchain NFC technology to deliver secured identity data. This advanced solution connects the digital data recorded on blockchain to the physical item, allowing for comprehensive verification of the identity of items – eliminating the challenge of product substitution and heightening supply chain transparency.
“DIGISEQ is the ideal partner to develop an end-to-end brand protection solution based on Infineon’s SECORA Blockchain. Our partner is experienced in providing secured end-to-end services and is a centerpiece between banks, product creators, and chip manufacturers”, said Maurizio Skerlj, Vice President and Product Line Head of Infineon’s Identity Solutions. “With counterfeit and pirated products on the rise brand protection has never been more important to enable economic growth of legitimate businesses as well as public health and safety. Our hardware-based SECORA Blockchain gives products a digital identity and blockchain makes it visible.”
In the report “Trends in Trade in Counterfeit and Pirated Goods”* from 2019, the Organization for Economic Co-operation and Development (OECD) and the EU Intellectual Property Office (EUIPO) stated that the industries most negatively impacted by counterfeiting activities are consumer goods, business-to-business products, IT goods and luxury items. The report shows that in 2016, imports of counterfeit and pirated products into the EU amounted to as much as 121 billion Euro (134 billion US-Dollar) representing 6.8 percent of EU imports, as compared to 5 percent in 2013. SECORA Blockchain with secured physical asset verification offers a promising anti-counterfeit solution that seeks to alleviate this trend and boost transparency in affected markets.
Reliable and secured verification of the digital identity
Today, blockchain is already used to provide a mechanism to prove the provenance of scarce or limited-edition goods. However, such processes often rely upon the public trust in the manufacturer and third-party handlers of a product. Even when vetting processes are put in place to clear contributors, sources for blockchain data are often dependent on data carriers like QR codes, which can be highly prone to replication or fraud. It is challenging to check if no substitution of the good occurred at any point of transfer, or if the object is truthfully as scarce as it is claimed to be.
Infineon’s and DIGISEQ’s joint project puts forth a powerful proposition that binds the physical item to its digital identity and footprint, allowing an instantaneous authentication system to determine the validity of goods throughout their lifetimes. SECORA Blockchain enables the connection between the physical item and the blockchain, which enhances blockchain setups.
The SECORA Blockchain device contains a crypto enabled NFC chip. It can effectively store the private key to sign transactions on the blockchain. Such a security controller is able to protect secret keys from logical and physical attacks, allowing to protect the system from unauthorized data. As project partner, DIGISEQ will provide the system with over-the-internet data-delivery capability. It allows unique secured identity data to be delivered into the chips that are physically embedded into the individual items. Item-level data will be configured to flow into the blockchain ledger automatically. This will work hand-in-hand with blockchain technology, which allows for transaction and exchange data to be encrypted and securely stored within a ledger through the item lifetime.
* OECD/EUIPO (2019), Trends in Trade in Counterfeit and Pirated Goods, Illicit Trade, OECD Publishing, Paris, https://doi.org/10.1787/g2g9f533-en
About DIGISEQ
DIGISEQ is an award-winning IoT platform that provides an end-to-end service which securely delivers data into everyday wearables, enabling items – from rings to bracelets – to have NFC payment, Access Control, Digital Identity and User Engagement contactless functionality. We connect an entire ecosystem, serving as a centerpiece between banks, product creators, retailers, chip manufacturers and service providers. Our platform offers businesses a seamless all-in-one solution for entering the wearable technology market, empowering them with our existing infrastructure, partners, hardware and security systems to create wearable technology. As pioneers and market leaders of passive wearable payment technology, we aim to be the world's largest issuing network.
More information is available at www.digiseq.co.uk.
Information Number
INFCSS202102-032
Press Photos
-
Based on SECORA™ Blockchain NFC technology, Infineon’s and DIGISEQ’s joint project puts forth a powerful proposition that binds the physical item to its digital identity and footprint, allowing an instantaneous authentication system to determine the validity of goods throughout their lifetimes.SECORA_Blockchain_Brand_ProtectionJPG | 492 kb | 2126 x 1535 px