Facility level power conversion: SST
We’re bringing you the latest from the world of semiconductors – straight to your ears! From quick takes on trending applications to deep dives on product innovations, our experts give you their take on the tech behind the tech.
Jul 14, 2026
In this episode of Podcast4Engineers, host Peter Balint speaks with Valerio Zerillo about the growing role of Solid-State Transformers (SSTs) in powering AI-driven data centers. The discussion explores how traditional low-frequency transformers are reaching their limits due to increasing power demands, space constraints, and scalability challenges. Valerio explains how SSTs leverage advanced power semiconductors, silicon carbide, gallium nitride technologies, and intelligent control systems to deliver higher efficiency, flexibility, and reduced footprint. The episode also looks ahead to the future of power infrastructure, including medium-voltage DC grids and the integration of renewable energy sources to support next-generation AI and high-power applications.
In this episode of the Podcast4Engineers, host Peter Balint speaks with Valerio Zerillo, Global Application Manager at Infineon.
Host:
Peter Balint has shaped visual and audio narratives at Infineon since 2021. He’s a video producer with 20 years of experience and has produced podcasts for the past 10 years. Over his career, Peter has interviewed speakers from all over Europe, bringing high-quality media production and engaging conversations to the forefront of his work.
Guest:
Valerio Zerillo is Global Application Manager for Solid-State Transformers and UPS at Infineon Technologies, with 15+ years in power electronics, critical infrastructure, and B2B product management. Formerly at Vertiv and Emerson, he led UPS innovation and efficiency programs. He holds an MSc in Electronics Engineering from the University of Bologna, with research at Linköping University.
More episodes
Full transcript
Guest: This 3000 kg single megawatt transformer can be immediately replaced by lightweight power semiconductors surrounded by gate drivers, sensors, and microcontrollers.
Host: Hello and thanks for joining this episode of Podcast4Engineers. It's the podcast you just have to listen to if you're interested in what's going on in the semiconductor market. I'm your host, Peter Balint, and today we continue with our We Power AI series. And today we look at facility-level power conversion. And we are specifically talking about the SST or solid-state transformer. And today we're joined by Valerio Zerillo. He's the global application manager for solid-state transformers and UPS. Thank you for joining us today.
Guest: Thank you, Peter, for having me.
Host: First question I have is let's look at the way things are done today. We've been using for a long time the low-frequency transformer for power conversion. To me, it seems like this could maybe be inefficient, definitely bulky. What now is prompting this change to something like solid-state?
Guest: That's a good point. Low frequency transformers have been used in decades by many industries, including data centers. They have been very reliable, available, and actually also pretty efficient in the way they connect the end loads to the grid infrastructure on the medium voltage. side. However, the recent increase in the power demand driven by the AI workloads has put this technology to its limits, specifically when it comes to space utilization, weight, and flexibility. Just to give you a reference, a 1 megawatt low frequency transformer working at 50 or 60 Hz in terms of operating frequency typically includes a large amount of copper or aluminum and iron. And for a 1 megawatt system, typically we are considering about 3000 kilograms of weight for this system. And if you put this into perspective and you multiply the amount of transformers you may need to power a 1 gigawatt data center, you may need 1000 of these large systems. We see, we find actually that solid-state transformers are a better way to solve this power connection challenge. And the reason is this 3000 kg single megawatt transformer can be immediately replaced by lightweight power semiconductors surrounded by gate drivers, sensors, and microcontrollers to make it as reliable as the low frequency transformers, as efficient, as them and more flexible when it comes to space utilization, weight, and scalability.
Host: Okay, so you say they can't keep up with the common needs as of today. Is this recently since this whole wave of AI usage, or has this been going on for a while?
Guest: Let's say the challenges on the traditional technologies like line frequency or low frequency transformers have been in place since a few years now, but it's really the rapid evolution of the AI data center power demand that is pushing to the limits of these applications. We have been seeing, actually we are seeing today a large increase in rack power. This is really the main challenge that traditional architecture is facing in order to be able to really connect in a more efficient way to the utility, medium voltage utility side.
Host: Okay. Now, when you think about this transformer in a solid-state form, does it— are we talking 100% solid-state or are there some magnetic components that still transfer over from the older technology?
Guest: That is absolutely correct. Solid-state transformers still use some sort of magnetic component, but the beauty of it is that the transformer is not as bulky, as large as the traditional low frequency transformers. We're talking about high frequency transformers. Just to give you a reference, still the same 1 megawatt low frequency transformer that weighs 3000 kg can be 40 times smaller and lighter with high frequency transformers that are typical technology that works in the range of 20, 30 kHz. of frequency and beyond. What is needed to be able to use this lighter and more compact technology? In the end, we need power semiconductors that are able to work at high frequencies, so have fast switching frequencies, and also being able at the same time to work with the voltage levels that are required to interface with the medium voltage grid.
What Infineon provides in this case is actually the silicon carbide technology that is able to both work at high frequency, so providing high efficiency in the power conversion stage and also having the right voltage classes to be able to interface with the medium voltage levels. And all of these are combined with the proven track record of high voltage silicon carbide technology that is already used in other applications, for example, solar and energy storage systems.
Host: So if you have to summarize, what can SST or solid-state transformers offer to this situation of AI centers popping up everywhere and having so much demand? What are the key points or the key takeaways from using a solid-state transformer to ease the issue of too much power needed?
Guest: Yeah. To put things into perspective, Peter, I would like probably to provide a brief overview about how power has evolved in terms of data center requirements for the rack. power specifically. In 2020, the typical rack power was in the range of 10 to 15 kW per rack. Then today we are typically talking about 100 kW, which is almost 10 times or more than that. And in the near future, there are projections that this rack power will actually reach several hundreds of kilowatts up to 1 megawatt in a single rack. This evolution of rack power levels is really challenging the traditional way the power is delivered to the rack.
For example, 1 megawatt rack, there is too much space taken from the power supplies to be actually to deliver the power required for the 1 megawatt computing rack. SSD in this game can play the role of freeing up space from the rack, from the white space. So instead of consuming space in the rack for the power supplies, with SSD we can remove that space, just leave all the space for the computing part and move the power conversion level, which is still required in a data center, upstream. In this case, from the rack level to the facility level and as close as possible to the medium voltage connection to the grid.
Host: Okay, so it sounds like that this is something that's not just nice to have, it's almost required, right? This has to happen.
Guest: Absolutely, yes. I mean, traditional architecture is not sustainable for this pace of increase in power demand. So, SST will definitely play a role in supporting the evolution for these increasing rack power levels.
Host: Okay, and we've talked about AI data centers, and you've made the case for SST in such a scenario, but what else, what other situations might benefit from SST?
Guest: Yeah, data centers and AI data centers are not the main application or the only application for SST, although it's probably the main one where this technology can really help solve the space utilization challenge. There are, however, other applications as well. For example, I could name the energy storage systems. So large utility-scale energy storage systems, these systems need reliable, efficient power conversion at medium voltage level. And typically, what they do is really transfer energy from and to the battery systems in the, for example, in case of battery energy storage systems. SST technology can also be used with energy storage systems to make sure that this transfer of energy from and to the battery to the grid is done in the most efficient and compact way. This is one example.
There is also another one which is about megawatt charging systems. These applications still had a strong demand for medium voltage to low voltage conversion done in a compact way and in a scalable way to make sure that the connection to the grid is, let's say, sustainable in a way. So again, SSD and the architecture behind SSD can really support megawatt charging systems of the future as well. Other applications that I found also relevant for SSD are, for example, solar, large solar inverters, and also marine.
Host: Let's get back to data centers for a while. How is the rollout going as far as SSD and their use in AI data centers?
Guest: I would say the rollout is going pretty fast. I was traveling throughout regions outside of Europe recently, and I was really fascinated to see the amount of development efforts that are being put into this technology. Demonstrations are happening now, today, this year, 2026, and there are field pilots that are expected in 2027. And all of this is in preparation for wider adoption starting from 2028. Definitely, there is a plan and a landscape, and the entire data center industry is actually preparing for that. I also wanted to mention that although the technology related to the SST is already available and scalable today, there are other elements beyond the SST itself that are still needed to make sure that this technology can be scaled up and used widely. For example, when talking about data centers that are using DC voltages or adopting DC microgrids, there are elements like DC voltage power production that are required to make sure that the SST technology can be deployed in field.
Host: Looking at this landscape of AI data centers and the SST, what is it that Infineon can offer or what is it you're working on that could aid in this situation?
Guest: So solid-state transformers, they are power systems that are doing power conversion from medium voltage to low voltage. Typically, these power systems are using modular architecture. textures with the stacked power cells. Because of the medium voltage connection, it's very important for SSD to leverage high voltage semiconductors. And here Infineon provides their silicon carbide EasyPACK™ modules. These modules are really designed for SSD, and the reason is they have a very wide voltage range from 750 volts up to 3300 V. And just to give you a reference, using a 3300 V silicon carbide EasyPACK™ in an SSD system can reduce the overall system complexity by 65% if this is compared with a traditional 1200 V silicon carbide device. So that's a lot of reduction in complexity. And high voltage typically in SSD need to come also with high reliability. Infineon is a pioneer in releasing to the market high voltage semiconductor technologies.
For example, for silicon carbide, Infineon released the 2000 V and the 2300 V, specifically tailoring the solar and energy storage systems applications for voltage levels in the range of 1500 V DC. It's very important to combine the two together. Still in the direction of reducing complexity, there are ongoing developments with silicon carbide discrete packages. which is another choice potentially available for SST architectures. And in some topologies and configurations, we also see gallium nitride technologies playing an important role thanks to the high efficiency and high switching frequencies. I also like to say that there is no power without control. So, Infineon's solution is really covering everything, not just the power switches, whether they are module or discrete packages, but also on the control side. And I would like to mention, of course, the auxiliary power supplies, the gate drivers, the current sensors, and the microcontrollers. All of them play an important role in making sure the SST can run efficiently, reliably in the highly demanding application for AI data centers.
Host: Okay, so Infineon offers a nice system that supports each other and works for a common solution.
Guest: Correct.
Host: Okay, good. And what if you were to look forward and maybe go down the road a little bit in this area of SST and AI data centers, sticking with that theme. What do you see? I mean, let's say 5 years down the road, do you have a vision of how things will be? Or maybe 10 years even?
Guest: That's a nice view. What I personally see is that SST today is already helping to transition to an architecture that can really reduce the space utilization or the space used by the large power converter systems interfaced with the medium voltage and also increase efficiency. And this is specifically relevant for DC loads. Loads with DC voltages, for example, we could name AI data centers and megawatt charging systems. This is already something happening today. In the future, it could be 5 years from now, for example, SST could also actually help with the transition from medium voltage AC grids to medium voltage DC grids. In this case, there is also a further reduction in the number of conversion stages, so a further improvement in overall efficiency. And also, there is the possibility to integrate seamlessly sources of green energy, which could be, for example, hydrogen in the future.
Host: Thanks so much for taking some of your time today to explain your part in rolling out SST in the AI data center world where they're probably most needed. Thank you.
Guest: Thank you, Peter.
Host: And thank you to our audience for joining today. Make sure you subscribe to the Podcast4Engineers so you get the latest updates, and we'll see you soon.