Automotive USB Hub and Charging Design
Understanding in-cabin USB charging systems
Every modern car needs power for phones, tablets, and other devices. That is why the automotive USB charger has become a core part of in-cabin design, and a well-built USB car charger that now sits at every seat.
Drivers and passengers expect fast charging and more than one extra USB port.
Modern USB car charger designs meet this need through:
- USB-C ports
- Power Delivery (PD) controllers and hubs
These parts must be small, safe, and built to automotive standards.
For years, cars relied on USB-A ports, which offered limited charging power and relatively slow data transfer. Most new vehicle designs now use USB-C, which supports higher power delivery through a compact connector and can also carry data and video, depending on the system design. This enables convenient charging ports for both front and rear passengers, and in many new vehicles USB-C is increasingly supplementing – or partially replacing – the traditional 12V outlet for powering personal devices.
The transition also aligns with global regulations: in the EU, the Common Charger Directive requires USB-C charging ports for smartphones, tablets, and many other electronic devices from December 2024, with laptops following in April 2026.
USB Power Delivery (PD) is the key to flexible charging. PD lets a port adjust its output to match the device, so one port can power a phone, a tablet, or a laptop.
Infineon's automotive USB-C controllers comply with USB PD revision 3.2 and support Programmable Power Supply (PPS) across a wide voltage range.
A single-port automotive USB-C PD controller can support power output of up to 100 W on one port, allowing the system to function as a versatile USB power source for a wide range of devices.
USB Power Delivery (PD) safely negotiates the required voltage and current between the charger and the connected device, enabling efficient charging across multiple power profiles. The charger only supplies the power that has been negotiated and requested by the connected device.
USB Power Delivery (PD) is the key to flexible charging. PD lets a port adjust its output to match the device, so one port can power a phone, a tablet, or a laptop.
Infineon's automotive USB-C controllers comply with USB PD revision 3.2 and support Programmable Power Supply (PPS) across a wide voltage range.
A single-port automotive USB-C PD controller can support power output of up to 100 W on one port, allowing the system to function as a versatile USB power source for a wide range of devices.
USB Power Delivery (PD) safely negotiates the required voltage and current between the charger and the connected device, enabling efficient charging across multiple power profiles. The charger only supplies the power that has been negotiated and requested by the connected device.
A USB hub automotive solution lets one system run many ports at once. The hub manages data from each port, while a PD controller manages the power. Together they form the heart of the in-cabin charger, and they let a single design charge multiple devices at the same time.
Automotive hub ICs face hard demands. They must be small, efficient, and built for heat, and they need strong protection on every port.
The main protections are:
- Overvoltage (OVP)
- Overcurrent (OCP)
- Short-circuit (SCP) defense
- ESD (electrostatic discharge) protection
Infineon's CCG7S integrates OVP, OCP, SCP, and ESD protection on chip, and it also adds VBUS short protection. This on-chip integration cuts the bill of materials, saves board space, and improves reliability.
A USB hub automotive solution lets one system run many ports at once. The hub manages data from each port, while a PD controller manages the power. Together they form the heart of the in-cabin charger, and they let a single design charge multiple devices at the same time.
Automotive hub ICs face hard demands. They must be small, efficient, and built for heat, and they need strong protection on every port.
The main protections are:
- Overvoltage (OVP)
- Overcurrent (OCP)
- Short-circuit (SCP) defense
- ESD (electrostatic discharge) protection
Infineon's CCG7S integrates OVP, OCP, SCP, and ESD protection on chip, and it also adds VBUS short protection. This on-chip integration cuts the bill of materials, saves board space, and improves reliability.
USB-C and hub ICs serve multiple locations throughout the vehicle cabin. The most common deployment is the head-unit power module, often built as a breakout box, which typically offers two or more USB-C ports for:
- Data transfer
- Apple CarPlay
- Android Auto
- Mass-storage access
- USB Power Delivery (PD) for charging connected devices
Beyond the head unit, automotive-grade controllers are also used in rear-seat chargers and rear-seat entertainment systems, extending the same charging and data capabilities to passengers in the rear.
High-end dual-port automotive USB-C PD controllers can support up to 100 W per port, so a single chip can serve two seats with full power in a dual-port setup.
This enables a dual-port automotive USB car charger design that delivers high charging power to multiple passengers simultaneously across both front and rear seating areas.
For single-port applications, a comparable single-port controller offers the same robust protection and thermal management in a more compact form factor.
Both single- and dual-port designs typically feature programmable temperature monitoring through external thermistors and integrated thermal throttling, allowing designers to customize how the charger responds to heat – critical for keeping cabins comfortable during long journeys.
These controllers can also be configured to support DisplayPort Alternate Mode for rear-seat entertainment applications, where a single USB-C connector can simultaneously deliver power and video to rear displays.
Infineon's EZ-PD™ CCG7D, for example, is a dual-port automotive USB-C PD controller supporting up to 100 W per port with these capabilities.
Cars are full of electrical noise, since motors, sensors, and radios all share a tight space. An automotive USB charger must not disturb these systems, and it must continue operating reliably in the presence of that noise.
This is the EMI/EMC challenge:
- EMI means the noise a part sends out.
- EMC means how well a part resists noise.
In automotive design, the key standard is CISPR 25, which sets limits to protect the car's radio receivers, such as AM, FM, GPS, and Bluetooth. Carmakers routinely require CISPR 25 compliance before they approve a part.
Designers meet these limits in a few ways:
- Efficient switching to lower emissions, plus filters and careful board layout.
- A tuneable switching frequency also helps, and Infineon's CCG7x buck-boost controller can run between 150 kHz and 600 kHz with input tolerance up to 40 V. This lets designers shift noise away from sensitive radio bands, which keeps the whole cabin stable.
Car parts must pass strict tests, and the main standard is AEC-Q100, which checks how an integrated circuit survives heat, stress, and time.
Infineon's EZ-PD™ portfolio includes AEC-Q100-qualified versions for automotive use. Automotive controllers:
- Carry an Automotive Grade-S rating
- Operate across a temperature range of −40° C to +105° C
- Run on an operating voltage range from 4 V to 24 V, which suits the car's battery line
Higher power means more heat. The cabin can already be hot from sun and engine warmth, and charging adds even more, so heat is one of the biggest design challenges for an in-cabin charger. Designers manage it by picking efficient PD controllers that waste less energy, and a buck-boost stage, integrated on chip, helps convert power efficiently.
When a port still gets too hot, the system uses thermal throttling. The CCG7x includes a 32-bit Arm® Cortex®-M0 processor that enables custom functions like multistep power throttling and temperature monitoring, and the chip also offers GPIOs for thermistors. So, it can read the port temperature in real time, and if it rises too high, the controller reduces the current. Charging slows but never stops in an unsafe way, and once the port cools, full power returns. A well-designed fast charger throttles in small steps, which keeps the experience smooth for the user.
USB-C does more than charge, since it also carries data and video. This is one of its strongest benefits in cars. A single USB-C port can run a rear-seat display, and the CCG7x supports DisplayPort Alternate Mode for this purpose.
One cable carries both the power and the picture:
- The PD controller supplies the power
- The hub and the port handle the data
This supports screens, tablets, and gaming devices in the back. So, USB-C turns one port into a flexible power source and a data link, and the result is a richer cabin experience for every passenger.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
What USB standards are typically used in automotive systems?
Most new cars use USB-C with USB Power Delivery (PD). USB-C handles both data and power through one reversible plug. Infineon's automotive USB-C controllers comply with USB PD revision 3.2. PD lets a port match its output to each device. Many systems pair a USB hub with a PD controller to run several ports at once.
What protection is required for automotive USB ports?
Automotive USB ports need overvoltage (OVP), overcurrent (OCP), and short-circuit (SCP) protection. They also need ESD protection against static pulses. On Infineon's controllers, these features are built into the PD controller, along with VBUS short protection. This keeps each port safe in the harsh cabin environment.
How much power can automotive USB-C ports deliver?
USB-C with PD covers a wide range. A basic port may deliver around 18W USB output for a phone. Infineon's automotive controllers scale up to 100W per port. The exact level depends on the controller and the system power budget.
What are the different thermal design considerations?
Heat is the main concern. The cabin can already be hot, and charging adds more heat. Designers use efficient controllers, smart part placement, and airflow to manage it. An integrated buck-boost stage also improves efficiency and lowers heat.
How is thermal throttling handled during high power charging?
Infineon's controllers use a built-in Arm® Cortex®-M0 processor and thermistor inputs to watch temperature in real time. If a port gets too hot, the controller lowers the current. Charging slows for a short time, then returns to full power once the port cools. This protects the device, the cable, and the car.
What charging power target is required per port?
It depends on the use. Front-seat phone ports often target 18W to 30W, and a quality USB cable must support that level. Rear-seat tablet ports may target 30W to 60W, where an automotive USB cable rated for higher power is needed. Laptop-capable ports may target up to 100W. These are common tiers, not fixed rules.
What is the automotive qualification level target for USB-C in-cabin charging?
Automotive ICs are qualified to AEC-Q100. Infineon's automotive USB-C controllers carry an Automotive Grade-S rating and operate from −40° C to +105° C. This makes them suitable for the temperature swings inside a vehicle cabin.
What controllers does Infineon offer for automotive USB charging?
Infineon's EZ-PD™ portfolio includes the CCG7S (single-port) and CCG7D (dual-port) supporting USB PD 3.2 with advanced thermal management and DisplayPort Alt Mode. For applications requiring USB PD 3.0, the CCG3PA provides a proven alternative. Choose based on your performance requirements and power delivery version.
Are waterproof or dustproof requirements applicable?
Full waterproofing is not always needed in a dry cabin. But ports near doors, cup holders, or open consoles can face spills and dust. Sealed connectors and basic dust resistance help these ports last.
Are rear-seat displays supported through USB-C?
Yes. One USB-C port can carry both power and video. This lets a single cable run a rear-seat screen. The PD controller supplies the power while the hub and port handle the data. Infineon's controllers target head-unit, rear-seat charger, and rear-seat entertainment uses.