Infineon and RT-Labs integrate six key industrial communication protocols into XMC7000 microcontroller family
Infineon and RT-Labs integrate six key industrial communication protocols into XMC7000 microcontroller family
Technology news
Munich, Germany – 20 March 2025 – As the industry embraces digital transformation and the principles of Industry 4.0, communication protocols in industrial automation are becoming more important than ever. To enable seamless data exchange and control in automation systems, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY), together with its partner RT-Labs, a provider of industrial communication solutions, has integrated six Fieldbus and Ethernet-based protocols in the firmware of the Infineon XMC7000 industrial microcontroller. The firmware is available through Infineon's ModusToolbox™ development platform, providing access to all major industrial communication protocols in a single software solution. This enables users to quickly and easily implement the required protocols on the XMC7000 microcontroller, fully utilizing its high-performance capabilities in various applications, including servo drives, I/O modules, robotic arms, industrial gateways, PLCs, and more.
“Infineon’s XMC microcontrollers have a long history of enabling the factory floor. As Industry 4.0 continues to build momentum, existing Fieldbus and Ethernet-based protocols are critical for industrial automation,” said Panagiotis Venardos, Senior Product Manager Microcontroller at Infineon. “We continue to invest in higher performance microcontrollers and connected MCUs to help drive further enhancements to how the factory floor seamlessly communicates. Our partner RT-Labs helps bring scale to this effort with their field-proven and highly optimized Ethernet and Fieldbus protocol stacks.”
“At RT-Labs, we believe industrial communication should be effortless. As a Premium Partner with Infineon, we’re bringing plug-and-play connectivity to ModusToolbox,” said Marcus Ekerhult, CMO RT-Labs. “With support for leading protocols and U-Phy technology, developers can now accelerate development and launch products faster while ensuring reliability and compliance. We’re excited for this partnership and the innovations it will unlock.”
Industrial communication protocols are standardized sets of rules and procedures that govern the exchange of data between devices and systems in an industrial automation environment. As a result of the collaboration between Infineon and RT-Labs, customers now have access to the following communication protocols: PROFINET RT, EtherNet/IP, CANopen, CC-Link, Modbus/TCP, EtherCAT Master. A GitHub repository hosts the middleware, ensuring up-to-date, easily accessible libraries. In addition, Infineon supports implementation by providing user-friendly code examples and comprehensive documentation, eliminating the need for in-depth expertise or extensive resources on the customer’s side.
Availability
The software is available now. Further information is available at www.infineon.com/XMC7000.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
INF XMC 7000
Infineon’s industrial microcontrollers XMC7000 enable seamless data exchange and control of automation systems
JPEG
2126x2004 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFCSS202503-082