Future-proof security solution: Infineon launches world’s first TPM with a PQC-protected firmware update mechanism
Future-proof security solution: Infineon launches world’s first TPM with a PQC-protected firmware update mechanism
Technology news
Munich, Germany – 15 February, 2022 – Quantum computing is expected to have a significant impact on cybersecurity, specifically on the confidentiality of encrypted data and on the integrity of digital signatures. To address these challenges, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is taking security to the next level with the new OPTIGA™ TPM (Trusted Platform Module) SLB 9672, a future-proof security solution with a post-quantum cryptography (PQC) protected firmware update mechanism using XMSS signatures.
This mechanism counteracts the threat of firmware corruption by attackers with access to quantum computers and increases long term survivability of the device by enabling a quantum-resistant firmware upgrade path. The standardized, out-of-the-box TPM provides a solid foundation for securely establishing the identity and software status of PCs, servers, and connected devices, and for protecting the integrity and confidentiality of data at rest and in transit.
Infineon’s latest addition of the OPTIGA TPM family is the industry’s first TPM to offer a firmware update mechanism with a 256-bits key length, along with an additional check based on PQC. With this strong and trusted update mechanism, the OPTIGA TPM SLB 9672 can still be updated if the standard algorithms are no longer trusted. Its design is engineered for improved computing performance with fail-safe features that counteract the effects of corrupted firmware. For instance, built-in fail-safe features enable TPM firmware recovery in accordance with the NIST SP 800-193 Platform Firmware Resiliency Guidelines.
This TPM also provides an expanded non-volatile memory to store new features such as additional certificates and cryptographic keys. Security evaluation and certification are performed by independent bodies according to the Common Criteria and FIPS requirements. The new TPM also fully complies with the Trusted Computing Group (TCG) requirements (TPM 2.0 standard version 1.59) and is certified according to the latest TPM 2.0 standard.
Featuring a standardized trust base, as well as various tools to support design activities (software/demo boards), this TPM enables easy integration with host software. It also supports the latest versions of Windows and Linux. Furthermore, the chip boasts an extended temperature range of -40°C to 105°C. Infineon is committed to the long-term availability of OPTIGA TPM SLB 9672 for a minimum of ten years and offers tailored support and maintenance through the Infineon Security Partner Network (ISPN). With this long-term commitment, customers can not only rely on the TPM’s continued availability but also on Infineon’s support.
Availability
The OPTIGA TPM SLB 9672 can be ordered now. More information is available at www.infineon.com/OPTIGA-TPM-SLB9672 and www.infineon.com/OPTIGA-TPM-SLB9672-kit.
Please note: An Online Media Briefing will be held on 16 February, 2022 during which Guillaume Raimbault, Senior Manager TPM Product Marketing & Management of Infineon’s Connected Secure Systems Division, will present additional information about the new OPTIGA TPM SLB 9672.
Press Photos
OPTIGA™-TPM SLB9672 combi
Infineon’s latest addition of the OPTIGA™ TPM family is the industry’s first TPM to offer a firmware update mechanism with a 256-bits key length, along with an additional check based on PQC. With this strong and trusted update mechanism, the OPTIGA TPM SLB 9672 can still be updated if the standard algorithms are no longer trusted. Its design is engineered for improved computing performance with fail-safe features that counteract the effects of corrupted firmware.
JPEG
1500x1025 px
OPTIGA™-TPM SLB9672
Infineon’s latest addition of the OPTIGA™ TPM family is the industry’s first TPM to offer a firmware update mechanism with a 256-bits key length, along with an additional check based on PQC. With this strong and trusted update mechanism, the OPTIGA TPM SLB 9672 can still be updated if the standard algorithms are no longer trusted. Its design is engineered for improved computing performance with fail-safe features that counteract the effects of corrupted firmware.
JPEG
2126x1503 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFCSS202202-051