- Smart TV
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
Nov 17, 2026
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
Nov 17, 2026
Business & Financial Press
Nov 11, 2026
Quarterly Report
Nov 10, 2026
Business & Financial Press
Nov 09, 2026
Infineon hybrid flyback controller XDP™ combined with CoolGaN™ IPS enable Anker to achieve higher efficiency and power density in charger designs
Infineon hybrid flyback controller XDP™ combined with CoolGaN™ IPS enable Anker to achieve higher efficiency and power density in charger designs
Technology news
Munich, Germany, and Shenzhen, China – 25 July, 2022 – With the rising number of mobile devices, notebooks and battery-powered equipment, the need for increased charging power and fast charging has emerged. For engineers, this trend poses the challenge of achieving ever-higher power levels in smaller form factors while simultaneously meeting thermal performance requirements. To address these contemporary design needs, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) combines the hybrid flyback (HFB) controller XDP™ digital power controller XDPS2201 and the CoolGaN™ integrated power stage (IPS) 600 V (IGI60F1414A1L) for high-efficiency and high-power density charger and adapter designs.
Anker has chosen Infineon’s next-generation HFB controller and the CoolGaN IPS for fast chargers above 100 W, achieving market-leading power density. “By combining Infineon's hybrid flyback controller with an integrated CoolGaN device in Anker's new charging lineup, we achieved an outstanding system-level efficiency beyond 95 percent,” said Adam White, Division President of Infineon’s Power and Sensor Systems Division. “This architecture reduces energy loss by 21 percent compared to other charging solutions. It is the first time that Infineon's HFB controller and CoolGaN IPS devices are combined and applied commercially in the consumer electronics market.”
“GaN has completely changed the way we charge our electronics by delivering superior power transfer efficiency, faster-charging speeds and improved portability to our chargers,” said Steven Yang, CEO of Anker Innovations.
More information about Infineon’s offering for USB-C adapters and chargers is available at www.infineon.com/usb-pd.
About Anker Innovations
Anker Innovations is a global leader in charging technology and a developer of unique, consumer electronic products that support premium audio, mobile entertainment and the emerging smart home space. This innovation is being led by its six key brands: Anker, AnkerWork, eufy, Nebula, Soundcore and now, AnkerMake. More information about Anker Innovations and its various brands is available at www.anker.com.
More information about Infineon’s contribution to energy efficiency: www.infineon.com/green-energy
Press Photos
anker 1
For the first time Infineon's hybrid flyback controller XDP™and CoolGaN™ IPS devices are combined and applied commercially in the consumer electronics market. The Anker charging devices achieves an outstanding system-level efficiency beyond 95 percent, its architecture reduces energy loss by 21 percent compared to other charging solutions.
JPEG
1514x2126 px
anker 2
For the first time Infineon's hybrid flyback controller XDP™and CoolGaN™ IPS devices are combined and applied commercially in the consumer electronics market. The Anker charging devices achieves an outstanding system-level efficiency beyond 95 percent, its architecture reduces energy loss by 21 percent compared to other charging solutions.
JPEG
2126x2126 px
Share in WeChat
Scan the QR code with your WeChat App to share this page.
Information Number : INFPSS202207-102